PlotColorsWidthsBuilderColor Enumeration¶
NXOpen.PlotColorsWidthsBuilder.Color is an alias for NXOpen.PlotColorsWidthsBuilderColor
-
class
NXOpen.
PlotColorsWidthsBuilderColor
¶ Bases:
object
Specifies the color option to use when plotting.
Enum Members
Enum Member Enum Member Description AsDisplayed As DisplayedPartColors Part ColorsCustomPalette Custom PaletteBlackOnWhite Black on WhiteLegacyColors Legacy ColorsColorsByWidth Colors by Width-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-