DirectionOnCurveOption Enumeration¶
NXOpen.Direction.OnCurveOption is an alias for NXOpen.DirectionOnCurveOption
-
class
NXOpen.
DirectionOnCurveOption
¶ Bases:
object
Specifies the direction in relation to a curve.
Enum Members
Enum Member Enum Member Description Tangent Creates direction tangent to curve.Normal Creates direction normal to curve.Binormal Creates direction binormal to curve (B = T x N).-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-