ArcCollection Class¶
-
class
NXOpen.
ArcCollection
¶ Bases:
object
Represents a collection of arcs.
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.Arc with the given identifier as recorded in a journal. |
Method Detail¶
FindObject¶
-
ArcCollection.
FindObject
¶ Finds the
NXOpen.Arc
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the arc Returns: Return type: NXOpen.Arc
New in version NX3.0.0.
License requirements: None.