RegionBoundaryRule Class¶
-
class
NXOpen.
RegionBoundaryRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects curves as specified by an enclosed region.New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the region boundary rule: NXOpen.RegionBoundaryRule |
Method Detail¶
Dispose¶
-
RegionBoundaryRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX6.0.0.
License requirements: None.
GetData¶
-
RegionBoundaryRule.
GetData
¶ Gets the data for the region boundary rule:
NXOpen.RegionBoundaryRule
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (seedObj, curves, seedPoint, distanceTolerance). seedObj is a
NXOpen.DisplayableObject
. Face or Sketch curves is a list ofNXOpen.Curve
. Curves input to create this rule seedPoint is aNXOpen.Point3d
. Seed point distanceTolerance is a float. Distance tolerance .. versionadded:: NX6.0.0License requirements: gateway (“UG GATEWAY”)