Spreadsheet Class¶
-
class
NXOpen.
Spreadsheet
¶ Bases:
NXOpen.TransientObject
Represents a class for internal spreadsheet.
To call functions from this class, use
Spreadsheet
object returned byNXOpen.SpreadsheetManager.Open()
. .. Usable only on WindowsNew in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Clear | Clears the contents of the current worksheet. |
Delete | Deletes (clears) one or more rows/columns of data from a worksheet. |
DeleteSheets | Deletes specified number of sheets beginning with the specified sheet (from the current worksheet, if no sheet is specified). |
Dispose | Free resources associated with the instance. |
EraseRange | Clears the contents of the specified range |
EvaluateCell | Returns the evaluated value of a cell. |
GetFormula | Retrieves a formula from a cell. |
GetNamedRange | Resolves the named reference and returns the range of cells that are named This method returns a list, of the following format: Start Row, Start Column, End Row, End Column, Start Sheet Number, End Sheet Number of the named reference. |
GetNumber | Retrieves a numeric value from a cell. |
GetNumberOfSheets | Returns the total number of sheets in the spreadsheet @return Number of sheets in the spreadsheet |
GetSheetNames | Returns list of existing sheet names in the spreadsheet. |
GetSheetNumber | Returns the current work sheet number of the spreadsheet. |
GetSheetNumberOfName | Returns sheet number of the sheet with given name. |
GetString | Returns the String in the cell @return Retrieves a string value from a cell |
GetValue | Returns a number, string or formula depending on the contents of the cell. |
InsertSheets | Inserts specified number of sheets before the specified sheet (or the current work sheet if no sheet is specified). |
Recalculate | Recalculates the spreadsheet. |
Save | Saves the spreadsheet in the part file. |
SetFormula | Stores a formula into a cell. |
SetNamedRange | Defines a name for the Range of cells. |
SetNumber | Stores a numeric value in the specified cell of the worksheet. |
SetSheetNumber | Sets the worksheet with specified index as current worksheet |
SetString | Sets the string in the cell. |
Terminate | Terminates excel sheet for opened part. |
Method Detail¶
Clear¶
-
Spreadsheet.
Clear
¶ Clears the contents of the current worksheet.
Signature
Clear()
New in version NX11.0.0.
License requirements: None.
Delete¶
-
Spreadsheet.
Delete
¶ Deletes (clears) one or more rows/columns of data from a worksheet.
Signature
Delete(start1, end1, sheet, operation)
Parameters: - start1 (int) – From where the deletion should start
- end1 (int) – Upto where the rows should be deleted
- sheet (int) – The sheet in which deletion should take place.(Current sheet, if no sheet is specified)
- operation (int) – 1 for row deletion and 2 for column deletion.
New in version NX11.0.0.
License requirements: None.
DeleteSheets¶
-
Spreadsheet.
DeleteSheets
¶ Deletes specified number of sheets beginning with the specified sheet (from the current worksheet, if no sheet is specified).
Signature
DeleteSheets(sheet, count)
Parameters: - sheet (int) – Sheet Number, starting from which sheets are to be deleted.
- count (int) – Number of sheets to be deleted
New in version NX11.0.0.
License requirements: None.
Dispose¶
-
Spreadsheet.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
EraseRange¶
-
Spreadsheet.
EraseRange
¶ Clears the contents of the specified range
Signature
EraseRange(row0, col0, row1, col1, sheet0, sheet1)
Parameters: - row0 (int) – Starting row for range
- col0 (int) – Starting column for range
- row1 (int) – Ending row for range
- col1 (int) – Ending column for range
- sheet0 (int) – Sheet number for start of the range
- sheet1 (int) – Sheet number for end of the range
New in version NX11.0.0.
License requirements: None.
EvaluateCell¶
-
Spreadsheet.
EvaluateCell
¶ Returns the evaluated value of a cell.
Signature
EvaluateCell(row, col, sheet)
Parameters: - row (int) – Row index of the cell
- col (int) – Column index of the cell
- sheet (int) – Sheet index (current worksheet, if zero is specified).
Returns: The value in a spreadsheet cell as either a string or a number
Return type: New in version NX11.0.0.
License requirements: None.
GetFormula¶
-
Spreadsheet.
GetFormula
¶ Retrieves a formula from a cell.
Signature
GetFormula(row, col, sheet)
Parameters: - row (int) – Row index of the cell
- col (int) – Column index of the cell
- sheet (int) – Sheet index (current worksheet, if zero is specified)
Returns: Retrieves a formula from a cell.
Return type: New in version NX11.0.0.
License requirements: None.
GetNamedRange¶
-
Spreadsheet.
GetNamedRange
¶ Resolves the named reference and returns the range of cells that are named This method returns a list, of the following format: Start Row, Start Column, End Row, End Column, Start Sheet Number, End Sheet Number of the named reference.
Signature
GetNamedRange(rangename)
Parameters: rangename (str) – Range name Returns: The range of cells for given range name Return type: list of int New in version NX11.0.0.
License requirements: None.
GetNumber¶
-
Spreadsheet.
GetNumber
¶ Retrieves a numeric value from a cell.
Signature
GetNumber(row, col, sheet)
Parameters: - row (int) – Row index of the cell
- col (int) – Column index of the cell
- sheet (int) – Sheet index (current worksheet, if zero is specified)
Returns: Retrieves a numerical value from a cell
Return type: New in version NX11.0.0.
License requirements: None.
GetNumberOfSheets¶
-
Spreadsheet.
GetNumberOfSheets
¶ Returns the total number of sheets in the spreadsheet
Signature
GetNumberOfSheets()
Returns: Number of sheets in the spreadsheet Return type: int New in version NX11.0.0.
License requirements: None.
GetSheetNames¶
-
Spreadsheet.
GetSheetNames
¶ Returns list of existing sheet names in the spreadsheet.
Signature
GetSheetNames()
Returns: List of sheet names from specified spreadsheet Return type: list of str New in version NX11.0.0.
License requirements: None.
GetSheetNumber¶
-
Spreadsheet.
GetSheetNumber
¶ Returns the current work sheet number of the spreadsheet.
Signature
GetSheetNumber()
Returns: Current work sheet number of the spreadsheet. Return type: int New in version NX11.0.0.
License requirements: None.
GetSheetNumberOfName¶
-
Spreadsheet.
GetSheetNumberOfName
¶ Returns sheet number of the sheet with given name.
Signature
GetSheetNumberOfName(sheetname)
Parameters: sheetname (str) – Sheet name Returns: Work sheet number of the given spreadsheet name. Return type: int New in version NX11.0.0.
License requirements: None.
GetString¶
-
Spreadsheet.
GetString
¶ Returns the String in the cell
Signature
GetString(row, col, sheet)
Parameters: - row (int) – Row index of the cell
- col (int) – Column index of the cell
- sheet (int) – Sheet index of the cell (current worksheet, if zero is specified).
Returns: Retrieves a string value from a cell
Return type: New in version NX11.0.0.
License requirements: None.
GetValue¶
-
Spreadsheet.
GetValue
¶ Returns a number, string or formula depending on the contents of the cell.
Signature
GetValue(row, col, sheet)
Parameters: - row (int) – Row index of the cell
- col (int) – Column index of the cell
- sheet (int) – Sheet index of the cell (current worksheet, if zero is specified).
Returns: The value in a spreadsheet cell as either a string or a number
Return type: New in version NX11.0.0.
License requirements: None.
InsertSheets¶
-
Spreadsheet.
InsertSheets
¶ Inserts specified number of sheets before the specified sheet (or the current work sheet if no sheet is specified).
Signature
InsertSheets(sheet, count)
Parameters: - sheet (int) – Sheet number, before which the sheets are to be inserted.
- count (int) – Number of sheets to be inserted.
New in version NX11.0.0.
License requirements: None.
Recalculate¶
-
Spreadsheet.
Recalculate
¶ Recalculates the spreadsheet.
Signature
Recalculate()
New in version NX11.0.0.
License requirements: None.
Save¶
-
Spreadsheet.
Save
¶ Saves the spreadsheet in the part file.
Signature
Save()
New in version NX11.0.0.
License requirements: None.
SetFormula¶
-
Spreadsheet.
SetFormula
¶ Stores a formula into a cell.
Signature
SetFormula(row, col, cellvalue, sheet)
Parameters: - row (int) – Row index of the cell
- col (int) – Column index of the cell
- cellvalue (
NXOpen.SpreadsheetCellData
) – - sheet (int) – Sheet index of the cell (current worksheet, if zero is specified).
New in version NX11.0.0.
License requirements: None.
SetNamedRange¶
-
Spreadsheet.
SetNamedRange
¶ Defines a name for the Range of cells.
Signature
SetNamedRange(rangename, row0, col0, row1, col1, sheet)
Parameters: - rangename (str) – Name to be given to the range
- row0 (int) – Starting row of the table, which is being named
- col0 (int) – Starting column of the table, which is being named
- row1 (int) – Row of the table, upto which the name will apply
- col1 (int) – Column of the table, upto which the name will apply
- sheet (int) – Sheet index of the table (current worksheet, if zero is specified).
New in version NX11.0.0.
License requirements: None.
SetNumber¶
-
Spreadsheet.
SetNumber
¶ Stores a numeric value in the specified cell of the worksheet.
Signature
SetNumber(row, col, cellvalue, sheet)
Parameters: - row (int) – Row index of the cell
- col (int) – Column index of the cell
- cellvalue (
NXOpen.SpreadsheetCellData
) – Numeric value to be set in the cell. - sheet (int) – Sheet index (current worksheet, if zero is specified).
New in version NX11.0.0.
License requirements: None.
SetSheetNumber¶
-
Spreadsheet.
SetSheetNumber
¶ Sets the worksheet with specified index as current worksheet
Signature
SetSheetNumber(sheet)
Parameters: sheet (int) – The number to which the current work sheet is to be set. New in version NX11.0.0.
License requirements: None.
SetString¶
-
Spreadsheet.
SetString
¶ Sets the string in the cell.
Signature
SetString(row, col, cellvalue, sheet)
Parameters: - row (int) – Row index of the cell.
- col (int) – Column index of the cell.
- cellvalue (
NXOpen.SpreadsheetCellData
) – String to be stored in this cell. - sheet (int) – Sheet index (current worksheet, if zero is specified).
New in version NX11.0.0.
License requirements: None.