IgesCreatorExportFromOption Enumeration¶
NXOpen.IgesCreator.ExportFromOption is an alias for NXOpen.IgesCreatorExportFromOption
-
class
NXOpen.
IgesCreatorExportFromOption
¶ Bases:
object
Export From Option
Enum Members
Enum Member Enum Member Description DisplayPart export data from displayed partExistingPart export data from existing part which is on disk-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-