FlatteningBuilderFlatteningConstantType Enumeration¶
NXOpen.FlatteningBuilder.FlatteningConstantType is an alias for NXOpen.FlatteningBuilderFlatteningConstantType
-
class
NXOpen.
FlatteningBuilderFlatteningConstantType
¶ Bases:
object
This enum defines the flattening constraints types.
Enum Members
Enum Member Enum Member Description NoConstraints No constraintsConstantCurveLength Force constant lengthConstantFaceArea Force constant areaConstantBodyVolume force constant volume of the body-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-