TracelineCollection Class¶
-
class
NXOpen.
TracelineCollection
¶ Bases:
object
Represents a collection of tracelines
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateAutomaticTraceline | Create an automatic traceline @return Created traceline |
Method Detail¶
CreateAutomaticTraceline¶
-
TracelineCollection.
CreateAutomaticTraceline
¶ Create an automatic traceline
Signature
CreateAutomaticTraceline(explosion, startPoint, startDirection, endPoint, endDirection, orientation, mode, solution, startOffset, endOffset, segmentIndices, segmentLengths)
Parameters: - explosion (
NXOpen.Assemblies.Explosion
) – Explosion - startPoint (
NXOpen.Point
) – Start point - startDirection (
NXOpen.Direction
) – Start direction - endPoint (
NXOpen.Point
) – End point - endDirection (
NXOpen.Direction
) – End direction - orientation (
NXOpen.Matrix3x3
) – Orientation - mode (
NXOpen.AutomaticTracelineModeOption
) – Mode - solution (int) – Solution number
- startOffset (float) – Start offset
- endOffset (float) – End offset
- segmentIndices (list of int) – Segment indices
- segmentLengths (list of float) – Segment lengths
Returns: Created traceline
Return type: New in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- explosion (