SpreadsheetManagerLookupMode Enumeration¶
NXOpen.SpreadsheetManager.LookupMode is an alias for NXOpen.SpreadsheetManagerLookupMode
-
class
NXOpen.
SpreadsheetManagerLookupMode
¶ Bases:
object
Modes of lookup in the table.
New in version NX11.0.0.
Enum Members
Enum Member Enum Member Description Exact Requires an exact matchHigher Returns the higher cellLower Returns the lower cellClosest Returns the closest cell-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-