WCS Class¶
-
class
NXOpen.
WCS
¶ Bases:
object
Represents the World Coordinate System.
The origin coordinates and orientation matrix are always relative to the absolute coordinate system.
In order to use any of the WCS methods, the display part must be the part that owns the WCS.
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
CoordinateSystem | Returns the CartesianCoordinateSystem associated with the WCS |
Origin | Returns or sets the origin of the WCS |
Visibility | Returns or sets the visibility of the WCS |
Methods¶
Method | Description |
---|---|
Rotate | Rotates the WCS about the specified axis. |
Save | Saves the WCS. |
SetCoordinateSystem | Changes the coordinate system of the WCS to a new coordinate system. |
SetCoordinateSystemCartesianAtCsys | Creates a WCS at a new coordinate system. |
SetOriginAndMatrix | Sets the origin and orientation matrix of the WCS |
Enumerations¶
WCSAxis Enumeration | Specifies the X, Y, or Z axis |
Property Detail¶
CoordinateSystem¶
-
WCS.
CoordinateSystem
¶ Returns the CartesianCoordinateSystem associated with the WCS
-------------------------------------
Getter Method
Signature
CoordinateSystem()
Returns: Return type: NXOpen.CartesianCoordinateSystem
New in version NX3.0.0.
License requirements: None.
Origin¶
-
WCS.
Origin
¶ Returns or sets the origin of the WCS
-------------------------------------
Getter Method
Signature
Origin()
Returns: Return type: NXOpen.Point3d
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Origin(origin)
Parameters: origin ( NXOpen.Point3d
) –New in version NX3.0.0.
License requirements: None.
Visibility¶
-
WCS.
Visibility
¶ Returns or sets the visibility of the WCS
-------------------------------------
Getter Method
Signature
Visibility()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility(isVisible)
Parameters: isVisible (bool) – New in version NX3.0.0.
License requirements: None.
Method Detail¶
Rotate¶
-
WCS.
Rotate
¶ Rotates the WCS about the specified axis.
The angle is in degrees.
Signature
Rotate(rotationAxis, angle)
Parameters: - rotationAxis (
NXOpen.WCSAxis
) – Which WCS axis to rotate about (X, Y, or Z) - angle (float) – Angle of rotation in degrees
New in version NX3.0.0.
License requirements: None.
- rotationAxis (
Save¶
-
WCS.
Save
¶ Saves the WCS.
A new cartesian coordinate system is created in the **work</b> part, even though the WCS is owned by the display part.
Signature
Save()
Returns: The saved coordinate system Return type: NXOpen.CartesianCoordinateSystem
New in version NX3.0.0.
License requirements: None.
SetCoordinateSystem¶
-
WCS.
SetCoordinateSystem
¶ Changes the coordinate system of the WCS to a new coordinate system.
The return value is the old coordinate system. The old coordinate system will be displayed after the WCS is moved to the location of the new coordinate system.
Signature
SetCoordinateSystem(newCs)
Parameters: newCs ( NXOpen.CartesianCoordinateSystem
) – The new coordinate system for the WCSReturns: The old coordinate system for the WCS Return type: NXOpen.CartesianCoordinateSystem
New in version NX4.0.0.
License requirements: None.
SetCoordinateSystemCartesianAtCsys¶
-
WCS.
SetCoordinateSystemCartesianAtCsys
¶ Creates a WCS at a new coordinate system.
The return value is the old coordinate system of wcs.
Signature
SetCoordinateSystemCartesianAtCsys(newCs)
Parameters: newCs ( NXOpen.CartesianCoordinateSystem
) – New coordinate system location for the WCSReturns: The old coordinate system for the WCS Return type: NXOpen.CartesianCoordinateSystem
New in version NX7.5.0.
License requirements: None.
SetOriginAndMatrix¶
-
WCS.
SetOriginAndMatrix
¶ Sets the origin and orientation matrix of the WCS
Signature
SetOriginAndMatrix(origin, matrix)
Parameters: - origin (
NXOpen.Point3d
) – Origin relative to the absolute coordinate system - matrix (
NXOpen.Matrix3x3
) – Orientation relative to the absolute coordinate system. Must be orthonormal.
New in version NX3.0.0.
License requirements: None.
- origin (