SketchPatternInstanceControl Enumeration¶
NXOpen.SketchPattern.InstanceControl is an alias for NXOpen.SketchPatternInstanceControl
-
class
NXOpen.
SketchPatternInstanceControl
¶ Bases:
object
Represents the type of instance control for circular patterns
Enum Members
Enum Member Enum Member Description FullCircle The pattern instance control type is Full CircleNumberOffset The pattern instance control type is number + offset-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-