SketchAssocType Enumeration¶
NXOpen.Sketch.AssocType is an alias for NXOpen.SketchAssocType
-
class
NXOpen.
SketchAssocType
¶ Bases:
object
Used in
NXOpen.SketchDimensionGeometry_Struct
to indicate what type of geometry to useEnum Members
.
- . csv-table::
header: “Enum Member”, “Enum Member Description” “NotSet”, ” Use the entire geometric item, as opposed to a point ” “StartPoint”, ” Start point. E.g. the start point of a line ” “EndPoint”, ” End point. E.g. the start point of a line ” “ArcCenter”, ” Center of an arc, circle, or ellipse ” “Tangency”, ” Create the dimension tangent to the geometric item ” “CurvePoint”, ” A point on a spline ” “AnchorPoint”, ” The anchor of a conic ” “Midpoint”, ” The midpoint of a curve “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.