LightSceneType Enumeration¶
NXOpen.Light.SceneType is an alias for NXOpen.LightSceneType
-
class
NXOpen.
LightSceneType
¶ Bases:
object
The predefined scene lights used in Basic Lights.
These are subtypes of
LightType.Scene
. Except for ambient light, all of the other lights are on the same side of the model as the observer.Enum Members
- the observer’s location “
- “LeftBottom”, ” Light from the bottom left of the view ” “Bottom”, ” Light from the bottom center of the view ” “RightBottom”, ” Light from the bottom right of the view “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.