InferSnapTypeSnapType Enumeration¶
NXOpen.InferSnapType.SnapType is an alias for NXOpen.InferSnapTypeSnapType
-
class
NXOpen.
InferSnapTypeSnapType
¶ Bases:
object
Specify the snap point type
Enum Members
Enum Member Enum Member Description NotSet No Snap pointStart Snap point startEnd Snap point endMid Snap point midKnot Snap point knotCenter Snap point center of arcExist exsisting pointQuadrant Snap point quadrant of circleIntersection Snap point intersectionCurve Snap point on curveSurf Snap point on surfaceOrigin Snap originDrfAid Snap point drafting aidDrfTangent Snap point drafting tangentPole Snap point at poleDefining Snap point at definingConicAnchor Snap point at conic anchorBoundedGrid Snap point on bounded gridFacetVertex Snap point on facet vertex-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-