ExpressionUnitsOption Enumeration¶
NXOpen.Expression.UnitsOption is an alias for NXOpen.ExpressionUnitsOption
-
class
NXOpen.
ExpressionUnitsOption
¶ Bases:
object
Indicates the units to use when getting an expression’s value.
Enum Members
Enum Member Enum Member Description Base Return expression value in base part units.Expression Return expression value in expression units.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-