ModelingViewSectionPlane Enumeration¶
NXOpen.ModelingView.SectionPlane is an alias for NXOpen.ModelingViewSectionPlane
-
class
NXOpen.
ModelingViewSectionPlane
¶ Bases:
object
This arbitrarily defines an initaial reference point.
If the ‘primary’ plane, which is farther from WCS, or the ‘secondary’ plane, which is closer to WCS, should be the active sectioning (cutting) plane .. deprecated:: NX5.0.0
This funcitonality is replaced byNXOpen.ModelingView.ActiveDynamicSection()
Enum Members
Enum Member Enum Member Description Primary PrimarySecondary Secondary-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-