MeasureFaces Class¶
-
class
NXOpen.
MeasureFaces
¶ Bases:
NXOpen.GenericMeasure
Represents the measurement of perimeter and area of a set of faces
To create or edit an instance of this class, use
NXOpen.MeasureFaceBuilder
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Accuracy | Returns the accuracy value for calculations of the measurement |
Area | Returns the value for area of the measurement |
MeasurementType | Returns the type of the measurement |
Perimeter | Returns the value for perimeter of the measurement |
Methods¶
Method | Description |
---|---|
CreateEmbedded | Creates and returns an embedded measurement expression. |
CreateEmbeddedObject | Creates an embedded measurement. |
CreateFeature | Creates and returns a measurement feature @return |
Dispose | Free resources associated with the measure. |
Information | Display information about a measurement. |
Enumerations¶
MeasureFacesActiveValue Enumeration | Indicates the type of embedded measurement to create |
Property Detail¶
Accuracy¶
-
MeasureFaces.
Accuracy
¶ Returns the accuracy value for calculations of the measurement
-------------------------------------
Getter Method
Signature
Accuracy()
Returns: Return type: float New in version NX4.0.0.
License requirements: None.
Method Detail¶
CreateEmbedded¶
-
MeasureFaces.
CreateEmbedded
¶ Creates and returns an embedded measurement expression.
Deprecated: Use CreateEmbeddedObject instead
Signature
CreateEmbedded(measurementType)
Parameters: measurementType ( NXOpen.MeasureFacesActiveValue
) –Returns: Return type: str New in version NX4.0.0.
Deprecated since version NX5.0.1: Use
MeasureFaces.CreateEmbeddedObject()
instead.License requirements: solid_modeling (“SOLIDS MODELING”)
CreateEmbeddedObject¶
-
MeasureFaces.
CreateEmbeddedObject
¶ Creates an embedded measurement.
The name of the measurement can be used in an expression formula.
Signature
CreateEmbeddedObject(measurementType)
Parameters: measurementType ( NXOpen.MeasureFacesActiveValue
) –Returns: a tuple Return type: A tuple consisting of (measurement, name). measurement is a NXOpen.Scalar
. the measurement name is a str. the name of the measurementNew in version NX5.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
CreateFeature¶
-
MeasureFaces.
CreateFeature
¶ Creates and returns a measurement feature
Signature
CreateFeature()
Returns: Return type: NXOpen.Measure
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)