HumanDataInverseKinematicsInitJoint Enumeration¶
NXOpen.HumanData.InverseKinematicsInitJoint is an alias for NXOpen.HumanDataInverseKinematicsInitJoint
-
class
NXOpen.
HumanDataInverseKinematicsInitJoint
¶ Bases:
object
This enum represents the motion initiation joint of hand dynamic drag
Enum Members
- without changing the upper body position. “
- “Waist”, ” Indicate starting arm motion at the waist and using the
entire upper body “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.