ValidationTabnotSectionValidator Class¶
-
class
NXOpen.
ValidationTabnotSectionValidator
¶ Bases:
NXOpen.ValidationAnnotationValidator
validator for a Tabnot Section
This is a test class.
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
ValidatorPrintLevel | Returns or sets the print level for validation. |
ValidatorVersion | Returns or sets the algorithm to use for validation. |
Methods¶
Method | Description |
---|---|
Destroy | Deletes the validator. |
SetValidatorPrintOodStatus | Set the ood status of features. |
Property Detail¶
ValidatorPrintLevel¶
-
ValidationTabnotSectionValidator.
ValidatorPrintLevel
¶ Returns or sets the print level for validation.
-------------------------------------
Getter Method
Signature
ValidatorPrintLevel()
Returns: Return type: NXOpen.ValidatorPrintLevel
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValidatorPrintLevel(level)
Parameters: level ( NXOpen.ValidatorPrintLevel
) –New in version NX7.5.0.
License requirements: None.
ValidatorVersion¶
-
ValidationTabnotSectionValidator.
ValidatorVersion
¶ Returns or sets the algorithm to use for validation.
-------------------------------------
Getter Method
Signature
ValidatorVersion()
Returns: Return type: NXOpen.ValidatorVersion
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValidatorVersion(version)
Parameters: version ( NXOpen.ValidatorVersion
) –New in version NX7.5.0.
License requirements: None.