SketchDeleteThirdCurveOption Enumeration¶
NXOpen.Sketch.DeleteThirdCurveOption is an alias for NXOpen.SketchDeleteThirdCurveOption
-
class
NXOpen.
SketchDeleteThirdCurveOption
¶ Bases:
object
Indicates whether the 3rd curve should be deleted when doing a 3 curve fillet
Enum Members
Enum Member Enum Member Description False Do not delete the 3rd curveTrue Delete the 3rd curve-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-