ModelingViewCollection Class¶
-
class
NXOpen.
ModelingViewCollection
¶ Bases:
object
Represents a collection of :py:class:`ModelingView`s.
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
ExpandCollapseModelViewNode | Expand or collapse the Model View node in the Part Navigator. |
FindObject | Finds the ModelingView with the given identifier as recorded in a journal. |
Property Detail¶
WorkView¶
-
ModelingViewCollection.
WorkView
¶ Returns the work view of the part.
-------------------------------------
Getter Method
Signature
WorkView()
Returns: Work view Return type: NXOpen.ModelingView
New in version NX4.0.0.
License requirements: None.
Method Detail¶
ExpandCollapseModelViewNode¶
-
ModelingViewCollection.
ExpandCollapseModelViewNode
¶ Expand or collapse the Model View node in the Part Navigator.
Signature
ExpandCollapseModelViewNode(expand)
Parameters: expand (bool) – New in version NX9.0.3.
License requirements: None.
FindObject¶
-
ModelingViewCollection.
FindObject
¶ Finds the
ModelingView
with the given identifier as recorded in a journal. An object may not return the same value as its JournalIdentifier in different versions of the software. However, newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the modeling view to be found Returns: View with this identifier Return type: NXOpen.ModelingView
New in version NX4.0.0.
License requirements: None.