LoadOptionsParent Enumeration¶
NXOpen.LoadOptions.Parent is an alias for NXOpen.LoadOptionsParent
-
class
NXOpen.
LoadOptionsParent
¶ Bases:
object
Options to allow you to specify how unloaded parents should be loaded when interpart data loading is turned on
New in version NX3.0.0.
Enum Members
- but fully load partially loaded parts with parent geometry. “
- “Immediate”, ” Fully load parts that satisfy one level of parent
references as well as any partially loaded parts with parent geometry. “
“All”, ” Recursively fully load all parts with parent geometry linkedto geometry in the parts selected for loading “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.