LoadOptionsBookmarkComponents Enumeration¶
NXOpen.LoadOptions.BookmarkComponents is an alias for NXOpen.LoadOptionsBookmarkComponents
-
class
NXOpen.
LoadOptionsBookmarkComponents
¶ Bases:
object
The options to specify what components to load and visualize when loading bookmarks.
**Note:</b> The visiblity and fully loaded state will only be restored for components that are part of the bookmark’s product assembly. The bookmark’s product assembly is the one that was the displayed part at the time the bookmark was saved.
New in version NX6.0.0.
Enum Members
- Don’t load invisible components. “
- “LoadLoaded”, ” Load and show only what was loaded on the bookmark’s save
- Load invisible components and keep them invisible. “
- “LoadLoadedAndNonDisplayed”, ” Load and show only what was loaded on the bookmark’s save, including non-display parts.
Load invisible components and keep them invisible. All non-display parts are invisible. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.