NXOpen.CAE.AbstractionManager |
Provides method for creating builder for |
NXOpen.CAE.AdaptivityExclusionZone |
Represents a NXOpen.CAE.AdaptivityExclusionZone . |
NXOpen.CAE.AdaptivityExclusionZoneBuilder |
Builds a NXOpen.CAE.AdaptivityExclusionZone object which represets adaptivity meta solution related exclusion zones. |
NXOpen.CAE.AdaptivityExclusionZoneCollection |
Represents a collection of correl meta solution. |
NXOpen.CAE.AdaptivityMetaSolution |
Represents a NXOpen.CAE.AdaptivityMetaSolution . |
NXOpen.CAE.AdaptivityMetaSolutionBuilder |
Builds a NXOpen.CAE.AdaptivityMetaSolution object which represets a recipe for generating adaptive remesh. |
NXOpen.CAE.AdaptivityMetaSolutionCollection |
Represents a collection of adaptivity meta solution. |
NXOpen.CAE.AdjacentFaceMethod |
Represents the output from the adjacent face smart selector method |
NXOpen.CAE.AfuAbscissaHeaderInfo |
Represents the data to define abscissa header information for an afu record |
NXOpen.CAE.AfuData |
the data used to create an AFU Data Record |
NXOpen.CAE.AfuDataConvertor |
Convert data values for the AFU Data Record |
NXOpen.CAE.AfuHeaderId |
the data used to create header id information for an AFU Data Record |
NXOpen.CAE.AfuManager |
AFU File and Data Record Manager |
NXOpen.CAE.AfuMathOperation |
Does math operations on the AFU Data Records |
NXOpen.CAE.AfuOrdinateHeaderInfo |
Represents the ordinate header information for an afu record |
NXOpen.CAE.AfuZHeaderInfo |
Represents the Z axis header information for an afu record |
NXOpen.CAE.AssignNodalCSBuilder |
Represents a NXOpen.CAE.AssignNodalCSBuilder |
NXOpen.CAE.AssyFEModel |
This class represents an Assembly Finite Element Model. |
NXOpen.CAE.AssyFemPart |
Represents an NX part of type .afm. |
NXOpen.CAE.AutoBCBuilder |
Builds one or more NXOpen.CAE.SimSimulationObject object(s). |
NXOpen.CAE.AutoMacViewerBuilder |
Represents the correlation pairing viewer builder |
NXOpen.CAE.AutoPairs |
Represents an autopairs obj |
NXOpen.CAE.AutoPairsBuilder |
Builds a NXOpen.CAE.AutoPairs object which represets a recipe for generating face pairs from a selected set of faces or solids in the model whose distance is less than a specified tolerance. |
NXOpen.CAE.AutomaticMorphBuilder |
Represents a NXOpen.CAE.AutomaticMorphBuilder |
NXOpen.CAE.AutomaticSweepBetweenSelection |
Builder for creating Manual Hex Mesh - Face Dependency type - Multi Face Automatic |
NXOpen.CAE.BCSelectionDisplayBuilder |
This class provides BC Selection Visual Display support, use this class to get the |
NXOpen.CAE.BaseFEModel |
This class represents an Assembly Finite Element Model. |
NXOpen.CAE.BaseFemPart |
Represents an NX part of type .afm. |
NXOpen.CAE.BaseIteration |
This class provides interfaces to query iteration attributes |
NXOpen.CAE.BaseLoadcase |
This class provides interfaces to query loadcase attributes |
NXOpen.CAE.BaseResultType |
This class provides interfaces to query result type attributes |
NXOpen.CAE.BeamEADBuilder |
This class provides Beam/Bar Associated Data Support |
NXOpen.CAE.BeamSection |
Represents a Beam Cross Section |
NXOpen.CAE.BeamSectionCollection |
Represents the collection of all NXOpen.CAE.BeamSection in a fem part |
NXOpen.CAE.BeamSectionOffsetOptions |
To create a new instance of this class, use NXOpen.CAE.CaePart.NewBeamSectionOffsetOptions |
NXOpen.CAE.BeamSectionOptions |
Represents the synchronize options to be used when a FEM part is created |
NXOpen.CAE.BeamSectionOrientationOptions |
To create a new instance of this class, use NXOpen.CAE.CaePart.NewBeamSectionOrientationOptions |
NXOpen.CAE.Bolt |
Represents Bolt |
NXOpen.CAE.BoltBuilder |
Represents a NXOpen.CAE.BoltBuilder |
NXOpen.CAE.BoltCollection |
Provides method for creating builder for |
NXOpen.CAE.BushingEADBuilder |
This class provides Bushing Associated Data Support |
NXOpen.CAE.CADModeling |
The CADModeling class provides method to create |
NXOpen.CAE.CAEBody |
Represents a CAE body geometry |
NXOpen.CAE.CAEConnection |
Represents Connection Recipe |
NXOpen.CAE.CAEConnectionBuilder |
Builder for creating Connection Recipes |
NXOpen.CAE.CAEConnectionCollection |
Provides method for creating builder for |
NXOpen.CAE.CAEEdge |
Represents a CAE edge geometry |
NXOpen.CAE.CAEFace |
Represents a CAE face geometry |
NXOpen.CAE.CAESet |
Represents a group of CAE object sets. |
NXOpen.CAE.CAEVertex |
Represents a CAE vertex geometry |
NXOpen.CAE.CAEWeldConnection |
Represents WeldConnection Recipe |
NXOpen.CAE.CAEWeldConnectionBuilder |
Builder for creating 1D Weld Connection |
NXOpen.CAE.CaeDOFSet |
Represents a dofset class NXOpen.CAE.CaeDOFSet . |
NXOpen.CAE.CaeDOFSetCollection |
Provides methods for managing DOFSet NXOpen.CAE.CaeDOFSet |
NXOpen.CAE.CaeDOFSetDisplay |
Represents a DOF Set display attributes |
NXOpen.CAE.CaeDataContainer |
Represents a list of named properties, where the property name is a unique string. |
NXOpen.CAE.CaeGroup |
Represents a group class NXOpen.CAE.CaeGroup . |
NXOpen.CAE.CaeGroupCollection |
Provides methods for managing set NXOpen.CAE.CaeGroup |
NXOpen.CAE.CaePart |
This is an abstract class for NX parts of type .fem and .sim |
NXOpen.CAE.CaeRegion |
Represents a cae region object |
NXOpen.CAE.CaeRegionBuilder |
Represents a NXOpen.CAE.CaeRegionBuilder builder |
NXOpen.CAE.CaeRegionCollection |
Provides methods for managing CAE.CaeRegion in a sim part |
NXOpen.CAE.CaeSession |
This class provides access to all session related CAE functionality |
NXOpen.CAE.CfdContactPreventionConstraint |
The contact prevention constraint is a type of constraint which is used by the Fluid Domain Recipe to generate a fluid domain. |
NXOpen.CAE.CfdContactPreventionConstraintBuilder |
Represents a NXOpen.CAE.CfdContactPreventionConstraint builder |
NXOpen.CAE.CfdContactPreventionConstraintCollection |
Provides methods for managing Contact Prevention Constraints:py:class:CAE.CfdContactPreventionConstraint in a fem part |
NXOpen.CAE.CfdLocalResolutionConstraint |
The local resolution constraint is a type of constraint which is used by the Fluid Domain Recipe to generate a fluid domain. |
NXOpen.CAE.CfdLocalResolutionConstraintBuilder |
Represents a NXOpen.CAE.CfdLocalResolutionConstraint builder |
NXOpen.CAE.CfdLocalResolutionConstraintCollection |
Provides methods for managing Local Resolution Constraints:py:class:CAE.CfdLocalResolutionConstraint in a fem part |
NXOpen.CAE.CircularEdgeMethod |
Represents the output from the circular edge smart selector method |
NXOpen.CAE.CircularImprintBuilder |
Builder for creating Circular Imprint |
NXOpen.CAE.ClippingParameters |
This class is worked as a packet of information that can be used to set the clipping parameters of a NXOpen.CAE.Post object. |
NXOpen.CAE.ComacViewerBuilder |
Represents the correlation MAC matrix viewer builder |
NXOpen.CAE.CombineTrisBuilder |
Builder for creating Combine Tris |
NXOpen.CAE.CompanionResult |
Represents additional results data that will augment a primary set of Analysis results associated to a NXOpen.CAE.SimSolution . |
NXOpen.CAE.CompanionResultBuilder |
Represents a NXOpen.CAE.CompanionResult builder and can |
NXOpen.CAE.CompanionResultCollection |
Provides methods for managing CompanionResults NXOpen.CAE.CompanionResult |
NXOpen.CAE.ConflictResolutionBuilder |
Represents a NXOpen.CAE.ConflictResolutionBuilder builder which can resolve conflicts between the two input BCs by a specified rule |
NXOpen.CAE.ConstraintResolutionBuilder |
Represents a NXOpen.CAE.ConstraintResolutionBuilder builder which can resolve conflicts between the two input constraints by a specified rule |
NXOpen.CAE.ContactMeshBuilder |
Represents a NXOpen.CAE.ContactMeshBuilder |
NXOpen.CAE.CorrelAlignmentBuilder |
This builder is used to control the alignment parameters of a NXOpen.CAE.CorrelSolution |
NXOpen.CAE.CorrelApplyAlignmentFromBuilder |
This builder is used to apply the alignment matrix read from selected xml file to the test model |
NXOpen.CAE.CorrelBaseBuilder |
Represents the abstract builder class for all objects defined in correl meta solution |
NXOpen.CAE.CorrelFineTuneAlignmentBuilder |
This builder is used to nudge the alignment by a fine adjustment |
NXOpen.CAE.CorrelManager |
Represents the correl manager that contains all correl and pre-test objects |
NXOpen.CAE.CorrelModePairingBuilder |
This builder is used to control the mode pairing behavior of a NXOpen.CAE.CorrelSolution |
NXOpen.CAE.CorrelSolution |
Represents a NXOpen.CAE.CorrelSolution , which is a meta-solution used to compare results from two structural dynamics solutions |
NXOpen.CAE.CorrelSolutionBuilder |
This is a manager to the CAE.CorrelSolution class. |
NXOpen.CAE.CorrelSolutionCollection |
Represents a collection of correl meta solution |
NXOpen.CAE.CreateJtBuilder |
Represents a NXOpen.CAE.CreateJtBuilder |
NXOpen.CAE.CrossSectionParameters |
This class is worked as a packet of information that can be used to change cross-section state. |
NXOpen.CAE.CylinderFaceMethod |
Represents the output from the cylinder face smart selector method |
NXOpen.CAE.DeformationParameters |
This class is worked as a packet of information that can be be used to deform NXOpen.CAE.Post objects. |
NXOpen.CAE.DeletePolygonFaceBuilder |
Builder for Delete Polygon Face |
NXOpen.CAE.DependentMesh |
Represents Mesh Recipe |
NXOpen.CAE.DependentMeshBuilder |
Represents a NXOpen.CAE.Mesh2d |
NXOpen.CAE.DependentMeshListItemBuilder |
Represents a NXOpen.CAE.DependentMeshListItemBuilder |
NXOpen.CAE.DependentMeshListItemBuilderList |
Represents a list of objects. |
NXOpen.CAE.DestinationCollectorBuilder |
Represents a Element Collector Container (Ecc) selection |
NXOpen.CAE.DurabilityAxisSearch |
Represents a NXOpen.CAE.DurabilityAxisSearch . |
NXOpen.CAE.DurabilityAxisSearchCollection |
Represents a collection of stress axes. |
NXOpen.CAE.DurabilityDamageEvaluationBuilder |
Represents the builder for evaluating durability damage. |
NXOpen.CAE.DurabilityDataControlBuilder |
Represents a builder class for the transient event data control. |
NXOpen.CAE.DurabilityEvaluateFatigueHistoryBuilder |
Represents the builder for evaluating fatigue histories. |
NXOpen.CAE.DurabilityEvent |
Represents a NXOpen.CAE.DurabilityEvent , which is an event of a durability solution process. |
NXOpen.CAE.DurabilityEventBuilder |
Represents the abstract builder class for all durability events. |
NXOpen.CAE.DurabilityEventCollection |
Represents a collection of durability events. |
NXOpen.CAE.DurabilityEventFatigueSettingsBuilder |
Represents a builder class for the event fatigue settings. |
NXOpen.CAE.DurabilityEventOverridesBuilder |
Represents a builder class for Event Overrides. |
NXOpen.CAE.DurabilityEventSolverBuilder |
Represents the builder for solving the durability event. |
NXOpen.CAE.DurabilityEventStrengthSettingsBuilder |
Represents a builder class for the event strength settings. |
NXOpen.CAE.DurabilityExcitation |
Represents a NXOpen.CAE.DurabilityExcitation . |
NXOpen.CAE.DurabilityExcitationBuilder |
Represents the abstract builder class for all durability excitations. |
NXOpen.CAE.DurabilityExcitationCollection |
Represents a collection of durability excitations. |
NXOpen.CAE.DurabilityFatigue |
Represents a NXOpen.CAE.DurabilityFatigue . |
NXOpen.CAE.DurabilityFatigueCollection |
Represents a collection of event fatigue settings. |
NXOpen.CAE.DurabilityFunctionExcitation |
Represents a NXOpen.CAE.DurabilityFunctionExcitation . |
NXOpen.CAE.DurabilityFunctionExcitationBuilder |
Represents a NXOpen.CAE.DurabilityFunctionExcitation builder. |
NXOpen.CAE.DurabilityLoadPattern |
Represents a NXOpen.CAE.DurabilityLoadPattern . |
NXOpen.CAE.DurabilityLoadPatternBuilder |
Represents a CAE.DurabilityLoadPattern builder. |
NXOpen.CAE.DurabilityManager |
Represents the durability manager that contains all durability objects. |
NXOpen.CAE.DurabilityMetaSolution |
Represents a NXOpen.CAE.DurabilityMetaSolution . |
NXOpen.CAE.DurabilityMetaSolutionBuilder |
Represents a NXOpen.CAE.DurabilityMetaSolution builder. |
NXOpen.CAE.DurabilityMetaSolutionCollection |
Represents a collection of correl meta solution. |
NXOpen.CAE.DurabilityRandomEvent |
Represents a NXOpen.CAE.DurabilityRandomEvent . |
NXOpen.CAE.DurabilityRandomEventBuilder |
Represents the builder for the random durability event. |
NXOpen.CAE.DurabilityRandomFatigue |
Represents a NXOpen.CAE.DurabilityRandomFatigue . |
NXOpen.CAE.DurabilityRandomFatigueBuilder |
Represents a builder class for the event fatigue settings. |
NXOpen.CAE.DurabilityRandomFatigueCollection |
Represents a collection of random fatigue. |
NXOpen.CAE.DurabilityResultPath |
Represents a NXOpen.CAE.DurabilityResultPath . |
NXOpen.CAE.DurabilityResultPathBuilder |
Represents a NXOpen.CAE.DurabilityResultPath builder. |
NXOpen.CAE.DurabilityResultsReportBuilder |
Represents the builder for reporting the durability results. |
NXOpen.CAE.DurabilitySolveOptions |
Represents a NXOpen.CAE.DurabilitySolveOptions . |
NXOpen.CAE.DurabilitySolveOptionsCollection |
Represents a collection of correl meta solution. |
NXOpen.CAE.DurabilitySolverBuilder |
Represents the builder for solving the durability solution process. |
NXOpen.CAE.DurabilityStaticEvent |
Represents a NXOpen.CAE.DurabilityStaticEvent . |
NXOpen.CAE.DurabilityStaticEventBuilder |
Represents the builder for the static durability event. |
NXOpen.CAE.DurabilityStrainGageAnalyzerBuilder |
Represents the builder for analyzing strain gage data. |
NXOpen.CAE.DurabilityStrength |
Represents a NXOpen.CAE.DurabilityStrength . |
NXOpen.CAE.DurabilityStrengthCollection |
Represents a collection of event strength settings. |
NXOpen.CAE.DurabilityStressAxesBuilder |
Represents a builder class for the event fatigue settings. |
NXOpen.CAE.DurabilityTransientEvent |
Represents a NXOpen.CAE.DurabilityTransientEvent . |
NXOpen.CAE.DurabilityTransientEventBuilder |
Represents the builder for the transient durability event. |
NXOpen.CAE.EdgeDensity |
Represents a CAE edge density |
NXOpen.CAE.EdgePathMethod |
Represents a NXOpen.CAE.EdgePathMethod . |
NXOpen.CAE.EdgeSticherBuilder |
Represents a NXOpen.CAE.EdgeSticherBuilder |
NXOpen.CAE.ElemEdgePathMethod |
Represents a NXOpen.CAE.ElemEdgePathMethod . |
NXOpen.CAE.ElementConnectivityBuilder |
Represents a NXOpen.CAE.ElementConnectivityBuilder |
NXOpen.CAE.ElementCreateBuilder |
Represents a NXOpen.CAE.ElementCreateBuilder which allows you to manually create elements from existing nodes. |
NXOpen.CAE.ElementDeleteBuilder |
Represents a NXOpen.CAE.ElementDeleteBuilder |
NXOpen.CAE.ElementExtractBuilder |
Builder for creating Element Extract |
NXOpen.CAE.ElementExtrudeBuilder |
Represents a NXOpen.CAE.ElementExtrudeBuilder |
NXOpen.CAE.ElementModifyLabelBuilder |
Represents a NXOpen.CAE.ElementModifyLabelBuilder |
NXOpen.CAE.ElementModifyOrderBuilder |
Represents a NXOpen.CAE.ElementModifyOrderBuilder |
NXOpen.CAE.ElementModifyTypeBuilder |
Represents a NXOpen.CAE.ElementModifyTypeBuilder |
NXOpen.CAE.ElementProjectBuilder |
Represents a NXOpen.CAE.ElementProjectBuilder |
NXOpen.CAE.ElementReflectBuilder |
Represents a NXOpen.CAE.ElementReflectBuilder |
NXOpen.CAE.ElementRevolveBuilder |
Represents a NXOpen.CAE.ElementRevolveBuilder |
NXOpen.CAE.ElementSplitBuilder |
Represents a NXOpen.CAE.ElementSplitBuilder |
NXOpen.CAE.ElementTranslateBuilder |
Represents a NXOpen.CAE.ElementTranslateBuilder |
NXOpen.CAE.ElementTypeBuilder |
Represents the specification of the FEA Element Type for a meshing dialog. |
NXOpen.CAE.ElementTypes |
Represents an NXOpen.CAE.ElementTypes class. |
NXOpen.CAE.FEElemEdge |
Represents a Finite Element Edge. |
NXOpen.CAE.FEElemFace |
Represents a Finite Element Face. |
NXOpen.CAE.FEElement |
Represents a Finite Element. |
NXOpen.CAE.FEElementLabelMap |
Represents a Elementl Label to an CAE.FEElement map, it can be used to quickly convert |
NXOpen.CAE.FEModel |
This class represents a Finite Element Model. |
NXOpen.CAE.FEModelOccAttribute |
This class represents an Interface to the Finite Element Model Attributes. |
NXOpen.CAE.FEModelOccurrence |
This class represents a Finite Element Model Occurrence. |
NXOpen.CAE.FENode |
Represents a Finite Element Node. |
NXOpen.CAE.FENodeLabelMap |
Represents a Nodel Label to an CAE.FENode map, it can be used to quickly convert |
NXOpen.CAE.FaceDensity |
Represents a CAE face density |
NXOpen.CAE.FaceFromBoundaryBuilder |
Builder for creating Polygon Face by boundary |
NXOpen.CAE.FacetProximityBuilder |
Represents a CAE.FacetProximityBuilder builder |
NXOpen.CAE.FeatureEdgeNodeMethod |
Represents the output from the feature edge node smart selector method |
NXOpen.CAE.FeatureElemEdgeMethod |
Represents the output from the feature element edge smart selector method |
NXOpen.CAE.FeatureElemFaceMethod |
Represents the output from the feature element face smart selector method |
NXOpen.CAE.FeatureElemMethod |
Represents the output from the feature element smart selector method |
NXOpen.CAE.FeatureNodeMethod |
Represents the output from the feature node smart selector method |
NXOpen.CAE.FeatureShellElemMethod |
Represents the output from the feature shell element smart selector method |
NXOpen.CAE.FemPart |
Represents an NX part of type .fem. |
NXOpen.CAE.FemSynchronizeOptions |
Represents the synchronize options to be used when a FEM part is created |
NXOpen.CAE.FilletFaceMethod |
Represents the output from the fillet face smart selector method |
NXOpen.CAE.FlatPatternsBuilder |
Represents a Flat Patterns Builder. |
NXOpen.CAE.FluidDomainBuilder |
Represents a NXOpen.CAE.FluidDomainRecipe |
NXOpen.CAE.FluidDomainCollection |
Provides methods for managing fluid domains:py:class:NXOpen.CAE.FluidDomainRecipe in a fem part |
NXOpen.CAE.FluidDomainRecipe |
Represents a FluidDomainRecipe |
NXOpen.CAE.FreeBodyResultsBuilder |
Represents a NXOpen.CAE.FreeBodyResultsBuilder |
NXOpen.CAE.FreezeGeometryBuilder |
Builder for creating Freeze Geometry |
NXOpen.CAE.FreezeGeometryRecipe |
Represents FreezeGeometryRecipe |
NXOpen.CAE.Function |
Represents a function object |
NXOpen.CAE.FunctionBuilder |
This builder class is used to create or edit NXOpen.CAE.Function objects. |
NXOpen.CAE.FunctionCollection |
Represents a collection of function objects |
NXOpen.CAE.GRMSearch |
Contains methods for searching Teamcenter for CAE objects, as well as a cache of already found items. |
NXOpen.CAE.GapEADBuilder |
This class provides Gap Associated Data Support |
NXOpen.CAE.GeneralGeometryBeamSection |
Represents a General Geometry Beam Cross Section |
NXOpen.CAE.GeneralGeometryBeamSectionBuilder |
Represents a NXOpen.CAE.GeneralGeometryBeamSectionBuilder |
NXOpen.CAE.GeometryRecipe |
Represents a Geometry Recipe |
NXOpen.CAE.GeometryRecipeCollection |
Provides methods for managing set NXOpen.CAE.GeometryRecipe |
NXOpen.CAE.GlobalLayupImportFromPptBuilder |
Represents a Global Layup IMport From Ppt Builder. |
NXOpen.CAE.GroupElemMethod |
Represents the output from the Group Element smart selector method |
NXOpen.CAE.GroupElemMethodElemOption |
Represents the output from the Group Element smart selector method |
NXOpen.CAE.GroupFaceMethod |
Represents the output from the Group Face smart selector method |
NXOpen.CAE.GroupMethod |
Represents the output from the Group smart selector method |
NXOpen.CAE.GroupNodeMethod |
Represents the output from the Group Node smart selector method |
NXOpen.CAE.IBeamSectionBuilder |
Represents a NXOpen.CAE.IBeamSectionBuilder |
NXOpen.CAE.IExportableFEEntity |
Represents an EXPORTABLE_FE_ENTITY. |
NXOpen.CAE.IFEModel |
This class represents an Interface to the Finite Element Model. |
NXOpen.CAE.IFolder |
This class represents an Interface to the Folder. |
NXOpen.CAE.IHierarchicalFEModel |
This class represents an Interface to the Finite Element Model. |
NXOpen.CAE.IMeshCollector |
Represents the base IMeshCollector class for MeshCollector and |
NXOpen.CAE.IMeshManager |
Manages meshes:py:class:NXOpen.CAE.IMeshManager in cae parts |
NXOpen.CAE.ImportedResult |
Represents analysis results for a imported solver results file. |
NXOpen.CAE.Iteration |
Represents iteration present in a NXOpen.CAE.Loadcase . |
NXOpen.CAE.Laminate |
Represents a Laminate, which is a specialized kind of NXOpen.CAE.PhysicalPropertyTable |
NXOpen.CAE.LaminateDampingFactorBuilder |
The builder for the damping factor. |
NXOpen.CAE.LaminateDrapingData |
Encapsulate the ply information related to the draping algorithm |
NXOpen.CAE.LaminateDrapingDataBuilder |
Represents a NXOpen.CAE.LaminateDrapingData builder |
NXOpen.CAE.LaminateDrapingExtension |
Encapsulate the ply information related to a ply draping extension |
NXOpen.CAE.LaminateDrapingExtensionBuilder |
Builder class for NXOpen.CAE.LaminateDrapingExtension |
NXOpen.CAE.LaminateDrapingOrientation |
Encapsulates the ply draping results |
NXOpen.CAE.LaminateDynamicEvent |
The Laminate Dynamic Event. |
NXOpen.CAE.LaminateDynamicEventBuilder |
Represents a NXOpen.CAE.LaminateDynamicEvent builder |
NXOpen.CAE.LaminateDynamicEventCollection |
Represents a collection of laminate dynamic events |
NXOpen.CAE.LaminateDynamicSim |
The Laminate Dynamic Simulation builder is the journalling interface to build the LaminateDyanmicSim object. |
NXOpen.CAE.LaminateDynamicSimBuilder |
Represents a NXOpen.CAE.LaminateDynamicSim builder |
NXOpen.CAE.LaminateDynamicSimCollection |
Represents a collection of laminate dynamic sims |
NXOpen.CAE.LaminateElementFilterBuilder |
Represents a NXOpen.CAE.LaminateGraphicalReport builder |
NXOpen.CAE.LaminateExtrudeSetup |
Extrude Setup |
NXOpen.CAE.LaminateExtrudeSetupBuilder |
Represents a NXOpen.CAE.LaminateExtrudeSetup builder |
NXOpen.CAE.LaminateExtrudeSetupCollection |
Represents a collection of laminate extrusion setups |
NXOpen.CAE.LaminateFiberOrientationOptions |
Laminate Fiber Orientation Options |
NXOpen.CAE.LaminateFiberOrientationOptionsBuilder |
Represents a NXOpen.CAE.LaminateFiberOrientationOptions builder |
NXOpen.CAE.LaminateFillSetupBuilder |
Represents a NXOpen.CAE.LaminateFillSetupBuilder builder |
NXOpen.CAE.LaminateGlobalLayup |
Represent a global layup in the ply based modeling. |
NXOpen.CAE.LaminateGlobalLayupCollection |
Represents a global layup, which is defined by a sequence of NXOpen.CAE.LaminateGlobalLayup , each with a name and a list of plies |
NXOpen.CAE.LaminateGlobalLayupMgr |
Represent the laminate global layup manager which manages all the global layups in the laminate ply-based modeling project |
NXOpen.CAE.LaminateGlobalLayupPlyGroupCollection |
Represents a laminate layup in the global layup context (ply based modeling), which is defined by a sequence of NXOpen.CAE.LaminatePlyGroup , each with a name and a list of plies. |
NXOpen.CAE.LaminateGraphicalReport |
Represents a laminate graphical report |
NXOpen.CAE.LaminateGraphicalReportBuilder |
Represents a CAE.LaminateGraphicalReport builder |
NXOpen.CAE.LaminateGraphicalReportCollection |
Represents a collection of CAE.LaminateGraphicalReport |
NXOpen.CAE.LaminateImportZonesBuilder |
Represents a NXOpen.CAE.LaminateImportZonesBuilder builder |
NXOpen.CAE.LaminateImportedLayupBuilder |
Represents a NXOpen.CAE.LaminateImportedLayupBuilder builder |
NXOpen.CAE.LaminateLayupOffset |
laminate layup offset |
NXOpen.CAE.LaminateLayupOffsetBuilder |
Represents a NXOpen.CAE.LaminateLayupOffset builder |
NXOpen.CAE.LaminateLayupOffsetCollection |
Represents a collection of layup offset rules |
NXOpen.CAE.LaminateLockAngleBuilder |
Represents a builder |
NXOpen.CAE.LaminateManager |
Represents the laminate manager that contains all laminate post report setups |
NXOpen.CAE.LaminateMatOrientation |
Laminate Material Orientation |
NXOpen.CAE.LaminateMatOrientationBuilder |
Represents a NXOpen.CAE.LaminateMatOrientation builder |
NXOpen.CAE.LaminateMatOrientationCollection |
Represents a collection of layup growth rules |
NXOpen.CAE.LaminateModeProperty |
Represents the properties of one normal mode |
NXOpen.CAE.LaminateModePropertyCollection |
Represents a collection of laminate mode properties |
NXOpen.CAE.LaminatePly |
Represents one ply in a laminate layup |
NXOpen.CAE.LaminatePlyCollection |
Represents a list of plies, which have a material, a thickness, an orientation, and a color |
NXOpen.CAE.LaminatePlyFilterBuilder |
Represents a NXOpen.CAE.LaminatePlyFilterBuilder |
NXOpen.CAE.LaminatePlyGroup |
Represents one ply group in a laminate layup |
NXOpen.CAE.LaminatePlyGroupCollection |
Represents a laminate layup, which is defined by a sequence of CAE.LaminatePlyGroup , each with a name and a list of plies |
NXOpen.CAE.LaminatePlyMaxThicknessVarBuilder |
Builder used to modify the ply maximum accepted thickness variation for laminate fill |
NXOpen.CAE.LaminatePostReport |
Represents an advanced post reporting setup for laminate results. |
NXOpen.CAE.LaminatePostReportBuilder |
Represents a NXOpen.CAE.LaminatePostReport builder |
NXOpen.CAE.LaminatePostReportCollection |
Represents a collection of laminate post reports |
NXOpen.CAE.LaminateQuickReport |
Represents a laminate quick report |
NXOpen.CAE.LaminateQuickReportBuilder |
Represents a NXOpen.CAE.LaminateQuickReport builder |
NXOpen.CAE.LaminateQuickReportCollection |
Represents a collection of CAE.LaminateQuickReport |
NXOpen.CAE.LaminateRandomEvent |
The Laminate Dynamic Event. |
NXOpen.CAE.LaminateRandomEventBuilder |
Represents a NXOpen.CAE.LaminateRandomEvent builder |
NXOpen.CAE.LaminateRelabelPliesBuilder |
Represents a CAE.LaminateDynamicEvent builder |
NXOpen.CAE.LaminateSelectEntitiesBuilder |
Represents a NXOpen.CAE.LaminateSelectEntitiesBuilder |
NXOpen.CAE.LaminateSineEvent |
The Laminate Sine Event. |
NXOpen.CAE.LaminateSineEventBuilder |
Represents a NXOpen.CAE.LaminateSineEvent builder |
NXOpen.CAE.LaminateSpreadsheetReport |
Represents a laminate spreadsheet report |
NXOpen.CAE.LaminateSpreadsheetReportBuilder |
Represents a NXOpen.CAE.LaminateSpreadsheetReport builder |
NXOpen.CAE.LaminateSpreadsheetReportCollection |
Represents a collection of NXOpen.CAE.LaminateSpreadsheetReport |
NXOpen.CAE.LaminateViewDrapingResultsBuilder |
Represents the builder for the draping results viewer |
NXOpen.CAE.LbcAssociationMgr |
Represents an abstract NXOpen.CAE.LbcAssociationMgr |
NXOpen.CAE.Loadcase |
Represents loadcases present in a NXOpen.CAE.Result . |
NXOpen.CAE.LocalRemeshBuilder |
Represents a NXOpen.CAE.LocalRemeshBuilder |
NXOpen.CAE.LumpedMassEADBuilder |
This class provides LumpedMass Associated Data Support |
NXOpen.CAE.MMCCreateBuilder |
Represents a NXOpen.CAE.MMCCreateBuilder which can be used to create or edit NXOpen.CAE.MeshMate objects. |
NXOpen.CAE.ManualMorphBuilder |
Represents a NXOpen.CAE.ManualMorphBuilder |
NXOpen.CAE.ManualNodeAssociationBuilder |
Represents a NXOpen.CAE.ManualNodeAssociationBuilder |
NXOpen.CAE.ManualSweepBetweenListItemSelection |
Represents a NXOpen.CAE.ManualSweepBetweenListItemSelection |
NXOpen.CAE.ManualSweepBetweenListItemSelectionList |
Represents a list of objects. |
NXOpen.CAE.ManualSweepBetweenSelection |
Builder for creating Manual Hex Mesh - Face Dependency type. |
NXOpen.CAE.MappedHole |
Represents a CAE mapped hole |
NXOpen.CAE.MappedMesh |
Represents Mesh Recipe |
NXOpen.CAE.MappedMeshBuilder |
Represents a Mapped Mesh Builder. |
NXOpen.CAE.MappedResult |
Represents analysis results for a imported solver results file. |
NXOpen.CAE.MaterialOptions |
Represents the material options to be used when assigning a material to cae part |
NXOpen.CAE.MechanicalLoadSumBuilder |
Represents a NXOpen.CAE.MechanicalLoadSumBuilder |
NXOpen.CAE.Mesh |
Represents a Mesh |
NXOpen.CAE.Mesh0d |
Represents 0d Mesh |
NXOpen.CAE.Mesh0dBuilder |
Represents 0D Mesh |
NXOpen.CAE.Mesh1d |
Represents 1d Mesh |
NXOpen.CAE.Mesh1dBuilder |
Represents 1d Mesh |
NXOpen.CAE.Mesh2d |
Represents 2d Mesh |
NXOpen.CAE.Mesh2dBuilder |
Represents 2D Mesh |
NXOpen.CAE.Mesh2dFree |
Represents 2d Mesh |
NXOpen.CAE.Mesh3d |
Represents 3d Mesh |
NXOpen.CAE.Mesh3dHexBuilder |
Represents 3D Hex Mesh |
NXOpen.CAE.Mesh3dTetBuilder |
Represents 3D Mesh |
NXOpen.CAE.MeshCollector |
Represents a MeshCollector |
NXOpen.CAE.MeshCollectorBuilder |
Represents a NXOpen.CAE.MeshCollectorBuilder |
NXOpen.CAE.MeshCollectorDisplayDefaults |
Represents the base MeshCollectorDisplayDefaults class for Mesh, MeshCollector and |
NXOpen.CAE.MeshCollectorDisplayDefaults0d |
Represents 0d Mesh Display Settings |
NXOpen.CAE.MeshCollectorDisplayDefaults1d |
Represents 1d Mesh Display Settings |
NXOpen.CAE.MeshCollectorDisplayDefaults2d |
Represents 2d Mesh Display Settings |
NXOpen.CAE.MeshCollectorDisplayDefaults3d |
Represents 3d Mesh Display Settings |
NXOpen.CAE.MeshCollectorOccurrence |
Represents a MeshCollector Occurrence |
NXOpen.CAE.MeshCollectorOccurrenceBuilder |
Represents a NXOpen.CAE.MeshCollectorOccurrenceBuilder |
NXOpen.CAE.MeshControl |
Represents a MeshControl |
NXOpen.CAE.MeshControlBuilder |
Represents a NXOpen.CAE.MeshControl |
NXOpen.CAE.MeshControlCollection |
Provides methods for managing mesh controls:py:class:NXOpen.CAE.MeshControl in a fem part |
NXOpen.CAE.MeshControlDisplayManager |
Provides method for creating builder for |
NXOpen.CAE.MeshControlDisplayOptionsBuilder |
Represents a NXOpen.CAE.MeshControlDisplayOptionsBuilder |
NXOpen.CAE.MeshDisplaySettings |
Represents the base MeshDisplaySettings class for Mesh class |
NXOpen.CAE.MeshDisplaySettings0d |
Represents 0d Mesh Display Settings |
NXOpen.CAE.MeshDisplaySettings1d |
Represents 1d Mesh Display Settings |
NXOpen.CAE.MeshDisplaySettings2d |
Represents 2d Mesh Display Settings |
NXOpen.CAE.MeshDisplaySettings3d |
Represents 3d Mesh Display Settings |
NXOpen.CAE.MeshFollower |
Represents Mesh Recipe |
NXOpen.CAE.MeshFromBoundaryBuilder |
Represents a NXOpen.CAE.MeshFromBoundaryBuilder |
NXOpen.CAE.MeshManager |
Creates Meshes:py:class:NXOpen.CAE.Mesh in a fem part |
NXOpen.CAE.MeshManagerOccurrence |
Manages MeshOccurrencs and MeshCollectorOccurrences in a fem part |
NXOpen.CAE.MeshManualSweepBetweenListItemSelection |
Represents a NXOpen.CAE.MeshManualSweepBetweenListItemSelection |
NXOpen.CAE.MeshManualSweepBetweenListItemSelectionList |
Represents a list of objects. |
NXOpen.CAE.MeshMate |
Represents a Mesh Mate |
NXOpen.CAE.MeshPoint |
Represents a smart NXOpen.CAE.MeshPoint . |
NXOpen.CAE.MeshPointCollection |
Provides methods for managing constraints NXOpen.CAE.MeshPoint in a sim part. |
NXOpen.CAE.MeshPointConicCenterBuilder |
Represents a NXOpen.CAE.MeshPointConicCenterBuilder |
NXOpen.CAE.MeshPointExistingPointBuilder |
Represents a NXOpen.CAE.MeshPointExistingPointBuilder |
NXOpen.CAE.MeshPointMultipleOnCurveBuilder |
Represents a NXOpen.CAE.MeshPointMultipleOnCurveBuilder |
NXOpen.CAE.MeshPointOnCurveBuilder |
Represents a NXOpen.CAE.MeshPointOnCurveBuilder |
NXOpen.CAE.MeshPointOnFaceBuilder |
Represents a NXOpen.CAE.MeshPointOnFaceBuilder |
NXOpen.CAE.MeshPointProjectBuilder |
Represents a NXOpen.CAE.MeshPointProjectBuilder |
NXOpen.CAE.MeshShellFromSolid |
Represents 2d Mesh that follows 3d mesh |
NXOpen.CAE.ModelCheckManager |
Provides method for creating builder for |
NXOpen.CAE.ModelDisplayBuilder |
This class provides Model Display Data Support |
NXOpen.CAE.ModelUpdateCorrelMethodBuilder |
Represents a NXOpen.CAE.ModelUpdateCorrelMethodBuilder |
NXOpen.CAE.ModelUpdateDesignVariable |
Represents a NXOpen.CAE.ModelUpdateDesignVariable , which is a meta-solution used to update finite element models to match real life test data |
NXOpen.CAE.ModelUpdateDesignVariablesCollection |
Represents a collection of durability events. |
NXOpen.CAE.ModelUpdateDesignVariablesRapidCreateBuilder |
This class is the builder that is used for the rapid creation of design variables. |
NXOpen.CAE.ModelUpdateOptimOptionsBuilder |
Represents a NXOpen.CAE.ModelUpdateOptimOptionsBuilder |
NXOpen.CAE.ModelUpdateOptionsBuilder |
Represents a NXOpen.CAE.ModelUpdateOptionsBuilder |
NXOpen.CAE.ModelUpdateOverallWeightsBuilder |
Represents a NXOpen.CAE.ModelUpdateOverallWeightsBuilder |
NXOpen.CAE.ModelUpdateSensitivityViewerBuilder |
Represents NXOpen.CAE.ModelUpdateSensitivityViewerBuilder |
NXOpen.CAE.ModelUpdateSolution |
Represents a NXOpen.CAE.ModelUpdateSolution , which is a meta-solution used to update finite element models to match real life test data |
NXOpen.CAE.ModelUpdateSolutionBuilder |
Represents a NXOpen.CAE.ModelUpdateSolutionBuilder |
NXOpen.CAE.ModelUpdateSolutionCollection |
Represents a collection of model update meta solution |
NXOpen.CAE.ModelingObjectPropertyTable |
Represents a Modeling Object Property Table |
NXOpen.CAE.ModelingObjectPropertyTableCollection |
Creates Modeling Object property tables:py:class:NXOpen.CAE.ModelingObjectPropertyTable in a fem model |
NXOpen.CAE.ModifiableFEModelOccAttribute |
This class represents an Interface to the Finite Element Model. |
NXOpen.CAE.MultipleElementCreateBuilder |
Represents a NXOpen.CAE.MultipleElementCreateBuilder which can be used to create mutiple elements in one efficient opertation. |
NXOpen.CAE.MultipleNodeCreateBuilder |
Represents a NXOpen.CAE.MultipleNodeCreateBuilder which can be used to create mutiple nodes in one efficient opertation. |
NXOpen.CAE.NamedPropTableWithTargetSet |
Represents a Solver Specific Modeling Object with associated target set(s) |
NXOpen.CAE.NamedPropertyTable |
Represents a NXOpen.CAE.NamedPropertyTable which is a superclass to NXOpen.CAE.PhysicalPropertyTable |
NXOpen.CAE.NodeAlignBuilder |
Represents a NXOpen.CAE.NodeAlignBuilder |
NXOpen.CAE.NodeAssociationBuilder |
Represents a NXOpen.CAE.NodeAssociationBuilder |
NXOpen.CAE.NodeCreateBuilder |
Represents a NXOpen.CAE.NodeCreateBuilder . |
NXOpen.CAE.NodeDeleteBuilder |
Represents a NXOpen.CAE.NodeDeleteBuilder |
NXOpen.CAE.NodeDissociationBuilder |
Represents a NXOpen.CAE.NodeDissociationBuilder |
NXOpen.CAE.NodeElementInfoBuilder |
Represents a NXOpen.CAE.NodeElementInfoBuilder |
NXOpen.CAE.NodeElementInfoManager |
Provides method for creating builder for |
NXOpen.CAE.NodeElementManager |
Provides method for creating builder for |
NXOpen.CAE.NodeModifyLabelBuilder |
Represents a NXOpen.CAE.NodeModifyLabelBuilder |
NXOpen.CAE.NodeModifyLocationBuilder |
Represents a NXOpen.CAE.NodeModifyLocationBuilder |
NXOpen.CAE.NodeProjectBuilder |
Represents a NXOpen.CAE.NodeProjectBuilder |
NXOpen.CAE.NodeReflectBuilder |
Represents a NXOpen.CAE.NodeReflectBuilder |
NXOpen.CAE.NodeRotateBuilder |
Represents a NXOpen.CAE.NodeRotateBuilder |
NXOpen.CAE.NodeTranslateBuilder |
Represents a NXOpen.CAE.NodeTranslateBuilder |
NXOpen.CAE.NodesBetweenNodesBuilder |
Represents a NXOpen.CAE.NodesBetweenNodesBuilder |
NXOpen.CAE.NodesOnCurveBuilder |
Represents a NXOpen.CAE.NodesOnCurveBuilder |
NXOpen.CAE.NodesRepositionBuilder |
Represents a NXOpen.CAE.NodesRepositionBuilder |
NXOpen.CAE.NxBcPlotContours |
Represents a NXOpen.CAE.NxBcPlotContours object returned from NXOpen.CAE.SimBcPlotContoursBuilder.CreatePlotObject in NXOpen.CAE.SimBcPlotContoursBuilder . |
NXOpen.CAE.OneDimensionalElementSplitBuilder |
Represents a NXOpen.CAE.OneDimensionalElementSplitBuilder |
NXOpen.CAE.PhysicalPropertyTable |
Represents a Physical Property Table |
NXOpen.CAE.PhysicalPropertyTableCollection |
Creates physical property tables:py:class:NXOpen.CAE.PhysicalPropertyTable in a fem model |
NXOpen.CAE.PolygonFaceOnMeshBuilder |
Builder for creating Polygon Face On Mesh |
NXOpen.CAE.PolygonGeometryManager |
Provides methods for managing set NXOpen.CAE.PolygonGeometryManager |
NXOpen.CAE.Post |
Represents Post-Processing |
NXOpen.CAE.Post3DGraphBuilder |
Represents a NXOpen.CAE.Post3DGraphBuilder |
NXOpen.CAE.PostAnnotation |
Controls appearance of a annoation object in a postview. |
NXOpen.CAE.PostAnnotationPreference |
Represents Post-Annotation Preferences |
NXOpen.CAE.PostGraph |
This class provides interfaces to query graph attributes |
NXOpen.CAE.PostGraphAcrossIterationsBuilder |
Represents a NXOpen.CAE.PostGraphAcrossIterationsBuilder |
NXOpen.CAE.PostGraphAlongPathBuilder |
Represents a NXOpen.CAE.PostGraphAlongPathBuilder |
NXOpen.CAE.PostGraphBuilder |
Represents a NXOpen.CAE.PostGraphBuilder |
NXOpen.CAE.PostGraphOrbitBuilder |
Represents a NXOpen.CAE.PostGraphOrbitBuilder |
NXOpen.CAE.PostGraphPreference |
Represents Post-Graph Preferences |
NXOpen.CAE.PostIdentifyPreference |
Represents Post-Identify Preferences |
NXOpen.CAE.PostJtExportBuilder |
Represents a NXOpen.CAE.PostJtExportBuilder used for exporting JTs of Result Types in Post Processing |
NXOpen.CAE.PostLegendPreference |
Represents Post-Legend Preferences |
NXOpen.CAE.PostPreference |
Represents Post Preferences |
NXOpen.CAE.PostResultNavigatorPreference |
Represents Post-ResultNavigator Preferences |
NXOpen.CAE.PreTestDofSet |
Represents Dof Set within a pre-test setup |
NXOpen.CAE.PreTestDofSetBuilder |
Represents a NXOpen.CAE.PreTestDofSet builder |
NXOpen.CAE.PreTestExciterConfig |
Represent a exciter selection configuration |
NXOpen.CAE.PreTestExciterConfigBuilder |
Represents a NXOpen.CAE.PreTestExciterConfig builder |
NXOpen.CAE.PreTestExciterConfigCollection |
Represents a collection of exciter selection configuration |
NXOpen.CAE.PreTestExciterSelectionControl |
Represents a pre-test exciter selection setup |
NXOpen.CAE.PreTestExciterSelectionDofSetCollection |
Represents a collection of exciter selection configuration. |
NXOpen.CAE.PreTestExportUnvBuilder |
This is a manager to the NXOpen.CAE.PreTestExportUnvBuilder class. |
NXOpen.CAE.PreTestSensorConfig |
Represent a sensor selection configuration |
NXOpen.CAE.PreTestSensorConfigBuilder |
Represents a NXOpen.CAE.PreTestSensorConfig builder |
NXOpen.CAE.PreTestSensorConfigCollection |
Represents a collection of sensor selection configuration |
NXOpen.CAE.PreTestSensorSelectionControl |
Represents a pre-test sensor selection setup |
NXOpen.CAE.PreTestSensorSelectionDofSetCollection |
Represents a collection of sensor selection configuration. |
NXOpen.CAE.PreTestSolution |
Represents a pre-test setup |
NXOpen.CAE.PreTestSolutionBuilder |
Represents a NXOpen.CAE.PreTestSolution builder |
NXOpen.CAE.PreTestSolutionCollection |
Represents a collection of pre-test setups |
NXOpen.CAE.PrimitiveMesh |
Represents Primitive Mesh |
NXOpen.CAE.PrimitiveMeshBuilder |
Represents Primitive Mesh |
NXOpen.CAE.ProjectNodesToCadGeometryBuilder |
Allows you to query the mesh nodes that are off the underlying Cad geometry by a given tolerance, and if requested this builder can adjust the node locations to put them back on to the underlying Cad geometry. |
NXOpen.CAE.PropertyTable |
Represents a property table |
NXOpen.CAE.ReassignElementsBuilder |
Represents a NXOpen.CAE.ReassignElementsBuilder |
NXOpen.CAE.RelatedElemEdgeMethod |
Represents the output from the related element edge smart selector method |
NXOpen.CAE.RelatedElemFaceMethod |
Represents the output from the related element face smart selector method |
NXOpen.CAE.RelatedElemMethod |
Represents the output from the related element smart selector method |
NXOpen.CAE.RelatedFaceMethod |
Represents the output from the related face smart selector method |
NXOpen.CAE.RelatedNodeMethod |
Represents the output from the related node smart selector method |
NXOpen.CAE.Result |
This class provides interfaces to query analysis results. |
NXOpen.CAE.ResultAccess |
Represents a specific result state for a given NXOpen.CAE.Result . |
NXOpen.CAE.ResultManager |
Manages results |
NXOpen.CAE.ResultMeasure |
Represents a ResultMeasure class NXOpen.CAE.ResultMeasure . |
NXOpen.CAE.ResultMeasureCollection |
Provides methods for managing ResultMeasures NXOpen.CAE.ResultMeasure |
NXOpen.CAE.ResultMeasureModelSubset |
Represents a a subset of the model upon which to calculate results |
NXOpen.CAE.ResultMeasureModelSubsetFE |
Represents a FE-based subset of the model upon which to calculate results |
NXOpen.CAE.ResultMeasureModelSubsetGeom |
Represents a geometry-based subset of the model upon which to calculate results |
NXOpen.CAE.ResultMeasureResultAllOptions |
Represents the combination of all result options for result measure |
NXOpen.CAE.ResultMeasureResultDirectionOptions |
Represents the result directional options for result measure |
NXOpen.CAE.ResultMeasureResultDirectionSectionOptions |
Represents the result directional and beam/shell section options for result measure |
NXOpen.CAE.ResultMeasureResultOptions |
Represents the basic result options for result measure |
NXOpen.CAE.ResultMeasureResultSectionOptions |
Represents the result with beam/shell section options for result measure |
NXOpen.CAE.ResultParameters |
This class is worked as a packet of information that can be either be used to change result state or pass around for information exchange between two NXOpen.CAE.ResultAccess objects. |
NXOpen.CAE.ResultParametersWithProbe |
To obtain an instance of this class use Session.ResultManager . |
NXOpen.CAE.ResultProbe |
Result Probe Object. |
NXOpen.CAE.ResultProbeBuilder |
Result probe Builder |
NXOpen.CAE.ResultType |
This class represents a result type from a result file. |
NXOpen.CAE.ResultVariable |
Controls Result Exp Object. |
NXOpen.CAE.ResultsCombinationBuilder |
Represents a NXOpen.CAE.ResultsCombinationBuilder |
NXOpen.CAE.ResultsEnvelopeBuilder |
Represents a NXOpen.CAE.ResultsEnvelopeBuilder |
NXOpen.CAE.ResultsManipulationBuilder |
Represents an abstract NXOpen.CAE.ResultsManipulationBuilder |
NXOpen.CAE.ResultsModelExportBuilder |
Represents a NXOpen.CAE.ResultsModelExportBuilder |
NXOpen.CAE.ResultsReductionBuilder |
Represents a NXOpen.CAE.ResultsReductionBuilder |
NXOpen.CAE.SelectCAEBody |
Represents a single object selection. |
NXOpen.CAE.SelectCAEBodyList |
Represents a list of objects on a selection list. |
NXOpen.CAE.SelectCAEEdge |
Represents a single object selection. |
NXOpen.CAE.SelectCAEEdgeList |
Represents a list of objects on a selection list. |
NXOpen.CAE.SelectCAEFace |
Represents a single object selection. |
NXOpen.CAE.SelectCAEFaceList |
Represents a list of objects on a selection list. |
NXOpen.CAE.SelectElementsBuilder |
Represents a NXOpen.CAE.SelectElementsBuilder |
NXOpen.CAE.SelectElementsManager |
Provides method for creating builder for |
NXOpen.CAE.SelectFEElemFaceList |
Represents a list of objects on a selection list. |
NXOpen.CAE.SelectFENode |
Represents a single object selection. |
NXOpen.CAE.SelectFENodeList |
Represents a list of objects on a selection list. |
NXOpen.CAE.SelectMeshList |
Represents a list of objects on a selection list. |
NXOpen.CAE.SetManager |
Represents a group of CAE object sets. |
NXOpen.CAE.ShapeMetricViewerBuilder |
Represents the correlation Shape metrics viewer builder |
NXOpen.CAE.Shell2SolidBuilder |
Represents 3D Tet Mesh |
NXOpen.CAE.ShellEADBuilder |
This class provides Shell Associated Data Support |
NXOpen.CAE.ShowAdjacentBuilder |
Represents a NXOpen.CAE.ShowAdjacentBuilder |
NXOpen.CAE.ShowHideBuilder |
Represents a NXOpen.CAE.ShowHideBuilder |
NXOpen.CAE.ShowHideManager |
Provides method for creating builder for |
NXOpen.CAE.ShowOnlyBuilder |
Represents a NXOpen.CAE.ShowOnlyBuilder |
NXOpen.CAE.SimAutoBcRecipe |
Represents a simulation recipe containing the parameters needed |
NXOpen.CAE.SimBC |
Represents BC class which is a superclass to NXOpen.CAE.SimLoad and NXOpen.CAE.SimConstraint . |
NXOpen.CAE.SimBCBuilder |
This is a manager to the CAE.SimBC class. |
NXOpen.CAE.SimBCDisplay |
Represents a BC display attributes |
NXOpen.CAE.SimBcGroup |
Represents a BC group in a solution or solution step |
NXOpen.CAE.SimBcPlotContoursBuilder |
Represents a NXOpen.CAE.SimBcPlotContoursBuilder builder which can be used to generate a plot of a NXOpen.CAE.SimBC in the graphics area. |
NXOpen.CAE.SimBcXyPlotBuilder |
Represents a NXOpen.CAE.SimBcXyPlotBuilder builder which can be used to generate a XY plot of a NXOpen.CAE.SimBC in the graphics area. |
NXOpen.CAE.SimCondition |
This class represents a Condition which defines a state where all or some values of NXOpen.CAE.SimConditionParam are known. |
NXOpen.CAE.SimConditionCollection |
This class is a collection of NXOpen.CAE.SimCondition . |
NXOpen.CAE.SimConditionParam |
This class represents a named measurable quantity. |
NXOpen.CAE.SimConditionParamCollection |
This class is a collection of NXOpen.CAE.SimConditionParam which represents a measurable environment. |
NXOpen.CAE.SimConditionSeqMgr |
This is the manager for Condition Sequences. |
NXOpen.CAE.SimConditionSequence |
This class represents a time history of NXOpen.CAE.SimCondition . |
NXOpen.CAE.SimConditionSequenceCollection |
This class is a collection of NXOpen.CAE.SimConditionSequence . |
NXOpen.CAE.SimConditionTimeStep |
This class represents a step in the time history of a NXOpen.CAE.SimConditionSequence . |
NXOpen.CAE.SimConditionTimeStepCollection |
This class is a collection of NXOpen.CAE.SimConditionTimeStep . |
NXOpen.CAE.SimConstraint |
Represents a constraint |
NXOpen.CAE.SimConstraintCollection |
Provides methods for managing constraints NXOpen.CAE.SimConstraint in a sim part |
NXOpen.CAE.SimConstraintGroup |
Represents a constraint group in a solution or solution step |
NXOpen.CAE.SimGroupContainer |
Represents UGS::CaeSim::LbcGroupContainer |
NXOpen.CAE.SimLbcFolder |
Represents a folder object in the .sim files |
NXOpen.CAE.SimLbcFolderCollection |
Provides methods for managing LbcFolders NXOpen.CAE.SimLbcFolder in a sim part |
NXOpen.CAE.SimLoad |
Represents a load |
NXOpen.CAE.SimLoadCollection |
Provides methods for managing loads NXOpen.CAE.SimLoad in a sim part |
NXOpen.CAE.SimLoadGroup |
Represents a load group in a solution or solution step |
NXOpen.CAE.SimLoadRecipe |
This is the class handling the attributes of a load recipe. |
NXOpen.CAE.SimLoadRecipeCollection |
This class is a collection of NXOpen.CAE.SimLoadRecipe . |
NXOpen.CAE.SimLoadRecipeLbcGenerator |
Handles generation of subcases and loads based on a CAE.SimLoadRecipe . |
NXOpen.CAE.SimLoadRecipeMapEntry |
These objects represent one line in a NXOpen.CAE.SimLoadRecipe ‘s mapping. |
NXOpen.CAE.SimLoadRecipeMapEntryCollection |
This class is a collection of :py:class:`NXOpen.CAE.SimLoadRecipeMapEntry`s. |
NXOpen.CAE.SimLoadRecipeMapEntryTargetTypes |
The class handles the enum definitions needed by load recipe map entries |
NXOpen.CAE.SimLoadRecipeMapping |
This is the class handling the mapping of a certain load type of a load recipe. |
NXOpen.CAE.SimLoadRecipeMappingCollection |
This class is a collection of :py:class:`NXOpen.CAE.SimLoadRecipeMapping`s. |
NXOpen.CAE.SimLoadRecipeSource |
This is the class handling the attributes of a source used by a load recipe. |
NXOpen.CAE.SimLoadRecipeSourceCollection |
This class is a collection of NXOpen.CAE.SimLoadRecipeSource . |
NXOpen.CAE.SimLoadRecipeTypes |
The class handles the enum definitions needed by load recipes |
NXOpen.CAE.SimLoadSet |
Represents a cae load set object |
NXOpen.CAE.SimLoadSetBuilder |
Represents a NXOpen.CAE.SimLoadSetBuilder builder |
NXOpen.CAE.SimLoadSetCollection |
Provides methods for managing NXOpen.CAE.SimLoadSet in a sim part |
NXOpen.CAE.SimMotionLoadsBuilder |
Represents a NXOpen.CAE.SimMotionLoadsBuilder |
NXOpen.CAE.SimMotionLoadsListItemBuilder |
Represents a NXOpen.CAE.SimMotionLoadsListItemBuilder |
NXOpen.CAE.SimPart |
Represents an NX part of type .sim. |
NXOpen.CAE.SimRecipe |
This is an abstract class. |
NXOpen.CAE.SimRecipeCollection |
Provides methods for managing NXOpen.CAE.SimRecipe in a sim part |
NXOpen.CAE.SimResultReference |
Represents a Result Reference in the .sim files |
NXOpen.CAE.SimSimulation |
This is the root object in a .sim file. |
NXOpen.CAE.SimSimulationObject |
Represents a simulation object |
NXOpen.CAE.SimSimulationObjectCollection |
Provides methods for managing simulation objects NXOpen.CAE.SimSimulationObject in a sim part |
NXOpen.CAE.SimSimulationObjectGroup |
Represents a simulation object group in a solution or solution step |
NXOpen.CAE.SimSolution |
Represents a solution in the .sim files |
NXOpen.CAE.SimSolutionCollection |
Provides methods for managing Solutions NXOpen.CAE.SimSolution in a NXOpen.CAE.SimSimulation |
NXOpen.CAE.SimSolutionStep |
Represents a subcase/step in a solution |
NXOpen.CAE.SketchCurves |
Represents a Beam Cross Section |
NXOpen.CAE.SketchCurvesCollection |
Represents the collection of all NXOpen.CAE.SketchCurves in a fem part |
NXOpen.CAE.SliverFaceMethod |
Represents the output from the sliver face smart selector method |
NXOpen.CAE.SmartSelectionManager |
Provides methods for creating smart selection methods |
NXOpen.CAE.SolidPropertyCheckBuilder |
Represents a NXOpen.CAE.SolidPropertyCheckBuilder |
NXOpen.CAE.SolutionManager |
Represents NXOpen.CAE.SolutionManager |
NXOpen.CAE.SolutionResult |
Represents analysis results for a given NXOpen.CAE.SimSolution . |
NXOpen.CAE.SolverAppendOption |
This class provides access to the append option setting for importing solver specific data into existing Fem/Sim |
NXOpen.CAE.SpiderElementBuilder |
Represents a NXOpen.CAE.SpiderElementBuilder |
NXOpen.CAE.SpringEADBuilder |
This class provides Spring Associated Data Support |
NXOpen.CAE.StandardBeamSection |
Represents a Standard Beam Cross Section |
NXOpen.CAE.StandardBeamSectionBuilder |
Represents a NXOpen.CAE.StandardBeamSectionBuilder |
NXOpen.CAE.StepManager |
Represents NXOpen.CAE.StepManager |
NXOpen.CAE.SuppressHoleBuilder |
Builder for creating Hole Suppression Hole |
NXOpen.CAE.SurfaceCoatBuilder |
Builder for creating Surface Coat |
NXOpen.CAE.SweepBetweenMeshBuilder |
Builder for creating swept mesh between faces. |
NXOpen.CAE.SweptMesh |
Represents swept Mesh |
NXOpen.CAE.TangentContinuousEdgeMethod |
Represents the output from the circular edge smart selector method |
NXOpen.CAE.TangentFaceMethod |
Represents the output from the tangent face smart selector method |
NXOpen.CAE.ThicknessBuilder |
Represents a NXOpen.CAE.ThicknessBuilder |
NXOpen.CAE.ThicknessPlotContours |
Represents a NXOpen.CAE.ThicknessPlotContours object returned from NXOpen.CAE.ThicknessPlotContoursBuilder.CreatePlotObject in NXOpen.CAE.ThicknessPlotContoursBuilder . |
NXOpen.CAE.ThicknessPlotContoursBuilder |
Represents a NXOpen.CAE.ThicknessPlotContoursBuilder builder which can be used to generate a plot of a NXOpen.CAE.SimBC in the graphics area. |
NXOpen.CAE.TransientResultsReductionBuilder |
Represents a NXOpen.CAE.TransientResultsReductionBuilder |
NXOpen.CAE.UnStitchEdgeBuilder |
Represents a NXOpen.CAE.UnStitchEdgeBuilder |
NXOpen.CAE.UserDefinedSolidBeamSection |
Represents a User-Defined Solid Beam Cross Section |
NXOpen.CAE.UserDefinedSolidBeamSectionBuilder |
Represents a NXOpen.CAE.UserDefinedSolidBeamSectionBuilder |
NXOpen.CAE.ViewLaminateBuilder |
Represents a View Laminate Builder. |
NXOpen.CAE.WeldBuilder |
Represents a NXOpen.CAE.WeldBuilder |
NXOpen.CAE.WeldRow |
Represents a CAE weld row |