CaeRegionBuilder Class¶
-
class
NXOpen.CAE.
CaeRegionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.CaeRegionBuilder
builderTo create a new instance of this class, use
NXOpen.CAE.SimSimulation.CreateCaeRegionBuilder
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
PropertyTable | Returns the Region’s property table |
Tag | Returns the Tag for this object. |
TargetSetManager | Returns the target set handler associated with the Region object |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
PropertyTable¶
-
CaeRegionBuilder.
PropertyTable
¶ Returns the Region’s property table
-------------------------------------
Getter Method
Signature
PropertyTable()
Returns: Return type: NXOpen.CAE.PropertyTable
New in version NX7.0.0.
License requirements: None.
TargetSetManager¶
-
CaeRegionBuilder.
TargetSetManager
¶ Returns the target set handler associated with the Region object
-------------------------------------
Getter Method
Signature
TargetSetManager()
Returns: target set manager Return type: NXOpen.CAE.SetManager
New in version NX7.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
CaeRegionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.