DurabilityStrainGageAnalyzerBuilder Class¶
-
class
NXOpen.CAE.
DurabilityStrainGageAnalyzerBuilder
¶ Bases:
NXOpen.Builder
Represents the builder for analyzing strain gage data.
To create a new instance of this class, use
NXOpen.CAE.DurabilityManager.CreateStrainGageAnalyzerBuilder
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AbsoluteMaximumPrincipalAngle | Returns or sets the absoluteMaximumPrincipalAngle. |
AbsoluteMaximumPrincipalStrain | Returns or sets the absoluteMaximumPrincipalStrain. |
AbsoluteMaximumPrincipalStress | Returns or sets the absoluteMaximumPrincipalStress. |
AbsoluteMaximumShearStrain | Returns or sets the absoluteMaximumShearStrain. |
AbsoluteMaximumShearStress | Returns or sets the absoluteMaximumShearStress. |
AxisDirectionSearchMethod | Returns or sets the axis direction search method. |
BiaxialityRatioHistory | Returns or sets the biaxialityRatioHistory. |
CriticalPlaneOption | Returns or sets the critical plane option. |
EffectiveStrain | Returns or sets the effective strain. |
EffectiveStress | Returns or sets the effective stress. |
GageConstruction | Returns or sets the gage construction. |
GagePoissonRatio | Returns or sets the gagePoissonRatio. |
GageSource | Returns or sets the gage source. |
GageType | Returns or sets the gage type. |
Kt1 | Returns or sets the kt1. |
Kt2 | Returns or sets the kt2. |
Kt3 | Returns or sets the kt3. |
MaterialTag | Returns or sets the materialTag. |
MaximumPrincipalAngle | Returns or sets the maximumPrincipalAngle. |
MaximumPrincipalStrain | Returns or sets the maximumPrincipalStrain. |
MaximumPrincipalStress | Returns or sets the maxPrinStress. |
MaximumShearStrain | Returns or sets the maximumShearStrain. |
MaximumShearStress | Returns or sets the maximumShearStress. |
SearchResolution | Returns the search resolution. |
SignedVonMisesStress | Returns or sets the signedVonMisesStress. |
Tag | Returns the Tag for this object. |
TargetFileName | Returns or sets the targetFileName. |
UseEffectiveBiaxialityRatio | Returns or sets the effective biaxiality ratio. |
VonMisesStress | Returns or sets the vonMisesStress. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UseStrainGageData | Use straingage data. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DurabilityStrainGageAnalyzerBuilderAxisDirectionSearchMethodEnum Enumeration | the axis direction search enum. |
DurabilityStrainGageAnalyzerBuilderCriticalPlaneOptionEnum Enumeration | the critical plane option enum. |
DurabilityStrainGageAnalyzerBuilderGageConstructionEnum Enumeration | the gage construction enum. |
DurabilityStrainGageAnalyzerBuilderGageSourceEnum Enumeration | the gage source enum. |
DurabilityStrainGageAnalyzerBuilderGageTypeEnum Enumeration | the gage type enum. |
Property Detail¶
AbsoluteMaximumPrincipalAngle¶
-
DurabilityStrainGageAnalyzerBuilder.
AbsoluteMaximumPrincipalAngle
¶ Returns or sets the absoluteMaximumPrincipalAngle.
-------------------------------------
Getter Method
Signature
AbsoluteMaximumPrincipalAngle()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
AbsoluteMaximumPrincipalAngle(absoluteMaximumPrincipalAngle)
Parameters: absoluteMaximumPrincipalAngle (bool) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
AbsoluteMaximumPrincipalStrain¶
-
DurabilityStrainGageAnalyzerBuilder.
AbsoluteMaximumPrincipalStrain
¶ Returns or sets the absoluteMaximumPrincipalStrain.
-------------------------------------
Getter Method
Signature
AbsoluteMaximumPrincipalStrain()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
AbsoluteMaximumPrincipalStrain(absoluteMaximumPrincipalStrain)
Parameters: absoluteMaximumPrincipalStrain (bool) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
AbsoluteMaximumPrincipalStress¶
-
DurabilityStrainGageAnalyzerBuilder.
AbsoluteMaximumPrincipalStress
¶ Returns or sets the absoluteMaximumPrincipalStress.
-------------------------------------
Getter Method
Signature
AbsoluteMaximumPrincipalStress()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
AbsoluteMaximumPrincipalStress(absoluteMaximumPrincipalStress)
Parameters: absoluteMaximumPrincipalStress (bool) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
AbsoluteMaximumShearStrain¶
-
DurabilityStrainGageAnalyzerBuilder.
AbsoluteMaximumShearStrain
¶ Returns or sets the absoluteMaximumShearStrain.
-------------------------------------
Getter Method
Signature
AbsoluteMaximumShearStrain()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
AbsoluteMaximumShearStrain(absoluteMaximumShearStrain)
Parameters: absoluteMaximumShearStrain (bool) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
AbsoluteMaximumShearStress¶
-
DurabilityStrainGageAnalyzerBuilder.
AbsoluteMaximumShearStress
¶ Returns or sets the absoluteMaximumShearStress.
-------------------------------------
Getter Method
Signature
AbsoluteMaximumShearStress()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
AbsoluteMaximumShearStress(absoluteMaximumShearStress)
Parameters: absoluteMaximumShearStress (bool) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
AxisDirectionSearchMethod¶
-
DurabilityStrainGageAnalyzerBuilder.
AxisDirectionSearchMethod
¶ Returns or sets the axis direction search method.
-------------------------------------
Getter Method
Signature
AxisDirectionSearchMethod()
Returns: Return type: NXOpen.CAE.DurabilityStrainGageAnalyzerBuilderAxisDirectionSearchMethodEnum
New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
AxisDirectionSearchMethod(axisDirectionSearchMethod)
Parameters: axisDirectionSearchMethod ( NXOpen.CAE.DurabilityStrainGageAnalyzerBuilderAxisDirectionSearchMethodEnum
) –New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
BiaxialityRatioHistory¶
-
DurabilityStrainGageAnalyzerBuilder.
BiaxialityRatioHistory
¶ Returns or sets the biaxialityRatioHistory.
-------------------------------------
Getter Method
Signature
BiaxialityRatioHistory()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
BiaxialityRatioHistory(biaxialityRatioHistory)
Parameters: biaxialityRatioHistory (bool) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
CriticalPlaneOption¶
-
DurabilityStrainGageAnalyzerBuilder.
CriticalPlaneOption
¶ Returns or sets the critical plane option.
-------------------------------------
Getter Method
Signature
CriticalPlaneOption()
Returns: Return type: NXOpen.CAE.DurabilityStrainGageAnalyzerBuilderCriticalPlaneOptionEnum
New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
CriticalPlaneOption(criticalPlaneOption)
Parameters: criticalPlaneOption ( NXOpen.CAE.DurabilityStrainGageAnalyzerBuilderCriticalPlaneOptionEnum
) –New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
EffectiveStrain¶
-
DurabilityStrainGageAnalyzerBuilder.
EffectiveStrain
¶ Returns or sets the effective strain.
-------------------------------------
Getter Method
Signature
EffectiveStrain()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
EffectiveStrain(effectiveStrain)
Parameters: effectiveStrain (bool) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
EffectiveStress¶
-
DurabilityStrainGageAnalyzerBuilder.
EffectiveStress
¶ Returns or sets the effective stress.
-------------------------------------
Getter Method
Signature
EffectiveStress()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
EffectiveStress(effectiveStress)
Parameters: effectiveStress (bool) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
GageConstruction¶
-
DurabilityStrainGageAnalyzerBuilder.
GageConstruction
¶ Returns or sets the gage construction.
-------------------------------------
Getter Method
Signature
GageConstruction()
Returns: Return type: NXOpen.CAE.DurabilityStrainGageAnalyzerBuilderGageConstructionEnum
New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
GageConstruction(gageConstruction)
Parameters: gageConstruction ( NXOpen.CAE.DurabilityStrainGageAnalyzerBuilderGageConstructionEnum
) –New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
GagePoissonRatio¶
-
DurabilityStrainGageAnalyzerBuilder.
GagePoissonRatio
¶ Returns or sets the gagePoissonRatio.
-------------------------------------
Getter Method
Signature
GagePoissonRatio()
Returns: Return type: float New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
GagePoissonRatio(gagePoissonRatio)
Parameters: gagePoissonRatio (float) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
GageSource¶
-
DurabilityStrainGageAnalyzerBuilder.
GageSource
¶ Returns or sets the gage source.
-------------------------------------
Getter Method
Signature
GageSource()
Returns: Return type: NXOpen.CAE.DurabilityStrainGageAnalyzerBuilderGageSourceEnum
New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
GageSource(gageSource)
Parameters: gageSource ( NXOpen.CAE.DurabilityStrainGageAnalyzerBuilderGageSourceEnum
) –New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
GageType¶
-
DurabilityStrainGageAnalyzerBuilder.
GageType
¶ Returns or sets the gage type.
-------------------------------------
Getter Method
Signature
GageType()
Returns: Return type: NXOpen.CAE.DurabilityStrainGageAnalyzerBuilderGageTypeEnum
New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
GageType(gageType)
Parameters: gageType ( NXOpen.CAE.DurabilityStrainGageAnalyzerBuilderGageTypeEnum
) –New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Kt1¶
-
DurabilityStrainGageAnalyzerBuilder.
Kt1
¶ Returns or sets the kt1.
-------------------------------------
Getter Method
Signature
Kt1()
Returns: Return type: float New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
Kt1(kt1)
Parameters: kt1 (float) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Kt2¶
-
DurabilityStrainGageAnalyzerBuilder.
Kt2
¶ Returns or sets the kt2.
-------------------------------------
Getter Method
Signature
Kt2()
Returns: Return type: float New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
Kt2(kt2)
Parameters: kt2 (float) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Kt3¶
-
DurabilityStrainGageAnalyzerBuilder.
Kt3
¶ Returns or sets the kt3.
-------------------------------------
Getter Method
Signature
Kt3()
Returns: Return type: float New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
Kt3(kt3)
Parameters: kt3 (float) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
MaterialTag¶
-
DurabilityStrainGageAnalyzerBuilder.
MaterialTag
¶ Returns or sets the materialTag.
-------------------------------------
Getter Method
Signature
MaterialTag()
Returns: Return type: NXOpen.PhysicalMaterial
New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
MaterialTag(materialTag)
Parameters: materialTag ( NXOpen.PhysicalMaterial
) –New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
MaximumPrincipalAngle¶
-
DurabilityStrainGageAnalyzerBuilder.
MaximumPrincipalAngle
¶ Returns or sets the maximumPrincipalAngle.
-------------------------------------
Getter Method
Signature
MaximumPrincipalAngle()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
MaximumPrincipalAngle(maximumPrincipalAngle)
Parameters: maximumPrincipalAngle (bool) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
MaximumPrincipalStrain¶
-
DurabilityStrainGageAnalyzerBuilder.
MaximumPrincipalStrain
¶ Returns or sets the maximumPrincipalStrain.
-------------------------------------
Getter Method
Signature
MaximumPrincipalStrain()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
MaximumPrincipalStrain(maximumPrincipalStrain)
Parameters: maximumPrincipalStrain (bool) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
MaximumPrincipalStress¶
-
DurabilityStrainGageAnalyzerBuilder.
MaximumPrincipalStress
¶ Returns or sets the maxPrinStress.
-------------------------------------
Getter Method
Signature
MaximumPrincipalStress()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
MaximumPrincipalStress(maximumPrincipalStress)
Parameters: maximumPrincipalStress (bool) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
MaximumShearStrain¶
-
DurabilityStrainGageAnalyzerBuilder.
MaximumShearStrain
¶ Returns or sets the maximumShearStrain.
-------------------------------------
Getter Method
Signature
MaximumShearStrain()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
MaximumShearStrain(maximumShearStrain)
Parameters: maximumShearStrain (bool) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
MaximumShearStress¶
-
DurabilityStrainGageAnalyzerBuilder.
MaximumShearStress
¶ Returns or sets the maximumShearStress.
-------------------------------------
Getter Method
Signature
MaximumShearStress()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
MaximumShearStress(maximumShearStress)
Parameters: maximumShearStress (bool) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
SearchResolution¶
-
DurabilityStrainGageAnalyzerBuilder.
SearchResolution
¶ Returns the search resolution.
-------------------------------------
Getter Method
Signature
SearchResolution()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
SignedVonMisesStress¶
-
DurabilityStrainGageAnalyzerBuilder.
SignedVonMisesStress
¶ Returns or sets the signedVonMisesStress.
-------------------------------------
Getter Method
Signature
SignedVonMisesStress()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
SignedVonMisesStress(signedVonMisesStress)
Parameters: signedVonMisesStress (bool) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
TargetFileName¶
-
DurabilityStrainGageAnalyzerBuilder.
TargetFileName
¶ Returns or sets the targetFileName.
-------------------------------------
Getter Method
Signature
TargetFileName()
Returns: Return type: str New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
TargetFileName(filename)
Parameters: filename (str) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
UseEffectiveBiaxialityRatio¶
-
DurabilityStrainGageAnalyzerBuilder.
UseEffectiveBiaxialityRatio
¶ Returns or sets the effective biaxiality ratio.
-------------------------------------
Getter Method
Signature
UseEffectiveBiaxialityRatio()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
UseEffectiveBiaxialityRatio(useEffectiveBiaxialityRatio)
Parameters: useEffectiveBiaxialityRatio (bool) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
VonMisesStress¶
-
DurabilityStrainGageAnalyzerBuilder.
VonMisesStress
¶ Returns or sets the vonMisesStress.
-------------------------------------
Getter Method
Signature
VonMisesStress()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
VonMisesStress(vonMisesStress)
Parameters: vonMisesStress (bool) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Method Detail¶
UseStrainGageData¶
-
DurabilityStrainGageAnalyzerBuilder.
UseStrainGageData
¶ Use straingage data.
Signature
UseStrainGageData(prefixName, name, afuName, numRecords, index1, index2, index3)
Parameters: - prefixName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- afuName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- numRecords (int) –
- index1 (int) –
- index2 (int) –
- index3 (int) –
New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Validate¶
-
DurabilityStrainGageAnalyzerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.