PhysicalMaterial Class¶
-
class
NXOpen.
PhysicalMaterial
¶ Bases:
NXOpen.Material
,NXOpen.CAE.IExportableFEEntity
Represents Physical Material
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AssignObjects | Assigns the material to solid bodies |
AssignToAllBodies | Assigns the material to all solid bodies |
AssignToBodiesNotUsingPreferredMaterial | Assigns the material to all solid bodies not using the preferred material. |
AssignToBodiesWithoutMaterials | Assigns the material to all solid bodies without a material already assigned. |
Copy | Creates new (copied) material with same properties as the original material. |
CopyLibMatlToPart | Copies a library material to a part. |
Delete | Deletes a material from the part. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAlternatename | Returns the material alternate name @return the alternate name for the material |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCategory | Returns the material category @return the category for the material |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDescription | Returns the material description @return the description for the material |
GetId | Returns the material id @return the id for the material |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetLibraryName | Returns the library name if the material was loaded from a library @return the name of the library or None for nonlibrary materials |
GetMaterialCategory | Returns the material category using international character set @return the category for the material |
GetMaterialEditable | Returns whether the material can be modified or not @return |
GetMaterialType | Returns the material type @return the type for the material |
GetParentlibrarymaterial | Returns the parent libary material information |
GetParentmaterial | Returns the parent material that the material was copied from @return material that the material was originally copied from (parent) |
GetPropTable | Returns the property table that contains the properties for this material. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSolverCardSyntax | Returns the solver card syntax strings for this entity. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetSubcategory | Returns the material sub-category @return the subcategory for the material |
GetTeamcenterMaterialItem | Returns the Teamcenter item if the material was loaded from Teamcenter @return the Teamcenter item or None for non-Teamcenter materials |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUsage | Finds the objects using this material |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
GetVersion | Returns the material version @return the material version or None for non-versioned materials |
HasParentlibrarymaterial | Returns whether the material was copied from a library material @return true if it is a copy of a library material and false if it is not |
HasParentmaterial | Returns whether the material was copied from another material @return true if it is a copy of another (parent) material and false if it is not |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
InfoMaterial | Displays the property values for the material in the information window. |
InfoMaterialToFile | Writes the property values for the material to a file. |
IsLoadedLibraryMaterial | Returns true if the material is loaded from a library (not Teamcenter) @return true if it a loaded library material and false if it is a local material or a Teamcenter item revision |
IsLoadedTeamcenterMaterialItem | Returns true if the material is loaded from Teamcenter @return true if it a loaded Teamcenter material and false if it is a local material or a loaded library material |
IsNonlibraryMaterial | Returns true if the material is locally defined (not a library/Teamcenter material) @return true if it is a locally defined material and false if it is a loaded library material or Teamcenter item revision |
Prints a representation of this object to the system log file. | |
ReplaceMaterialAssignment | Replaces all assignments of one material with another material in the part where the material is assigned. |
ResyncWithLibraryDefinition | Re-synchronizes a loaded library material to match its latest library definition. |
SetAlternatename | Sets the material alternate name |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetCategory | Sets the material category |
SetDescription | Sets the material description |
SetId | Sets the material id |
SetMaterialCategory | Sets the material category using international character set |
SetMaterialEditable | Sets whether a material can be modified or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetSubcategory | Sets the material sub-category |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
UnassignAllObjects | Removes the material assignment from all the objects that has it currently assigned |
UpdateMaterialProperties | Re-synchronizes a material with its definition. |
Enumerations¶
PhysicalMaterialAssignWarning Enumeration | Indicates the underlying issues when trying to assign material |
PhysicalMaterialCategory Enumeration | The different categories of materials. |
PhysicalMaterialType Enumeration | The different types of materials. |
Property Detail¶
IsOccurrence¶
-
PhysicalMaterial.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
PhysicalMaterial.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
PhysicalMaterial.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
PhysicalMaterial.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
PhysicalMaterial.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
PhysicalMaterial.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
AssignObjects¶
-
PhysicalMaterial.
AssignObjects
¶ Assigns the material to solid bodies
Signature
AssignObjects(objects)
Parameters: objects (list of NXOpen.NXObject
) – objects to assign this material toNew in version NX6.0.0.
License requirements: None.
AssignToAllBodies¶
-
PhysicalMaterial.
AssignToAllBodies
¶ Assigns the material to all solid bodies
Signature
AssignToAllBodies()
New in version NX7.5.3.
License requirements: None.
AssignToBodiesNotUsingPreferredMaterial¶
-
PhysicalMaterial.
AssignToBodiesNotUsingPreferredMaterial
¶ Assigns the material to all solid bodies not using the preferred material.
Invalid bodies are skipped and a warning code will be returned.
Signature
AssignToBodiesNotUsingPreferredMaterial()
Returns: Returns a warning code if any Return type: NXOpen.PhysicalMaterialAssignWarning
New in version NX7.5.3.
License requirements: None.
AssignToBodiesWithoutMaterials¶
-
PhysicalMaterial.
AssignToBodiesWithoutMaterials
¶ Assigns the material to all solid bodies without a material already assigned.
Invalid bodies are skipped and a warning code will be returned.
Signature
AssignToBodiesWithoutMaterials()
Returns: Returns a warning code if any Return type: NXOpen.PhysicalMaterialAssignWarning
New in version NX7.5.3.
License requirements: None.
Copy¶
-
PhysicalMaterial.
Copy
¶ Creates new (copied) material with same properties as the original material.
The name of the new (copied) material will be unique and based on the name of the original material.
Signature
Copy(partObject)
Parameters: partObject ( NXOpen.NXObject
) – object in part where to copy material toReturns: the new material copied from this material Return type: NXOpen.PhysicalMaterial
New in version NX6.0.0.
License requirements: None.
CopyLibMatlToPart¶
-
PhysicalMaterial.
CopyLibMatlToPart
¶ Overloaded method CopyLibMatlToPart
CopyLibMatlToPart(partObject)
CopyLibMatlToPart(partObject, editable)
-------------------------------------
Copies a library material to a part.
Signature
CopyLibMatlToPart(partObject)
Parameters: partObject ( NXOpen.NXObject
) – object in part where to copy material toReturns: the new material copied from this material Return type: NXOpen.PhysicalMaterial
New in version NX6.0.2.
License requirements: None.
-------------------------------------
Copies a library material to a part. The copied (local) material can either be set to be editable or non-editable which determines whether the material can be modified or not.
Signature
CopyLibMatlToPart(partObject, editable)
Parameters: - partObject (
NXOpen.NXObject
) – object in part where to copy material to - editable (bool) – when true, creates a local material ready for user editting. When false, it creates an exact copy of a loaded library material. The difference between loading and copying with this set to false is loading will get the latest library version whereas if the library material passed in is not synchronized with the latest version, the copy will also not be synchronized with the latest version.
Returns: the new material copied from this material
Return type: New in version NX8.5.0.
License requirements: None.
-------------------------------------
Delete¶
-
PhysicalMaterial.
Delete
¶ Deletes a material from the part.
Signature
Delete()
New in version NX6.0.0.
License requirements: None.
FindObject¶
-
PhysicalMaterial.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAlternatename¶
-
PhysicalMaterial.
GetAlternatename
¶ Returns the material alternate name
Signature
GetAlternatename()
Returns: the alternate name for the material Return type: str New in version NX8.5.0.
License requirements: None.
GetCategory¶
-
PhysicalMaterial.
GetCategory
¶ Returns the material category
Signature
GetCategory()
Returns: the category for the material Return type: str New in version NX6.0.0.
License requirements: None.
GetDescription¶
-
PhysicalMaterial.
GetDescription
¶ Returns the material description
Signature
GetDescription()
Returns: the description for the material Return type: str New in version NX6.0.0.
License requirements: None.
GetId¶
-
PhysicalMaterial.
GetId
¶ Returns the material id
Signature
GetId()
Returns: the id for the material Return type: int New in version NX7.5.0.
License requirements: None.
GetLibraryName¶
-
PhysicalMaterial.
GetLibraryName
¶ Returns the library name if the material was loaded from a library
Signature
GetLibraryName()
Returns: the name of the library or None for nonlibrary materials Return type: str New in version NX7.5.3.
License requirements: None.
GetMaterialCategory¶
-
PhysicalMaterial.
GetMaterialCategory
¶ Returns the material category using international character set
Signature
GetMaterialCategory()
Returns: the category for the material Return type: str New in version NX8.5.0.
License requirements: None.
GetMaterialEditable¶
-
PhysicalMaterial.
GetMaterialEditable
¶ Returns whether the material can be modified or not
Signature
GetMaterialEditable()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
GetMaterialType¶
-
PhysicalMaterial.
GetMaterialType
¶ Returns the material type
Signature
GetMaterialType()
Returns: the type for the material Return type: NXOpen.PhysicalMaterialType
New in version NX6.0.0.
License requirements: None.
GetParentlibrarymaterial¶
-
PhysicalMaterial.
GetParentlibrarymaterial
¶ Returns the parent libary material information
Signature
GetParentlibrarymaterial()
Returns: a tuple Return type: A tuple consisting of (parentName, parentLibraryName). parentName is a str. parentLibraryName is a str. New in version NX8.5.0.
License requirements: None.
GetParentmaterial¶
-
PhysicalMaterial.
GetParentmaterial
¶ Returns the parent material that the material was copied from
Signature
GetParentmaterial()
Returns: material that the material was originally copied from (parent) Return type: NXOpen.PhysicalMaterial
New in version NX8.5.0.
License requirements: None.
GetPropTable¶
-
PhysicalMaterial.
GetPropTable
¶ Returns the property table that contains the properties for this material.
Signature
GetPropTable()
Returns: Return type: NXOpen.BasePropertyTable
New in version NX7.5.3.
License requirements: None.
GetSolverCardSyntax¶
-
PhysicalMaterial.
GetSolverCardSyntax
¶ Returns the solver card syntax strings for this entity.
Signature
GetSolverCardSyntax()
Returns: Return type: list of str New in version NX8.5.0.
License requirements: None.
GetSubcategory¶
-
PhysicalMaterial.
GetSubcategory
¶ Returns the material sub-category
Signature
GetSubcategory()
Returns: the subcategory for the material Return type: str New in version NX8.5.0.
License requirements: None.
GetTeamcenterMaterialItem¶
-
PhysicalMaterial.
GetTeamcenterMaterialItem
¶ Returns the Teamcenter item if the material was loaded from Teamcenter
Signature
GetTeamcenterMaterialItem()
Returns: the Teamcenter item or None for non-Teamcenter materials Return type: str New in version NX7.5.3.
License requirements: None.
GetUsage¶
-
PhysicalMaterial.
GetUsage
¶ Finds the objects using this material
Signature
GetUsage()
Returns: the objects using the material Return type: list of NXOpen.NXObject
New in version NX6.0.0.
License requirements: None.
GetVersion¶
-
PhysicalMaterial.
GetVersion
¶ Returns the material version
Signature
GetVersion()
Returns: the material version or None for non-versioned materials Return type: str New in version NX7.5.3.
License requirements: None.
HasParentlibrarymaterial¶
-
PhysicalMaterial.
HasParentlibrarymaterial
¶ Returns whether the material was copied from a library material
Signature
HasParentlibrarymaterial()
Returns: true if it is a copy of a library material and false if it is not Return type: bool New in version NX8.5.0.
License requirements: None.
HasParentmaterial¶
-
PhysicalMaterial.
HasParentmaterial
¶ Returns whether the material was copied from another material
Signature
HasParentmaterial()
Returns: true if it is a copy of another (parent) material and false if it is not Return type: bool New in version NX8.5.0.
License requirements: None.
InfoMaterial¶
-
PhysicalMaterial.
InfoMaterial
¶ Displays the property values for the material in the information window.
Signature
InfoMaterial()
New in version NX7.5.3.
License requirements: None.
InfoMaterialToFile¶
-
PhysicalMaterial.
InfoMaterialToFile
¶ Writes the property values for the material to a file.
Signature
InfoMaterialToFile(bOverride, pcFileName)
Parameters: - bOverride (bool) – if the file already exists, true override the file, false append to the file
- pcFileName (str) – the full path including filename of file where the information should be written NOTE: The full Unicode character set is not supported for this parameter.
New in version NX7.5.3.
License requirements: None.
IsLoadedLibraryMaterial¶
-
PhysicalMaterial.
IsLoadedLibraryMaterial
¶ Returns true if the material is loaded from a library (not Teamcenter)
Signature
IsLoadedLibraryMaterial()
Returns: true if it a loaded library material and false if it is a local material or a Teamcenter item revision Return type: bool New in version NX7.5.3.
License requirements: None.
IsLoadedTeamcenterMaterialItem¶
-
PhysicalMaterial.
IsLoadedTeamcenterMaterialItem
¶ Returns true if the material is loaded from Teamcenter
Signature
IsLoadedTeamcenterMaterialItem()
Returns: true if it a loaded Teamcenter material and false if it is a local material or a loaded library material Return type: bool New in version NX7.5.3.
License requirements: None.
IsNonlibraryMaterial¶
-
PhysicalMaterial.
IsNonlibraryMaterial
¶ Returns true if the material is locally defined (not a library/Teamcenter material)
Signature
IsNonlibraryMaterial()
Returns: true if it is a locally defined material and false if it is a loaded library material or Teamcenter item revision Return type: bool New in version NX7.5.3.
License requirements: None.
Print¶
-
PhysicalMaterial.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
ReplaceMaterialAssignment¶
-
PhysicalMaterial.
ReplaceMaterialAssignment
¶ Replaces all assignments of one material with another material in the part where the material is assigned.
The part needs to be fully loaded, the new material needs to be in the same part as the original material and the material type needs to be a valid material assignment target.
Signature
ReplaceMaterialAssignment(newMatl)
Parameters: newMatl ( NXOpen.PhysicalMaterial
) – the new material tag, None is not allowed.New in version NX10.0.0.
License requirements: None.
ResyncWithLibraryDefinition¶
-
PhysicalMaterial.
ResyncWithLibraryDefinition
¶ Re-synchronizes a loaded library material to match its latest library definition.
Signature
ResyncWithLibraryDefinition()
New in version NX7.5.2.
License requirements: None.
SetAlternatename¶
-
PhysicalMaterial.
SetAlternatename
¶ Sets the material alternate name
Signature
SetAlternatename(materialAlternatename)
Parameters: materialAlternatename (str) – the alternate name for the material New in version NX8.5.0.
License requirements: None.
SetCategory¶
-
PhysicalMaterial.
SetCategory
¶ Sets the material category
Signature
SetCategory(materialCategory)
Parameters: materialCategory (str) – the category for the material NOTE: The full Unicode character set is not supported for this parameter. New in version NX6.0.0.
License requirements: None.
SetDescription¶
-
PhysicalMaterial.
SetDescription
¶ Sets the material description
Signature
SetDescription(materialDescription)
Parameters: materialDescription (str) – the description for the material New in version NX6.0.0.
License requirements: None.
SetId¶
-
PhysicalMaterial.
SetId
¶ Sets the material id
Signature
SetId(materialId)
Parameters: materialId (int) – the id for the material New in version NX7.5.0.
License requirements: None.
SetMaterialCategory¶
-
PhysicalMaterial.
SetMaterialCategory
¶ Sets the material category using international character set
Signature
SetMaterialCategory(materialCategory)
Parameters: materialCategory (str) – the category for the material New in version NX8.5.0.
License requirements: None.
SetMaterialEditable¶
-
PhysicalMaterial.
SetMaterialEditable
¶ Sets whether a material can be modified or not.
Note: library materials cannot be set to be able to be modified.
Signature
SetMaterialEditable(isEditable)
Parameters: isEditable (bool) – New in version NX10.0.0.
License requirements: None.
SetName¶
-
PhysicalMaterial.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetSubcategory¶
-
PhysicalMaterial.
SetSubcategory
¶ Sets the material sub-category
Signature
SetSubcategory(materialSubcategory)
Parameters: materialSubcategory (str) – the subcategory for the material New in version NX8.5.0.
License requirements: None.