PhysicalMaterialType Enumeration¶
NXOpen.PhysicalMaterial.Type is an alias for NXOpen.PhysicalMaterialType
-
class
NXOpen.
PhysicalMaterialType
¶ Bases:
object
The different types of materials.
The material list generated will be filtered based on the material type chosen
Enum Members
Enum Member Enum Member Description Isotropic IsotropicOrthotropic OrthotropicAnisotropic AnisotropicFluid FluidGeneralHyperelastic Hyperelastic - GeneralMooneyrivlin Mooney RivlinMooneyrivlintestdata Mooney Rivlin - test data optionPolynomial PolynomialReducedpolynomial Reduced PolynomialOgden OgdenOgdentestdata Ogden - test data optionFoam FoamFoamtestdata Foam - test data optionBlatz Blatz-KoArrudaboyce Arruda-BoyceArrudaboycetestdata Arruda-Boyce - test data optionNeohooke Neo HookeNeohooketestdata Neo Hooke - test data optionMarlow MarlowVanderwaals Van Der WaalsYeoh YeohYeohtestdata Yeoh - test data optionGent GentGasket GasketGasketbehavior Gasket BehaviorShapememoryalloy Shape Memory AlloySussmanbathe Sussman-Bathe hyperelastic materialGasketdisplacement Gasket with length-based loadingDamageinterface Damage interface materialMultiplefluid Multiple fluid material-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-