SketchCurvesCollection Class¶
-
class
NXOpen.CAE.
SketchCurvesCollection
¶ Bases:
object
Represents the collection of all
NXOpen.CAE.SketchCurves
in a fem partTo obtain an instance of this class, refer to
NXOpen.CAE.BaseFemPart
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.CAE.SketchCurves with the given identifier as recorded in a journal. |
Method Detail¶
FindObject¶
-
SketchCurvesCollection.
FindObject
¶ Finds the
NXOpen.CAE.SketchCurves
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Sketch Curves name Returns: Sketch Curves with this identifier Return type: NXOpen.CAE.SketchCurves
New in version NX5.0.0.
License requirements: None.