SolidPropertyCheckBuilder Class¶
-
class
NXOpen.CAE.
SolidPropertyCheckBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.SolidPropertyCheckBuilder
To create a new instance of this class, use
NXOpen.CAE.ModelCheckManager.CreateSolidPropertyCheckBuilder
New in version NX5.0.1.
Properties¶
Property | Description |
---|---|
DefaultTemperatureOption | Returns or sets the output mass split option option |
DisplayCgOption | Returns or sets the output mass split option option |
Elements | Returns the selected elements |
EvaluationTemparature | Returns the output temperature option in C |
OutputOption | Returns or sets the detail output option |
ReferenceCsys | Returns or sets the reference csys |
SplitMass | Returns or sets the output mass split option option |
Tag | Returns the Tag for this object. |
UserSpecifiedUnit | Returns or sets the output result unit |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SolidPropertyCheckBuilderUserUnit Enumeration | User Specified output unit |
Property Detail¶
DefaultTemperatureOption¶
-
SolidPropertyCheckBuilder.
DefaultTemperatureOption
¶ Returns or sets the output mass split option option
-------------------------------------
Getter Method
Signature
DefaultTemperatureOption()
Returns: Return type: bool New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefaultTemperatureOption(defaultTemperatureOption)
Parameters: defaultTemperatureOption (bool) – New in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
DisplayCgOption¶
-
SolidPropertyCheckBuilder.
DisplayCgOption
¶ Returns or sets the output mass split option option
-------------------------------------
Getter Method
Signature
DisplayCgOption()
Returns: Return type: bool New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayCgOption(displayCG)
Parameters: displayCG (bool) – New in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
Elements¶
-
SolidPropertyCheckBuilder.
Elements
¶ Returns the selected elements
-------------------------------------
Getter Method
Signature
Elements()
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX6.0.0.
License requirements: None.
EvaluationTemparature¶
-
SolidPropertyCheckBuilder.
EvaluationTemparature
¶ Returns the output temperature option in C
-------------------------------------
Getter Method
Signature
EvaluationTemparature()
Returns: Return type: NXOpen.Expression
New in version NX5.0.1.
License requirements: None.
OutputOption¶
-
SolidPropertyCheckBuilder.
OutputOption
¶ Returns or sets the detail output option
-------------------------------------
Getter Method
Signature
OutputOption()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputOption(outputOpt)
Parameters: outputOpt (bool) – New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ReferenceCsys¶
-
SolidPropertyCheckBuilder.
ReferenceCsys
¶ Returns or sets the reference csys
-------------------------------------
Getter Method
Signature
ReferenceCsys()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceCsys(referenceCsys)
Parameters: referenceCsys ( NXOpen.CoordinateSystem
) –New in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
SplitMass¶
-
SolidPropertyCheckBuilder.
SplitMass
¶ Returns or sets the output mass split option option
-------------------------------------
Getter Method
Signature
SplitMass()
Returns: Return type: bool New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
SplitMass(splitMass)
Parameters: splitMass (bool) – New in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
UserSpecifiedUnit¶
-
SolidPropertyCheckBuilder.
UserSpecifiedUnit
¶ Returns or sets the output result unit
-------------------------------------
Getter Method
Signature
UserSpecifiedUnit()
Returns: Return type: NXOpen.CAE.SolidPropertyCheckBuilderUserUnit
New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserSpecifiedUnit(userSpecifiedUnit)
Parameters: userSpecifiedUnit ( NXOpen.CAE.SolidPropertyCheckBuilderUserUnit
) –New in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
SolidPropertyCheckBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.