ModelCheckManager Class¶
-
class
NXOpen.CAE.
ModelCheckManager
¶ Bases:
object
Provides method for creating builder for node element operation commands in a fem part
To obtain an instance of this class, refer to
NXOpen.CAE.CaePart
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CheckModelConsistency | Checks model consistency for all NXOpen.CAE.CAEBody in a NXOpen.CAE.FemPart , to find out the CAE bodies which is inconsistent to the master bodies, output the body list to log file or listing window if there is no log file name specified. |
CreateAlignShellElementNormalBuilder | Provides access for creating align 2D element normal builders in a cae part @return |
CreateDuplicateElementsCheckBuilder | Provides access for creating duplicate elements builder in a cae part. |
CreateDuplicateNodesCheckBuilder | Provides access for creating duplicate nodes builder in a cae part. |
CreateElementEdgeCheckBuilder | Provides access for creating Model Check builders in a cae part @return |
CreateElementMaterialOrientationCheckBuilder | Provides access for creating element material orientation builder in a cae part. |
CreateElementQualityCheckBuilder | Provides access for creating element quality Check builders in a cae part @return |
CreateFaceClearanceCheckBuilder | Provides access for creating face clearance check builder in a NXOpen.CAE.FemPart part. |
CreateMechanicalLoadSumBuilder | Creates a builder for mechanical load summary command @return |
CreateModelSetupCheckBuilder | Provides access for creating model setup check builder in a NXOpen.CAE.SimPart part or NXOpen.CAE.AssyFemPart @return |
CreateReverseShellElementNormalBuilder | Provides access for creating reverse 2D element normal builders in a cae part @return |
CreateSolidPropertyCheckBuilder | Creates a builder for solid properties check command @return |
Method Detail¶
CheckModelConsistency¶
-
ModelCheckManager.
CheckModelConsistency
¶ Checks model consistency for all
NXOpen.CAE.CAEBody
in aNXOpen.CAE.FemPart
, to find out the CAE bodies which is inconsistent to the master bodies, output the body list to log file or listing window if there is no log file name specified.If the master part is not loaded, a
NXOpen.CAE.CaeGroup
is created to contain these failed bodies.If the master part is loaded, continue to fix the inconsistent CAE bodies by deleting and recreating them. The mesh recipes associated with the bodies will be deleted while fixing model consistency. A
NXOpen.CAE.CaeGroup
is created to contain the bodies created newlySignature
CheckModelConsistency(logFileName)
Parameters: logFileName (str) – the full log file name NOTE: The full Unicode character set is not supported for this parameter. Returns: a tuple Return type: A tuple consisting of (fixConsistency, caeBodySet). fixConsistency is a bool. indicates whether the inconsistency is fixed caeBodySet is a NXOpen.CAE.CaeGroup
. the group constains the failed CAE bodies or new CAE bodies recreatedNew in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateAlignShellElementNormalBuilder¶
-
ModelCheckManager.
CreateAlignShellElementNormalBuilder
¶ Provides access for creating align 2D element normal builders in a cae part
Signature
CreateAlignShellElementNormalBuilder()
Returns: Return type: NXOpen.CAE.ModelCheck.AlignShellElementNormalBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateDuplicateElementsCheckBuilder¶
-
ModelCheckManager.
CreateDuplicateElementsCheckBuilder
¶ Provides access for creating duplicate elements builder in a cae part.
Duplicate elements can only be deleted when this builder is created in a
NXOpen.CAE.BaseFemPart
part.Signature
CreateDuplicateElementsCheckBuilder()
Returns: Return type: NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateDuplicateNodesCheckBuilder¶
-
ModelCheckManager.
CreateDuplicateNodesCheckBuilder
¶ Provides access for creating duplicate nodes builder in a cae part.
Duplicate nodes can only be merged when this builder is created in a
NXOpen.CAE.BaseFemPart
part.Signature
CreateDuplicateNodesCheckBuilder()
Returns: Return type: NXOpen.CAE.ModelCheck.DuplicateNodesCheckBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateElementEdgeCheckBuilder¶
-
ModelCheckManager.
CreateElementEdgeCheckBuilder
¶ Provides access for creating Model Check builders in a cae part
Signature
CreateElementEdgeCheckBuilder()
Returns: Return type: NXOpen.CAE.ModelCheck.ElementEdgeCheckBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateElementMaterialOrientationCheckBuilder¶
-
ModelCheckManager.
CreateElementMaterialOrientationCheckBuilder
¶ Provides access for creating element material orientation builder in a cae part.
Signature
CreateElementMaterialOrientationCheckBuilder()
Returns: Return type: NXOpen.CAE.ModelCheck.ElementMaterialOrientationCheckBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateElementQualityCheckBuilder¶
-
ModelCheckManager.
CreateElementQualityCheckBuilder
¶ Provides access for creating element quality Check builders in a cae part
Signature
CreateElementQualityCheckBuilder()
Returns: Return type: NXOpen.CAE.ModelCheck.ElementQualityCheckBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateFaceClearanceCheckBuilder¶
-
ModelCheckManager.
CreateFaceClearanceCheckBuilder
¶ Provides access for creating face clearance check builder in a
NXOpen.CAE.FemPart
part.Signature
CreateFaceClearanceCheckBuilder()
Returns: Return type: NXOpen.CAE.ModelCheck.FaceClearanceCheckBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateMechanicalLoadSumBuilder¶
-
ModelCheckManager.
CreateMechanicalLoadSumBuilder
¶ Creates a builder for mechanical load summary command
Signature
CreateMechanicalLoadSumBuilder()
Returns: Return type: NXOpen.CAE.MechanicalLoadSumBuilder
New in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateModelSetupCheckBuilder¶
-
ModelCheckManager.
CreateModelSetupCheckBuilder
¶ Provides access for creating model setup check builder in a
NXOpen.CAE.SimPart
part orNXOpen.CAE.AssyFemPart
Signature
CreateModelSetupCheckBuilder()
Returns: Return type: NXOpen.CAE.ModelCheck.ModelSetupCheckBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateReverseShellElementNormalBuilder¶
-
ModelCheckManager.
CreateReverseShellElementNormalBuilder
¶ Provides access for creating reverse 2D element normal builders in a cae part
Signature
CreateReverseShellElementNormalBuilder()
Returns: Return type: NXOpen.CAE.ModelCheck.ReverseShellElementNormalBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateSolidPropertyCheckBuilder¶
-
ModelCheckManager.
CreateSolidPropertyCheckBuilder
¶ Creates a builder for solid properties check command
Signature
CreateSolidPropertyCheckBuilder()
Returns: Return type: NXOpen.CAE.SolidPropertyCheckBuilder
New in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)