ReverseShellElementNormalBuilder Class¶
-
class
NXOpen.CAE.ModelCheck.
ReverseShellElementNormalBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ModelCheck.ReverseShellElementNormalBuilder
used to reverse normals for specified shell elements.You can reverse shell element normals by using either
Builder.Commit
orNXOpen.CAE.ModelCheck.ReverseShellElementNormalBuilder.ReverseNormals
. The difference between these two methods isBuilder.Commit
reverses the normals and updates normal display, but it does not return the shell elements which were reversed successfully.NXOpen.CAE.ModelCheck.ReverseShellElementNormalBuilder.ReverseNormals
reverses normals and returns the shell elements which were reversed successfully. Both of the methods are only available in fem context.To create a new instance of this class, use
NXOpen.CAE.ModelCheckManager.CreateReverseShellElementNormalBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
SelectionList | Returns the selected objects to be checked. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DisplayNormals | Display normals of NXOpen.CAE.ModelCheck.ReverseShellElementNormalBuilder.SelectionList |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ReverseNormals | Reverses normals specified in NXOpen.CAE.ModelCheck.ReverseShellElementNormalBuilder.SelectionList and returns those elements whose normals were reversed successfully. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SelectionList¶
-
ReverseShellElementNormalBuilder.
SelectionList
¶ Returns the selected objects to be checked.
The objects must be
NXOpen.CAE.Mesh
orNXOpen.CAE.FEElement
-------------------------------------
Getter Method
Signature
SelectionList()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX8.5.0.
License requirements: None.
Method Detail¶
DisplayNormals¶
-
ReverseShellElementNormalBuilder.
DisplayNormals
¶ Display normals of
NXOpen.CAE.ModelCheck.ReverseShellElementNormalBuilder.SelectionList
Signature
DisplayNormals()
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ReverseNormals¶
-
ReverseShellElementNormalBuilder.
ReverseNormals
¶ Reverses normals specified in
NXOpen.CAE.ModelCheck.ReverseShellElementNormalBuilder.SelectionList
and returns those elements whose normals were reversed successfully.This method will only reverse the normals for shell elements in the current work fem part.
Signature
ReverseNormals()
Returns: Return type: list of NXOpen.CAE.FEElement
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Validate¶
-
ReverseShellElementNormalBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.