AssyFemPart Class¶
-
class
NXOpen.CAE.
AssyFemPart
¶ Bases:
NXOpen.CAE.BaseFemPart
Represents an NX part of type .afm.
Use the
NXOpen.PartCollection
class to load or create a part.New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
BaseFEModel | Returns the femodel NXOpen.CAE.BaseFEModel associated with the part |
ComponentAssembly | Returns the component assembly. |
FieldManager | Returns the field main. |
FullPath | Returns the full path of the part. |
FullPathForAssociatedCadPart | Returns the full pathname of the associated cad part |
IsFullyLoaded | Returns the load status of a part. |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsReadOnly | Returns the read-only status of a part. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Leaf | Returns the leaf name of the part. |
MasterCadPart | Returns the master cad part associated with the assembly fem part |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PartPreviewMode | Returns or sets the preview mode |
PartUnits | Returns the units of the part file. |
Prototype | Returns the prototype of this object if it is an occurrence. |
SaveDisplayFacets | Returns or sets whether display quality facets are saved in the part file |
Tag | Returns the Tag for this object. |
UniqueIdentifier | Returns or sets the unique identifier for this part used to determine whether parts can be quietly substituted during part open. |
Methods¶
Method | Description |
---|---|
AssignPermanentName | Saves a temporary part with the given name. |
CanBeDisplayPart | Returns true if the part can be displayed and false if not displayed @return |
Close | Closes an open part. |
CompleteStructure | Make additions necessary to complete the incomplete assembly structure of the input part |
CreateDynamicSectionBuilder | Creates a NXOpen.Display.DynamicSectionBuilder The base part must be a displayable part, otherwise an exception will be thrown. |
CreateEffectivityConditionBuilder | Creates a NXOpen.EffectivityConditionBuilder @return |
CreateFacetSettingsBuilder | Creates a builder for the Facet Settings dialog @return |
CreateGatewayGroupBuilder | Creates a Groups builder @return GroupBuilder object |
CreateModelDisplayBuilder | Creates a builder for model display controls command @return |
CreatePerspectiveOptionsBuilder | Creates a builder for the Perspective Options dialog @return |
CreateReferenceSet | Creates a NXOpen.ReferenceSet object @return New reference set object |
CreateSolverAppendOption | Returns a solver append option object for importing the solver specific data into an existing NXOpen.CAE.FemPart or NXOpen.CAE.SimPart . |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteReferenceSet | Deletes a NXOpen.ReferenceSet object |
DeleteSolverAppendOption | Deletes a solver append option object for importing the solver specific data into an existing NXOpen.CAE.FemPart or NXOpen.CAE.SimPart . |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
ExportJt | Exports JT file |
ExportSimulation | Exports the Simulation data for a NXOpen.CAE.CaePart . |
FinalizeCreation | Finalizes the creation of the assembly fem part file. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAbstractionType | Gets axisymmetric abstraction type assoicated with the BaseFem part @return the axisymmetric abstraction type. |
GetAllReferenceSets | Get all the NXOpen.ReferenceSet objects in this part. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCollaborativeContentType | The collaborative content type of this part. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetCsysFlattenedLabel | Gets the resolved label of csys in cae part. |
GetDescription | Gets the description assoicated with the Cae part |
GetEnableMeshMorph | Gets the enable mesh morphing flag @return Flag to determine whether the mesh morphing is enabled |
GetHistoryInformation | Get history of part @return list of history data for the part. |
GetIncompleteStatus | Inquire whether the provided part is flagged as being incomplete @return |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetMakeUniqueName | Gets the Unique name on a part for the Make Unique operation @return |
GetPreviewImage | Get the preview image This will return the graphic preview image of the part (when available). |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSolverAndAnalysisType | Gets solver and analysis type assoicated with the BaseFem part |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetTransientStatus | Inquire whether the provided part is flagged as being transient @return |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
ImportExistingSimulation | Imports the solver specific data into an existing NXOpen.CAE.FemPart or NXOpen.CAE.SimPart . |
LoadFeatureDataForSelection | Ensure that feature data is loaded for a part. |
LoadFully | Ensures that this part is fully loaded. |
LoadThisPartFully | Ensures that this part is fully loaded. |
NewBeamSectionOffsetOptions | Creates a NXOpen.CAE.BeamSectionOffsetOptions @return |
NewBeamSectionOptions | Creates a NXOpen.CAE.BeamSectionOptions @return the syncrhonize options object created |
NewBeamSectionOrientationOptions | Creates a NXOpen.CAE.BeamSectionOrientationOptions @return |
NewMaterialOptions | Creates a NXOpen.CAE.MaterialOptions @return the material options object created |
Prints a representation of this object to the system log file. | |
RegenerateDisplayFacets | Regenerates display specific cached facets in the part. |
ReinstateTransience | Reinstate the transient status to the formerly transient input part |
RemoveTransience | Remove the transient status from the input part |
Reopen | Reopens a loaded part. |
ReopenAs | Reopens a loaded part. |
ReverseBlankAll | Reverse blank all the objects in the part. |
Save | Saves the part whether it is modified or not. |
SaveAs | Creates copy of target part. |
SaveBookmark | Saves a bookmark file. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetDescription | Sets the description assoicated with the Cae part |
SetEnableMeshMorph | Sets the enable mesh morphing flag |
SetMakeUniqueName | Sets the unique name on part for the Make Unique operation |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetSolverAndAnalysisType | Sets solver and analysis type assoicated with the BaseFem part. |
SetSolverAndAnalysisTypeAndAbstraction | Sets solver and analysis type and axisymmetric abstraction associated with the BaseFem part |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
IsOccurrence¶
-
AssyFemPart.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
AssyFemPart.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
MasterCadPart¶
-
AssyFemPart.
MasterCadPart
¶ Returns the master cad part associated with the assembly fem part
-------------------------------------
Getter Method
Signature
MasterCadPart()
Returns: Master CAD part associated to the fem part Return type: NXOpen.Part
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Name¶
-
AssyFemPart.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
AssyFemPart.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
AssyFemPart.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
AssyFemPart.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
FinalizeCreation¶
-
AssyFemPart.
FinalizeCreation
¶ Overloaded method FinalizeCreation
FinalizeCreation(cadPart, solverTypeName, analysisTypeType, abstractionType, description)
FinalizeCreation(cadPart, solverTypeName, analysisTypeType, description)
-------------------------------------
Finalizes the creation of the assembly fem part file. This method should be called immediately after creating the assembly fem part file. This method should be called only once for each assembly fem part file. The second call to the method will raise an error.
Signature
FinalizeCreation(cadPart, solverTypeName, analysisTypeType, abstractionType, description)
Parameters: - cadPart (
NXOpen.Part
) – the cad part to be associated with the fem part - solverTypeName (str) – the name of the solver. Refer to NX help for more information NOTE: The full Unicode character set is not supported for this parameter.
- analysisTypeType (str) – the name of the analysis type. Refer to NX help for more information NOTE: The full Unicode character set is not supported for this parameter.
- abstractionType (
NXOpen.CAE.BaseFemPartAxisymAbstractionType
) – the axisymmetric abstraction type. Refer to NX help for more information - description (list of str) – description NOTE: The full Unicode character set is not supported for this parameter.
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Finalizes the creation of the assembly fem part file. This method should be called immediately after creating the assembly fem part file. This method should be called only once for each assembly fem part file. The second call to the method will raise an error. Axisymmetric abstraction type is set internally using pre-nx9 techniques using solver name and analysis type.
Signature
FinalizeCreation(cadPart, solverTypeName, analysisTypeType, description)
Parameters: - cadPart (
NXOpen.Part
) – the cad part to be associated with the fem part - solverTypeName (str) – the name of the solver. Refer to NX help for more information NOTE: The full Unicode character set is not supported for this parameter.
- analysisTypeType (str) – the name of the analysis type. Refer to NX help for more information NOTE: The full Unicode character set is not supported for this parameter.
- description (list of str) – description NOTE: The full Unicode character set is not supported for this parameter.
New in version NX6.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.CAE.AssyFemPart.FinalizeCreation
that includes abstraction type instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
FindObject¶
-
AssyFemPart.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
AssyFemPart.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
AssyFemPart.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.