MaterialOptions Class¶
-
class
NXOpen.CAE.
MaterialOptions
¶ Bases:
NXOpen.TransientObject
Represents the material options to be used when assigning a material to cae part
To create a new instance of this class, use
NXOpen.CAE.CaePart.NewMaterialOptions
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Material | Returns or sets |
MaterialInherited | Returns or sets |
Property Detail¶
Material¶
-
MaterialOptions.
Material
¶ Returns or sets
-------------------------------------
Getter Method
Signature
Material()
Returns: Return type: NXOpen.PhysicalMaterial
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Material(material)
Parameters: material ( NXOpen.PhysicalMaterial
) –New in version NX5.0.0.
License requirements: None.
MaterialInherited¶
-
MaterialOptions.
MaterialInherited
¶ Returns or sets
-------------------------------------
Getter Method
Signature
MaterialInherited()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaterialInherited(bInherited)
Parameters: bInherited (bool) – New in version NX5.0.0.
License requirements: None.