BeamSectionOrientationOptions Class¶
-
class
NXOpen.CAE.
BeamSectionOrientationOptions
¶ Bases:
NXOpen.TransientObject
To create a new instance of this class, use
NXOpen.CAE.CaePart.NewBeamSectionOrientationOptions
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
DirectionType | Returns or sets the direction type |
MethodType | Returns or sets the orientation definition method |
Node | Returns or sets the node used to orient beam. |
OrientedElement | Returns or sets the element to be oriented. |
Vector | Returns or sets the orientation vector. |
Enumerations¶
BeamSectionOrientationOptionsMethod Enumeration | Represents the orientation definition method |
Property Detail¶
DirectionType¶
-
BeamSectionOrientationOptions.
DirectionType
¶ Returns or sets the direction type
-------------------------------------
Getter Method
Signature
DirectionType()
Returns: Return type: NXOpen.CAE.BeamSectionDirectionOption
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DirectionType(directionType)
Parameters: directionType ( NXOpen.CAE.BeamSectionDirectionOption
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
MethodType¶
-
BeamSectionOrientationOptions.
MethodType
¶ Returns or sets the orientation definition method
-------------------------------------
Getter Method
Signature
MethodType()
Returns: Return type: NXOpen.CAE.BeamSectionOrientationOptionsMethod
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MethodType(methodType)
Parameters: methodType ( NXOpen.CAE.BeamSectionOrientationOptionsMethod
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Node¶
-
BeamSectionOrientationOptions.
Node
¶ Returns or sets the node used to orient beam.
Only available when the orientation method is
CAE.BeamSectionOrientationOptionsMethod.ByNode
-------------------------------------
Getter Method
Signature
Node()
Returns: Return type: NXOpen.CAE.FENode
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Node(node)
Parameters: node ( NXOpen.CAE.FENode
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
OrientedElement¶
-
BeamSectionOrientationOptions.
OrientedElement
¶ Returns or sets the element to be oriented.
Only available when the orientation method is
CAE.BeamSectionOrientationOptionsMethod.ByVector
-------------------------------------
Getter Method
Signature
OrientedElement()
Returns: Return type: NXOpen.CAE.FEElement
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientedElement(orientedElement)
Parameters: orientedElement ( NXOpen.CAE.FEElement
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Vector¶
-
BeamSectionOrientationOptions.
Vector
¶ Returns or sets the orientation vector.
Only available when definition method is
CAE.BeamSectionOrientationOptionsMethod.ByVector
-------------------------------------
Getter Method
Signature
Vector()
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector(vector)
Parameters: vector ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)