FENode Class¶
-
class
NXOpen.CAE.
FENode
¶ Bases:
NXOpen.TaggedObject
,NXOpen.IFitTo
,NXOpen.CAE.IExportableFEEntity
Represents a Finite Element Node.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Coordinates | Returns the node cooridnates in absolute space |
DisplacementCsys | Returns the nodes displacement coordinate system or None if it is the absolute coordinate system |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Label | Returns the node label |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
ReferenceCsys | Returns the nodes reference coordinate system or None if it is the absolute coordinate system |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetElements | Returns the elements which refer to this node @return |
GetSolverCardSyntax | Returns the solver card syntax strings for this entity. |
Prints a representation of this object to the system log file. | |
SetName | Sets the custom name of the object. |
Property Detail¶
Coordinates¶
-
FENode.
Coordinates
¶ Returns the node cooridnates in absolute space
-------------------------------------
Getter Method
Signature
Coordinates()
Returns: Return type: NXOpen.Point3d
New in version NX7.5.2.
License requirements: None.
DisplacementCsys¶
-
FENode.
DisplacementCsys
¶ Returns the nodes displacement coordinate system or None if it is the absolute coordinate system
-------------------------------------
Getter Method
Signature
DisplacementCsys()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX7.5.2.
License requirements: None.
IsOccurrence¶
-
FENode.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
FENode.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Label¶
-
FENode.
Label
¶ Returns the node label
-------------------------------------
Getter Method
Signature
Label()
Returns: Return type: int New in version NX7.5.2.
License requirements: None.
Name¶
-
FENode.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
FENode.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
FENode.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
FENode.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
ReferenceCsys¶
-
FENode.
ReferenceCsys
¶ Returns the nodes reference coordinate system or None if it is the absolute coordinate system
-------------------------------------
Getter Method
Signature
ReferenceCsys()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX7.5.2.
License requirements: None.
Method Detail¶
FindObject¶
-
FENode.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetElements¶
-
FENode.
GetElements
¶ Returns the elements which refer to this node
Signature
GetElements()
Returns: Return type: list of NXOpen.CAE.FEElement
New in version NX7.5.2.
License requirements: None.
GetSolverCardSyntax¶
-
FENode.
GetSolverCardSyntax
¶ Returns the solver card syntax strings for this entity.
Signature
GetSolverCardSyntax()
Returns: Return type: list of str New in version NX8.5.0.
License requirements: None.
Print¶
-
FENode.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
FENode.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.