BeamSectionOptions Class¶
-
class
NXOpen.CAE.
BeamSectionOptions
¶ Bases:
NXOpen.TransientObject
Represents the synchronize options to be used when a FEM part is created These options will be used to synchronize the specified entities from the master CAD part file to the FEM part file
To create a new instance of this class, use
NXOpen.CAE.CaePart.NewBeamSectionOptions
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BeamAftSection | Returns or sets the section of aft beam end |
BeamForeSection | Returns or sets the section of fore beam end |
BeamSectionTapered | Returns or sets the flag indicating whether the beam section is tapered |
BeamSectionTaperedChaining | Returns or sets the flag indicating whether the beam section is in tapered chaining |
Property Detail¶
BeamAftSection¶
-
BeamSectionOptions.
BeamAftSection
¶ Returns or sets the section of aft beam end
-------------------------------------
Getter Method
Signature
BeamAftSection()
Returns: Return type: NXOpen.CAE.BeamSection
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BeamAftSection(beamSection)
Parameters: beamSection ( NXOpen.CAE.BeamSection
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
BeamForeSection¶
-
BeamSectionOptions.
BeamForeSection
¶ Returns or sets the section of fore beam end
-------------------------------------
Getter Method
Signature
BeamForeSection()
Returns: Return type: NXOpen.CAE.BeamSection
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BeamForeSection(beamSection)
Parameters: beamSection ( NXOpen.CAE.BeamSection
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
BeamSectionTapered¶
-
BeamSectionOptions.
BeamSectionTapered
¶ Returns or sets the flag indicating whether the beam section is tapered
-------------------------------------
Getter Method
Signature
BeamSectionTapered()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BeamSectionTapered(bTapered)
Parameters: bTapered (bool) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
BeamSectionTaperedChaining¶
-
BeamSectionOptions.
BeamSectionTaperedChaining
¶ Returns or sets the flag indicating whether the beam section is in tapered chaining
-------------------------------------
Getter Method
Signature
BeamSectionTaperedChaining()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BeamSectionTaperedChaining(bTaperedChaining)
Parameters: bTaperedChaining (bool) – New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)