Part Class¶
-
class
NXOpen.
Part
¶ Bases:
NXOpen.BasePart
Represents an NX part of type .prt.
Use the
NXOpen.PartCollection
class to load or create a part.New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
CAMSetup | Returns the CAM setup of the work part |
ComponentAssembly | Returns the component assembly. |
CurrentFeature | Returns the current feature. |
FieldManager | Returns the field main. |
FullPath | Returns the full path of the part. |
HasReuseTemplate | Returns the indicator that the part contains a reuse template. |
InspectionSetup | Returns the CMM Inspection setup of the work part |
IsBookletPart | Returns the status on whether input part is bookletPart or not a bookletPart. |
IsFullyLoaded | Returns the load status of a part. |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsReadOnly | Returns the read-only status of a part. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
KinematicConfigurator | Returns the NXOpen.SIM.KinematicConfigurator instance of the work part |
Leaf | Returns the leaf name of the part. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PartPreviewMode | Returns or sets the preview mode |
PartUnits | Returns the units of the part file. |
Prototype | Returns the prototype of this object if it is an occurrence. |
SaveDisplayFacets | Returns or sets whether display quality facets are saved in the part file |
Tag | Returns the Tag for this object. |
UniqueIdentifier | Returns or sets the unique identifier for this part used to determine whether parts can be quietly substituted during part open. |
Methods¶
Method | Description |
---|---|
AssignPermanentName | Saves a temporary part with the given name. |
CanBeDisplayPart | Returns true if the part can be displayed and false if not displayed @return |
Close | Closes an open part. |
CompleteStructure | Make additions necessary to complete the incomplete assembly structure of the input part |
ConvertPreNX9CompoundWelds | Convert any existing pre-NX9 Compound Weld User Defined Objects to NX features. |
CreateBoundingObjectBuilder | Creates an NXOpen.GeometricUtilities.BoundingObjectBuilder object. |
CreateCamSetup | Creates CAM setup @return the created cam setup |
CreateDynamicSectionBuilder | Creates a NXOpen.Display.DynamicSectionBuilder The base part must be a displayable part, otherwise an exception will be thrown. |
CreateEffectivityConditionBuilder | Creates a NXOpen.EffectivityConditionBuilder @return |
CreateEmptyBlendSetbackBuilder | Creates a NXOpen.GeometricUtilities.BlendSetbackBuilder object @return New empty object |
CreateEmptyBoundaryDefinitionBuilder | Creates boundary definition builder object @return |
CreateEmptyExpressionCollectorSet | Creates an empty ExpressionCollectorSet item @return New ExpressionCollectorSet object |
CreateEmptyExpressionSectionSet | Creates an empty ExpressionSectionSet item @return New ExpressionSectionSet object |
CreateEmptyRegionPoint | Creates an empty item that contains a point and its corresponding body context for a region @return New empty Region point object |
CreateEmptyTransitionCurveBuilder | Creates a NXOpen.GeometricUtilities.TransitionCurveBuilder object @return New empty object |
CreateEmptyTwoExpressionsCollectorSet | Creates an empty TwoExpressionCollectorSet item that contains a NXOpen.ScCollector collection and two corresponding expressions @return New TwoExpressionsCollectorSet object |
CreateEmptyTwoExpressionsSectionSet | Creates an empty TwoExpressionSectionSet item that contains a NXOpen.Section section and two corresponding expressions @return New TwoExpressionsSectionSet object |
CreateExpressionCollectorSet | Creates an ExpressionCollectorSet item that contains a NXOpen.ScCollector collection and a corresponding expression @return New ExpressionCollectorSet object |
CreateExpressionSectionSet | Creates an ExpressionSectionSet item that contains a NXOpen.Section collection and a corresponding expression @return New ExpressionSectionSet object |
CreateFacetSettingsBuilder | Creates a builder for the Facet Settings dialog @return |
CreateGatewayGroupBuilder | Creates a Groups builder @return GroupBuilder object |
CreateInspectionSetup | Creates CMM Inspection setup @return the created CMM Inspection setup |
CreateKinematicConfigurator | Create an instance of NXOpen.SIM.KinematicConfigurator class that will be used to manage all Machine tool Builder and Configurator objects @return The new Machine Tool Configurator |
CreateObjectList | Creates an empty list that can be populated with any NXObject @return ObjectList object |
CreatePartFamily | Create a part family of the part. |
CreatePerspectiveOptionsBuilder | Creates a builder for the Perspective Options dialog @return |
CreatePointSetAlignmentBuilder | Creates point set alignment builder object @return |
CreatePointsFromFileBuilder | Creates a NXOpen.GeometricUtilities.PointsFromFileBuilder object @return New empty object |
CreateReferenceSet | Creates a NXOpen.ReferenceSet object @return New reference set object |
CreateRegionPoint | Creates an item that contains a point and its corresponding body context for a region @return Region point object |
CreateSelectionList | Creates a NXOpen.GeometricUtilities.SelectionList object. |
CreateTwoExpressionsCollectorSet | Creates an TwoExpressionCollectorSet item that contains a NXOpen.ScCollector collection and two corresponding expressions @return New TwoExpressionsCollectorSet object |
CreateTwoExpressionsSectionSet | Creates an TwoExpressionSectionSet item that contains a NXOpen.Section section and two corresponding expressions @return New TwoExpressionsSectionSet object |
CreateWavelinkRepository | Create the link repository to handle interpart selection @return |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteCamSetup | Delete CAM setup |
DeleteInspectionSetup | Delete CMM Inspection setup |
DeleteReferenceSet | Deletes a NXOpen.ReferenceSet object |
DeleteRetainedDraftingObjectsInCurrentLayout | Deletes all retained drafting objects in the current layout of part that are currently in the retained state. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAllReferenceSets | Get all the NXOpen.ReferenceSet objects in this part. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCollaborativeContentType | The collaborative content type of this part. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetFamilyInstance | Obtains the NXOpen.PartFamily.Instance from part. |
GetHistoryInformation | Get history of part @return list of history data for the part. |
GetIncompleteStatus | Inquire whether the provided part is flagged as being incomplete @return |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetInterpartChildren | Returns a list of child parts in the current session that contain interpart geometry. |
GetInterpartParents | Returns a list of parts in the current session that contain the defining geometry for linked geometry in this part. |
GetMakeUniqueName | Gets the Unique name on a part for the Make Unique operation @return |
GetPartFamilyManager | Create an instance of a NXOpen.PartFamilyManager class that will be used to edit part family of the part. |
GetPreviewImage | Get the preview image This will return the graphic preview image of the part (when available). |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetTransientStatus | Inquire whether the provided part is flagged as being transient @return |
GetUpdateStatusReport | Get feature update status report @return list of affected features |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
LoadFeatureDataForSelection | Ensure that feature data is loaded for a part. |
LoadFully | Ensures that this part is fully loaded. |
LoadThisPartFully | Ensures that this part is fully loaded. |
MakeAllFeaturesInactive | Makes all the features of the part inactive |
MakeNoPartModuleActive | Deactivates any part module that is active in the given part. |
NewPartFamilyMemberData | Create an instance of a NXOpen.PartFamilyMemberData class that will be used to store the member count and member values of each member. |
NewPartFamilyMemberValues | Create an instance of a NXOpen.PartFamilyMemberValues class that will be used to store the attribute values of a member. |
NewPartFamilyTemplateManager | Creates an instance of a NXOpen.PartFamily.TemplateManager class that will be used to manage part family associated with this part @return |
Prints a representation of this object to the system log file. | |
RegenerateDisplayFacets | Regenerates display specific cached facets in the part. |
ReinstateTransience | Reinstate the transient status to the formerly transient input part |
RemoveTransience | Remove the transient status from the input part |
Reopen | Reopens a loaded part. |
ReopenAs | Reopens a loaded part. |
ResetTimestampToLatestFeature | Sets the timestamp for the part to the timestamp of the latest feature in the part. |
ReverseBlankAll | Reverse blank all the objects in the part. |
Save | Saves the part whether it is modified or not. |
SaveAs | Creates copy of target part. |
SaveBookmark | Saves a bookmark file. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetMakeUniqueName | Sets the unique name on part for the Make Unique operation |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
PartPartFamilyAttrType Enumeration | The part family attribute types. |
PartRelations Enumeration | The relations of the part file. |
PartUnits Enumeration | The units of the part file. |
Structs¶
PartFeatureUpdateStatus_Struct Struct | Contains feature update status report |
PartPartFamilyAttributeData_Struct Struct | Contains part family attributes information |
Property Detail¶
CAMSetup¶
-
Part.
CAMSetup
¶ Returns the CAM setup of the work part
-------------------------------------
Getter Method
Signature
CAMSetup()
Returns: the cam setup of the part Return type: NXOpen.CAM.CAMSetup
New in version NX4.0.0.
License requirements: cam_base (“CAM BASE”)
CurrentFeature¶
-
Part.
CurrentFeature
¶ Returns the current feature.
-------------------------------------
Getter Method
Signature
CurrentFeature()
Returns: Return type: NXOpen.Features.Feature
New in version NX3.0.0.
License requirements: None.
HasReuseTemplate¶
-
Part.
HasReuseTemplate
¶ Returns the indicator that the part contains a reuse template.
-------------------------------------
Getter Method
Signature
HasReuseTemplate()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
InspectionSetup¶
-
Part.
InspectionSetup
¶ Returns the CMM Inspection setup of the work part
-------------------------------------
Getter Method
Signature
InspectionSetup()
Returns: the CMM Inspection setup of the part Return type: NXOpen.CAM.InspectionSetup
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IsBookletPart¶
-
Part.
IsBookletPart
¶ Returns the status on whether input part is bookletPart or not a bookletPart.
-------------------------------------
Getter Method
Signature
IsBookletPart()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
IsOccurrence¶
-
Part.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Part.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
KinematicConfigurator¶
-
Part.
KinematicConfigurator
¶ Returns the
NXOpen.SIM.KinematicConfigurator
instance of the work part-------------------------------------
Getter Method
Signature
KinematicConfigurator()
Returns: The Machine Tool Configurator of the work part Return type: NXOpen.SIM.KinematicConfigurator
New in version NX7.5.0.
License requirements: None.
Name¶
-
Part.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Part.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Part.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
Part.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
ConvertPreNX9CompoundWelds¶
-
Part.
ConvertPreNX9CompoundWelds
¶ Convert any existing pre-NX9 Compound Weld User Defined Objects to NX features.
Signature
ConvertPreNX9CompoundWelds()
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CreateBoundingObjectBuilder¶
-
Part.
CreateBoundingObjectBuilder
¶ Creates an
NXOpen.GeometricUtilities.BoundingObjectBuilder
object.Signature
CreateBoundingObjectBuilder()
Returns: Return type: NXOpen.GeometricUtilities.BoundingObjectBuilder
New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CreateCamSetup¶
-
Part.
CreateCamSetup
¶ Creates CAM setup
Signature
CreateCamSetup(templateName)
Parameters: templateName (str) – the name of the template type NOTE: The full Unicode character set is not supported for this parameter. Returns: the created cam setup Return type: NXOpen.CAM.CAMSetup
New in version NX4.0.0.
License requirements: cam_base (“CAM BASE”)
CreateEmptyBlendSetbackBuilder¶
-
Part.
CreateEmptyBlendSetbackBuilder
¶ Creates a
NXOpen.GeometricUtilities.BlendSetbackBuilder
objectSignature
CreateEmptyBlendSetbackBuilder()
Returns: New empty object Return type: NXOpen.GeometricUtilities.BlendSetbackBuilder
New in version NX9.0.0.
License requirements: None.
CreateEmptyBoundaryDefinitionBuilder¶
-
Part.
CreateEmptyBoundaryDefinitionBuilder
¶ Creates boundary definition builder object
Signature
CreateEmptyBoundaryDefinitionBuilder()
Returns: Return type: NXOpen.GeometricUtilities.BoundaryDefinitionBuilder
New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
CreateEmptyExpressionCollectorSet¶
-
Part.
CreateEmptyExpressionCollectorSet
¶ Creates an empty ExpressionCollectorSet item
Signature
CreateEmptyExpressionCollectorSet()
Returns: New ExpressionCollectorSet object Return type: NXOpen.ExpressionCollectorSet
New in version NX5.0.0.
License requirements: None.
CreateEmptyExpressionSectionSet¶
-
Part.
CreateEmptyExpressionSectionSet
¶ Creates an empty ExpressionSectionSet item
Signature
CreateEmptyExpressionSectionSet()
Returns: New ExpressionSectionSet object Return type: NXOpen.ExpressionSectionSet
New in version NX5.0.0.
License requirements: None.
CreateEmptyRegionPoint¶
-
Part.
CreateEmptyRegionPoint
¶ Creates an empty item that contains a point and its corresponding body context for a region
Signature
CreateEmptyRegionPoint()
Returns: New empty Region point object Return type: NXOpen.RegionPoint
New in version NX5.0.0.
License requirements: None.
CreateEmptyTransitionCurveBuilder¶
-
Part.
CreateEmptyTransitionCurveBuilder
¶ Creates a
NXOpen.GeometricUtilities.TransitionCurveBuilder
objectSignature
CreateEmptyTransitionCurveBuilder()
Returns: New empty object Return type: NXOpen.GeometricUtilities.TransitionCurveBuilder
New in version NX9.0.0.
License requirements: None.
CreateEmptyTwoExpressionsCollectorSet¶
-
Part.
CreateEmptyTwoExpressionsCollectorSet
¶ Creates an empty TwoExpressionCollectorSet item that contains a
NXOpen.ScCollector
collection and two corresponding expressionsSignature
CreateEmptyTwoExpressionsCollectorSet()
Returns: New TwoExpressionsCollectorSet object Return type: NXOpen.GeometricUtilities.TwoExpressionsCollectorSet
New in version NX8.5.0.
License requirements: None.
CreateEmptyTwoExpressionsSectionSet¶
-
Part.
CreateEmptyTwoExpressionsSectionSet
¶ Creates an empty TwoExpressionSectionSet item that contains a
NXOpen.Section
section and two corresponding expressionsSignature
CreateEmptyTwoExpressionsSectionSet()
Returns: New TwoExpressionsSectionSet object Return type: NXOpen.GeometricUtilities.TwoExpressionsSectionSet
New in version NX9.0.0.
License requirements: None.
CreateExpressionCollectorSet¶
-
Part.
CreateExpressionCollectorSet
¶ Creates an ExpressionCollectorSet item that contains a
NXOpen.ScCollector
collection and a corresponding expressionSignature
CreateExpressionCollectorSet(collector, value, unitsType, index)
Parameters: - collector (
NXOpen.ScCollector
) – Selection object - value (str) – initial expression string
- unitsType (str) – units of expression
- index (int) – This parameter has no effect, and is ignored
Returns: New ExpressionCollectorSet object
Return type: New in version NX5.0.0.
License requirements: None.
- collector (
CreateExpressionSectionSet¶
-
Part.
CreateExpressionSectionSet
¶ Creates an ExpressionSectionSet item that contains a
NXOpen.Section
collection and a corresponding expressionSignature
CreateExpressionSectionSet(section, value, unitsType, index)
Parameters: - section (
NXOpen.Section
) – Section object - value (str) – initial expression string
- unitsType (str) – units of expression
- index (int) – This parameter has no effect, and is ignored
Returns: New ExpressionSectionSet object
Return type: New in version NX5.0.0.
License requirements: None.
- section (
CreateInspectionSetup¶
-
Part.
CreateInspectionSetup
¶ Creates CMM Inspection setup
Signature
CreateInspectionSetup(templateName)
Parameters: templateName (str) – the name of the template type NOTE: The full Unicode character set is not supported for this parameter. Returns: the created CMM Inspection setup Return type: NXOpen.CAM.InspectionSetup
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CreateKinematicConfigurator¶
-
Part.
CreateKinematicConfigurator
¶ Create an instance of
NXOpen.SIM.KinematicConfigurator
class that will be used to manage all Machine tool Builder and Configurator objectsSignature
CreateKinematicConfigurator()
Returns: The new Machine Tool Configurator Return type: NXOpen.SIM.KinematicConfigurator
New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”) OR resource_manager_nx (“Teamcenter Resource Manager”)
CreateObjectList¶
-
Part.
CreateObjectList
¶ Creates an empty list that can be populated with any NXObject
Signature
CreateObjectList()
Returns: ObjectList object Return type: NXOpen.ObjectList
New in version NX4.0.0.
License requirements: None.
CreatePartFamily¶
-
Part.
CreatePartFamily
¶ Create a part family of the part.
Signature
CreatePartFamily(attributeData, memberData)
Parameters: - attributeData (list of
NXOpen.PartPartFamilyAttributeData_Struct
) – the attributes data - memberData (
NXOpen.PartFamilyMemberData
) – the member data
Returns: the new
NXOpen.PartFamilyManager
instanceReturn type: New in version NX6.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.PartFamily.TemplateManager.CreatePartFamily
insteadLicense requirements: None.
- attributeData (list of
CreatePointSetAlignmentBuilder¶
-
Part.
CreatePointSetAlignmentBuilder
¶ Creates point set alignment builder object
Signature
CreatePointSetAlignmentBuilder()
Returns: Return type: NXOpen.GeometricUtilities.PointSetAlignmentBuilder
New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
CreatePointsFromFileBuilder¶
-
Part.
CreatePointsFromFileBuilder
¶ Creates a
NXOpen.GeometricUtilities.PointsFromFileBuilder
objectSignature
CreatePointsFromFileBuilder()
Returns: New empty object Return type: NXOpen.GeometricUtilities.PointsFromFileBuilder
New in version NX8.5.0.
License requirements: None.
CreateRegionPoint¶
-
Part.
CreateRegionPoint
¶ Creates an item that contains a point and its corresponding body context for a region
Signature
CreateRegionPoint(point, body)
Parameters: - point (
NXOpen.Point
) – Point object - body (
NXOpen.Body
) – Body context object for point
Returns: Region point object
Return type: New in version NX5.0.0.
License requirements: None.
- point (
CreateSelectionList¶
-
Part.
CreateSelectionList
¶ Creates a
NXOpen.GeometricUtilities.SelectionList
object.Signature
CreateSelectionList()
Returns: Return type: NXOpen.GeometricUtilities.SelectionList
New in version NX8.0.0.
License requirements: None.
CreateTwoExpressionsCollectorSet¶
-
Part.
CreateTwoExpressionsCollectorSet
¶ Creates an TwoExpressionCollectorSet item that contains a
NXOpen.ScCollector
collection and two corresponding expressionsSignature
CreateTwoExpressionsCollectorSet(collector, value, valueTwo, unitsType, index)
Parameters: - collector (
NXOpen.ScCollector
) – Selection object - value (str) – initial expression string
- valueTwo (str) – initial expression string for second expression
- unitsType (str) – units of expression
- index (int) – This parameter has no effect, and is ignored
Returns: New TwoExpressionsCollectorSet object
Return type: New in version NX8.5.0.
License requirements: None.
- collector (
CreateTwoExpressionsSectionSet¶
-
Part.
CreateTwoExpressionsSectionSet
¶ Creates an TwoExpressionSectionSet item that contains a
NXOpen.Section
section and two corresponding expressionsSignature
CreateTwoExpressionsSectionSet(section, value, valueTwo, unitsType, index)
Parameters: - section (
NXOpen.Section
) – Selection object - value (str) – initial expression string for first expression
- valueTwo (str) – initial expression string for second expression
- unitsType (str) – units of expression
- index (int) – This parameter has no effect, and is ignored
Returns: New TwoExpressionsSectionSet object
Return type: New in version NX9.0.0.
License requirements: None.
- section (
CreateWavelinkRepository¶
-
Part.
CreateWavelinkRepository
¶ Create the link repository to handle interpart selection
Signature
CreateWavelinkRepository()
Returns: Return type: NXOpen.GeometricUtilities.WaveLinkRepository
New in version NX6.0.0.
License requirements: None.
DeleteCamSetup¶
-
Part.
DeleteCamSetup
¶ Delete CAM setup
Signature
DeleteCamSetup()
New in version NX4.0.0.
License requirements: cam_base (“CAM BASE”)
DeleteInspectionSetup¶
-
Part.
DeleteInspectionSetup
¶ Delete CMM Inspection setup
Signature
DeleteInspectionSetup()
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DeleteRetainedDraftingObjectsInCurrentLayout¶
-
Part.
DeleteRetainedDraftingObjectsInCurrentLayout
¶ Deletes all retained drafting objects in the current layout of part that are currently in the “retained” state.
Signature
DeleteRetainedDraftingObjectsInCurrentLayout()
New in version NX3.0.0.
License requirements: None.
FindObject¶
-
Part.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetFamilyInstance¶
-
Part.
GetFamilyInstance
¶ Obtains the
NXOpen.PartFamily.Instance
from part.Signature
GetFamilyInstance()
Returns: Return type: NXOpen.PartFamily.Instance
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetInterpartChildren¶
-
Part.
GetInterpartChildren
¶ Returns a list of child parts in the current session that contain interpart geometry.
Signature
GetInterpartChildren()
Returns: Return type: list of NXOpen.Part
New in version NX3.0.0.
License requirements: None.
GetInterpartParents¶
-
Part.
GetInterpartParents
¶ Returns a list of parts in the current session that contain the defining geometry for linked geometry in this part.
Signature
GetInterpartParents()
Returns: Return type: list of NXOpen.Part
New in version NX3.0.0.
License requirements: None.
GetPartFamilyManager¶
-
Part.
GetPartFamilyManager
¶ Create an instance of a
NXOpen.PartFamilyManager
class that will be used to edit part family of the part.Signature
GetPartFamilyManager()
Returns: the new NXOpen.PartFamilyManager
instanceReturn type: NXOpen.PartFamilyManager
New in version NX6.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Part.NewPartFamilyTemplateManager
insteadLicense requirements: None.
GetUpdateStatusReport¶
-
Part.
GetUpdateStatusReport
¶ Get feature update status report
Signature
GetUpdateStatusReport()
Returns: a tuple Return type: A tuple consisting of (updateStatus, numFailed). updateStatus is a list of NXOpen.PartFeatureUpdateStatus_Struct
. list of affected features numFailed is a int. number of failed featuresNew in version NX3.0.0.
License requirements: None.
MakeAllFeaturesInactive¶
-
Part.
MakeAllFeaturesInactive
¶ Makes all the features of the part inactive
Signature
MakeAllFeaturesInactive()
New in version NX7.5.4.
License requirements: solid_modeling (“SOLIDS MODELING”)
MakeNoPartModuleActive¶
-
Part.
MakeNoPartModuleActive
¶ Deactivates any part module that is active in the given part.
Signature
MakeNoPartModuleActive()
New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
NewPartFamilyMemberData¶
-
Part.
NewPartFamilyMemberData
¶ Create an instance of a
NXOpen.PartFamilyMemberData
class that will be used to store the member count and member values of each member.Signature
NewPartFamilyMemberData()
Returns: the new NXOpen.PartFamilyMemberData
instanceReturn type: NXOpen.PartFamilyMemberData
New in version NX6.0.0.
Deprecated since version NX9.0.0: Create and use
NXOpen.PartFamily.InstanceDefinition
objects usingNXOpen.PartFamily.TemplateManager.AddInstanceDefinition
License requirements: None.
NewPartFamilyMemberValues¶
-
Part.
NewPartFamilyMemberValues
¶ Create an instance of a
NXOpen.PartFamilyMemberValues
class that will be used to store the attribute values of a member.Signature
NewPartFamilyMemberValues()
Returns: the new NXOpen.PartFamilyMemberValues
instanceReturn type: NXOpen.PartFamilyMemberValues
New in version NX6.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.PartFamily.InstanceDefinition
andNXOpen.PartFamily.InstanceDefinition.SetValueOfAttribute
License requirements: None.
NewPartFamilyTemplateManager¶
-
Part.
NewPartFamilyTemplateManager
¶ Creates an instance of a
NXOpen.PartFamily.TemplateManager
class that will be used to manage part family associated with this partSignature
NewPartFamilyTemplateManager()
Returns: Return type: NXOpen.PartFamily.TemplateManager
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Print¶
-
Part.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
ResetTimestampToLatestFeature¶
-
Part.
ResetTimestampToLatestFeature
¶ Sets the timestamp for the part to the timestamp of the latest feature in the part.
Use this when you have deleted the latest feature and you want to reuse the timestamp assigned to that feature
Signature
ResetTimestampToLatestFeature()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
Part.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.