LaminateSpreadsheetReportBuilderFilteringType Enumeration¶
NXOpen.CAE.LaminateSpreadsheetReportBuilder.FilteringType is an alias for NXOpen.CAE.LaminateSpreadsheetReportBuilderFilteringType
-
class
NXOpen.CAE.
LaminateSpreadsheetReportBuilderFilteringType
¶ Bases:
object
Filtering rule for the spreadsheet post report
Enum Members
Enum Member Enum Member Description None Don’t filter any valuesStressXX Filter values based on Stress XX componentStressYY Filter values based on Stress YY componentStressZZ Filter values based on Stress ZZ componentStressXY Filter values based on Stress XY componentStressZX Filter values based on Stress ZX componentStressYZ Filter values based on Stress YZ componentStressMaxP Filter values based on the maximum principal stressStressMinP Filter values based on the minimum principal stressStressMaxS Filter values based on the maximum shear stressStrainXX Filter values based on Strain XX componentStrainYY Filter values based on Strain YY componentStrainZZ Filter values based on Strain ZZ componentStrainXY Filter values based on Strain XY componentStrainZX Filter values based on Strain ZX componentStrainYZ Filter values based on Strain YZ componentStrainMaxP Filter values based on the maximum principal strainStrainMinP Filter values based on the minimum principal strainStrainMaxS Filter values based on the maximum shear strainPlyFailureIndex Filter values based on the ply failure indexPlyStrengthRatio Filter values based on the ply strength ratioPlyMarginofSafety Filter values based on the ply margin of safetyBondFailureIndex Filter values based on the bonding failure indexBondStrengthRatio Filter values based on the bonding strength ratioBondMarginofSafety Filter values based on the bonding margin of safety-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-