PreTestDofSetBuilder Class¶
-
class
NXOpen.CAE.
PreTestDofSetBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.PreTestDofSet
builderTo create a new instance of this class, use
NXOpen.CAE.PreTestSolutionCollection.CreatePretestDofsetBuilder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
DofSetSelect | Returns or sets the referrenced NXOpen.CAE.CaeDOFSet |
Nodes | Returns the selected nodes |
NodesEnabled | Returns or sets the manual selection toggle value |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DofSetSelect¶
-
PreTestDofSetBuilder.
DofSetSelect
¶ Returns or sets the referrenced
NXOpen.CAE.CaeDOFSet
-------------------------------------
Getter Method
Signature
DofSetSelect()
Returns: Return type: NXOpen.CAE.CaeDOFSet
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
-------------------------------------
Setter Method
Signature
DofSetSelect(dofSetSelect)
Parameters: dofSetSelect ( NXOpen.CAE.CaeDOFSet
) –New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
Nodes¶
-
PreTestDofSetBuilder.
Nodes
¶ Returns the selected nodes
-------------------------------------
Getter Method
Signature
Nodes()
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
NodesEnabled¶
-
PreTestDofSetBuilder.
NodesEnabled
¶ Returns or sets the manual selection toggle value
-------------------------------------
Getter Method
Signature
NodesEnabled()
Returns: Return type: bool New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
-------------------------------------
Setter Method
Signature
NodesEnabled(nodesEnabled)
Parameters: nodesEnabled (bool) – New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
Method Detail¶
Validate¶
-
PreTestDofSetBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.