PreTestSolutionCollection Class¶
-
class
NXOpen.CAE.
PreTestSolutionCollection
¶ Bases:
object
Represents a collection of pre-test setups
To obtain an instance of this class, refer to
NXOpen.CAE.CorrelManager
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
ActivePretest | Returns or sets the active pre-test |
Methods¶
Method | Description |
---|---|
ClonePretest | Clone a pre-test @return Cloned Pre-Test |
CreateAutoMacViewerBuilder | Creates an AutoMAC results display builder @return AutoMac Builder. |
CreateExciterConfigBuilder | Creates a exciter configuration dialog builder @return Exciter Configuration Builder. |
CreatePretestBuilder | Creates a pre-test dialog builder @return Pre-Test Builder |
CreatePretestDofsetBuilder | Creates a dof set dialog builder @return Dof Set Builder. |
CreateSensorConfigBuilder | Creates a sensor configuration dialog builder @return Sensor Configuration Builder. |
DeletePretest | Delete a pre-test |
FindObject | Finds a pre-test setup with specified name @return Pre-Test found |
Property Detail¶
ActivePretest¶
-
PreTestSolutionCollection.
ActivePretest
¶ Returns or sets the active pre-test
-------------------------------------
Getter Method
Signature
ActivePretest()
Returns: Active Pre-Test Return type: NXOpen.CAE.PreTestSolution
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActivePretest(pretest)
Parameters: pretest ( NXOpen.CAE.PreTestSolution
) – Pre-Test to be set activeNew in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
Method Detail¶
ClonePretest¶
-
PreTestSolutionCollection.
ClonePretest
¶ Clone a pre-test
Signature
ClonePretest(source)
Parameters: source ( NXOpen.CAE.PreTestSolution
) – Pre-Test to be clonedReturns: Cloned Pre-Test Return type: NXOpen.CAE.PreTestSolution
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
CreateAutoMacViewerBuilder¶
-
PreTestSolutionCollection.
CreateAutoMacViewerBuilder
¶ Creates an AutoMAC results display builder
Signature
CreateAutoMacViewerBuilder(macInput)
Parameters: macInput ( NXOpen.TaggedObject
) – Mac Input.Returns: AutoMac Builder. Return type: NXOpen.CAE.AutoMacViewerBuilder
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
CreateExciterConfigBuilder¶
-
PreTestSolutionCollection.
CreateExciterConfigBuilder
¶ Creates a exciter configuration dialog builder
Signature
CreateExciterConfigBuilder(exciterConfig)
Parameters: exciterConfig ( NXOpen.CAE.PreTestExciterConfig
) – Exciter Configuration being edited.Returns: Exciter Configuration Builder. Return type: NXOpen.CAE.PreTestExciterConfigBuilder
New in version NX8.0.0.
License requirements: nx_correl_base (“FE Correlation”)
CreatePretestBuilder¶
-
PreTestSolutionCollection.
CreatePretestBuilder
¶ Creates a pre-test dialog builder
Signature
CreatePretestBuilder(pretest)
Parameters: pretest ( NXOpen.CAE.PreTestSolution
) – Edited Pre-Test. Can be NULL if creating a new Pre-Test.Returns: Pre-Test Builder Return type: NXOpen.CAE.PreTestSolutionBuilder
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
CreatePretestDofsetBuilder¶
-
PreTestSolutionCollection.
CreatePretestDofsetBuilder
¶ Creates a dof set dialog builder
Signature
CreatePretestDofsetBuilder(dofset)
Parameters: dofset ( NXOpen.CAE.PreTestDofSet
) – Dof Set being edited.Returns: Dof Set Builder. Return type: NXOpen.CAE.PreTestDofSetBuilder
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
CreateSensorConfigBuilder¶
-
PreTestSolutionCollection.
CreateSensorConfigBuilder
¶ Creates a sensor configuration dialog builder
Signature
CreateSensorConfigBuilder(sensorConfig)
Parameters: sensorConfig ( NXOpen.CAE.PreTestSensorConfig
) – Sensor Configuration being edited.Returns: Sensor Configuration Builder. Return type: NXOpen.CAE.PreTestSensorConfigBuilder
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
DeletePretest¶
-
PreTestSolutionCollection.
DeletePretest
¶ Delete a pre-test
Signature
DeletePretest(pretest)
Parameters: pretest ( NXOpen.CAE.PreTestSolution
) – Pre-Test to be deletedNew in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
FindObject¶
-
PreTestSolutionCollection.
FindObject
¶ Finds a pre-test setup with specified name
Signature
FindObject(name)
Parameters: name (str) – Pre-Test name to be found Returns: Pre-Test found Return type: NXOpen.CAE.PreTestSolution
New in version NX7.5.0.
License requirements: None.