SimLoadRecipe Class¶
-
class
NXOpen.CAE.
SimLoadRecipe
¶ Bases:
NXOpen.TaggedObject
This is the class handling the attributes of a load recipe.
To create a new instance of this class, use
NXOpen.CAE.SimLoadRecipeCollection.Create
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
DataType | Returns the data type of a NXOpen.CAE.SimLoadRecipe |
Description | Returns or sets the description of a NXOpen.CAE.SimLoadRecipe . |
Name | Returns or sets the name of a NXOpen.CAE.SimLoadRecipe . |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Autofill | Fills the mapping tables of the load recipe based on available functions in the data sources. |
DisableLoadCondition | Disables a load condition in the Load Recipe. |
DisableTrackingValue | Disables a tracking value in the Load Recipe. |
EnableLoadCondition | Enables a load condition in the Load Recipe. |
EnableTrackingValue | Enables a tracking value in the Load Recipe. |
ExportToCSVFile | Exports mapping entries to a CSV file. |
GetLoadConditionHandlingType | Gets the type of load conditions handling of the NXOpen.CAE.SimLoadRecipe @return |
ImportFromCSVFile | Imports mapping entries from a CSV file. |
LoadLoadConditions | Loads all the load conditions available in the data sources and enables them. |
LoadTrackingValues | Loads all the tracking values available in the data sources and enables them. |
NewLbcGeneratorFromLoadRecipe | Creates a new NXOpen.CAE.SimLoadRecipeLbcGenerator . |
SetLoadConditionHandlingType | Sets the type of load conditions handling of the NXOpen.CAE.SimLoadRecipe |
Validation | Validation of the Load Recipe |
Property Detail¶
DataType¶
-
SimLoadRecipe.
DataType
¶ Returns the data type of a
NXOpen.CAE.SimLoadRecipe
-------------------------------------
Getter Method
Signature
DataType()
Returns: Return type: NXOpen.CAE.SimLoadRecipeTypesDataTypes
New in version NX10.0.0.
License requirements: None.
Description¶
-
SimLoadRecipe.
Description
¶ Returns or sets the description of a
NXOpen.CAE.SimLoadRecipe
.-------------------------------------
Getter Method
Signature
Description()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Description(description)
Parameters: description (str) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Name¶
-
SimLoadRecipe.
Name
¶ Returns or sets the name of a
NXOpen.CAE.SimLoadRecipe
.-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Autofill¶
-
SimLoadRecipe.
Autofill
¶ Fills the mapping tables of the load recipe based on available functions in the data sources.
Creates and adds
NXOpen.CAE.SimLoadRecipeMapEntry
instances to the load recipe. Sets the value ofNXOpen.CAE.SimLoadRecipeMapEntry.Target`
for each map entry to the entity label read from the data sources. This method doesn’t create entries withNXOpen.CAE.SimLoadRecipeMapEntry.TargetType`
which refer to groups or meshes.The parameters available in the data sources are filled for each entry in the following format: “ME:<ja_lt>target label<ja_gt>”.
Signature
Autofill()
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
DisableLoadCondition¶
-
SimLoadRecipe.
DisableLoadCondition
¶ Disables a load condition in the Load Recipe.
Disabled load conditions will not be used when creating a solution from load recipe.
Signature
DisableLoadCondition(loadCondition)
Parameters: loadCondition (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
DisableTrackingValue¶
-
SimLoadRecipe.
DisableTrackingValue
¶ Disables a tracking value in the Load Recipe.
Disabled tracking values will not be used when creating a solution from load recipe.
Signature
DisableTrackingValue(trackingValue)
Parameters: trackingValue (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EnableLoadCondition¶
-
SimLoadRecipe.
EnableLoadCondition
¶ Enables a load condition in the Load Recipe.
Only enabled load conditions will be used when creating a solution from load recipe.
Signature
EnableLoadCondition(loadCondition)
Parameters: loadCondition (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EnableTrackingValue¶
-
SimLoadRecipe.
EnableTrackingValue
¶ Enables a tracking value in the Load Recipe.
Only enabled tracking values will be used when creating a solution from load recipe.
Signature
EnableTrackingValue(trackingValue)
Parameters: trackingValue (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ExportToCSVFile¶
-
SimLoadRecipe.
ExportToCSVFile
¶ Exports mapping entries to a CSV file.
Signature
ExportToCSVFile(filePath)
Parameters: filePath (str) – Path of the CSV file NOTE: The full Unicode character set is not supported for this parameter. Returns: True if the mapping table entries contain the CSV delimiter character. If this is true, it will cause inconsistencies when importing the file. :rtype: bool
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetLoadConditionHandlingType¶
-
SimLoadRecipe.
GetLoadConditionHandlingType
¶ Gets the type of load conditions handling of the
NXOpen.CAE.SimLoadRecipe
Signature
GetLoadConditionHandlingType()
Returns: Return type: NXOpen.CAE.SimLoadRecipeTypesLoadConditionHandling
New in version NX10.0.0.
License requirements: None.
ImportFromCSVFile¶
-
SimLoadRecipe.
ImportFromCSVFile
¶ Imports mapping entries from a CSV file.
Signature
ImportFromCSVFile(filePath, csvDelim)
Parameters: - filePath (str) – Path of the CSV file NOTE: The full Unicode character set is not supported for this parameter.
- csvDelim (str) – Delimiter character used in the CSV file. If None, the comma character will be used. If this string contains more then one character, only the first one will be used. NOTE: The full Unicode character set is not supported for this parameter.
Returns: a tuple
Return type: A tuple consisting of (noParsedContent, invalidLoadType, invalidEntityType, invalidNbrOfParameters). noParsedContent is a bool. True if no valid data could be parsed from the file. invalidLoadType is a bool. True if an invalid load type was found. All data for this load type will be ignored. invalidEntityType is a bool. True if an invalid entity type was found. The entities with invalid entity type will be ignored. invalidNbrOfParameters is a bool. True if an invalid number of parameters was found for an entry. If the number of parameters is less then expected, it will populate the first values for which it has values. If the number of parameters is more then expected, the last values will be ignored.
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
LoadLoadConditions¶
-
SimLoadRecipe.
LoadLoadConditions
¶ Loads all the load conditions available in the data sources and enables them.
Signature
LoadLoadConditions()
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
LoadTrackingValues¶
-
SimLoadRecipe.
LoadTrackingValues
¶ Loads all the tracking values available in the data sources and enables them.
Signature
LoadTrackingValues()
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
NewLbcGeneratorFromLoadRecipe¶
-
SimLoadRecipe.
NewLbcGeneratorFromLoadRecipe
¶ Creates a new
NXOpen.CAE.SimLoadRecipeLbcGenerator
.Signature
NewLbcGeneratorFromLoadRecipe()
Returns: Return type: NXOpen.CAE.SimLoadRecipeLbcGenerator
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetLoadConditionHandlingType¶
-
SimLoadRecipe.
SetLoadConditionHandlingType
¶ Sets the type of load conditions handling of the
NXOpen.CAE.SimLoadRecipe
Signature
SetLoadConditionHandlingType(lcHandling)
Parameters: lcHandling ( NXOpen.CAE.SimLoadRecipeTypesLoadConditionHandling
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)