SimLoadRecipeMapEntry Class¶
-
class
NXOpen.CAE.
SimLoadRecipeMapEntry
¶ Bases:
NXOpen.TaggedObject
These objects represent one line in a
NXOpen.CAE.SimLoadRecipe
‘s mapping.Use CAE.SimLoadRecipeMapEntryCollection.Create
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
Target | Returns or sets the target of a NXOpen.CAE.SimLoadRecipeMapEntry . |
TargetType | Returns or sets the target type of a NXOpen.CAE.SimLoadRecipeMapEntry . |
Methods¶
Method | Description |
---|---|
GetParameters | Returns the parameters of a NXOpen.CAE.SimLoadRecipeMapEntry . |
SetParameters | Sets the parameters of a NXOpen.CAE.SimLoadRecipeMapEntry . |
Property Detail¶
Target¶
-
SimLoadRecipeMapEntry.
Target
¶ Returns or sets the target of a
NXOpen.CAE.SimLoadRecipeMapEntry
.The target value depends on the
NXOpen.CAE.SimLoadRecipeMapEntry.TargetType`
.It represents the followings:
- Node label if the target type is
CAE.SimLoadRecipeMapEntryTargetTypesTargetTypes.Node
- Element label and face index in the form “elem_label:face_index” if the target type is
CAE.SimLoadRecipeMapEntryTargetTypesTargetTypes.Face
- Name of a Mesh if the target type is
CAE.SimLoadRecipeMapEntryTargetTypesTargetTypes.NodeMesh
or
- Name of a Mesh if the target type is
CAE.SimLoadRecipeMapEntryTargetTypesTargetTypes.FaceMesh
- Name of a group if the target type is
CAE.SimLoadRecipeMapEntryTargetTypesTargetTypes.NodeGroup
or
- Name of a group if the target type is
CAE.SimLoadRecipeMapEntryTargetTypesTargetTypes.FaceGroup
-------------------------------------
Getter Method
Signature
Target()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Target(target)
Parameters: target (str) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
TargetType¶
-
SimLoadRecipeMapEntry.
TargetType
¶ Returns or sets the target type of a
NXOpen.CAE.SimLoadRecipeMapEntry
.-------------------------------------
Getter Method
Signature
TargetType()
Returns: Return type: NXOpen.CAE.SimLoadRecipeMapEntryTargetTypesTargetTypes
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetType(targetType)
Parameters: targetType ( NXOpen.CAE.SimLoadRecipeMapEntryTargetTypesTargetTypes
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
GetParameters¶
-
SimLoadRecipeMapEntry.
GetParameters
¶ Returns the parameters of a
NXOpen.CAE.SimLoadRecipeMapEntry
.Signature
GetParameters()
Returns: Return type: list of str New in version NX10.0.0.
License requirements: None.
SetParameters¶
-
SimLoadRecipeMapEntry.
SetParameters
¶ Sets the parameters of a
NXOpen.CAE.SimLoadRecipeMapEntry
.The size of parameters array and the value of numParameters must be equal to the current number of parameters of the entry.
Signature
SetParameters(parameters)
Parameters: parameters (list of str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)