SimLoadRecipeCollection Class¶
-
class
NXOpen.CAE.
SimLoadRecipeCollection
¶ Bases:
object
This class is a collection of
NXOpen.CAE.SimLoadRecipe
.To obtain an instance of this class, refer to
NXOpen.CAE.SimSimulation
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
Copy | Copies a Load Recipe with all attributes and add it to the collection. |
Create | Creates a new Load Recipe and adds it to the collection. |
Delete | Delete a list of load recipes |
Find | Finds a Load Recipe with a specified name. |
Method Detail¶
Copy¶
-
SimLoadRecipeCollection.
Copy
¶ Copies a Load Recipe with all attributes and add it to the collection.
This method gives proper unique name to the created Load Recipe.
Signature
Copy(recipeToCopy)
Parameters: recipeToCopy ( NXOpen.CAE.SimLoadRecipe
) –Returns: Return type: NXOpen.CAE.SimLoadRecipe
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Create¶
-
SimLoadRecipeCollection.
Create
¶ Creates a new Load Recipe and adds it to the collection.
Signature
Create(name, description, dataType)
Parameters: - name (str) – Name of the load recipe. If None, then a valid unique name will be generated. NOTE: The full Unicode character set is not supported for this parameter.
- description (str) – NOTE: The full Unicode character set is not supported for this parameter.
- dataType (
NXOpen.CAE.SimLoadRecipeTypesDataTypes
) –
Returns: Return type: New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Delete¶
-
SimLoadRecipeCollection.
Delete
¶ Delete a list of load recipes
Signature
Delete(recipes)
Parameters: recipes (list of NXOpen.CAE.SimLoadRecipe
) – The recipes to be deletedNew in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Find¶
-
SimLoadRecipeCollection.
Find
¶ Finds a Load Recipe with a specified name.
Signature
Find(name)
Parameters: name (str) – name of the load recipe Returns: Return type: NXOpen.CAE.SimLoadRecipe
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)