ResultFiletype Enumeration¶
NXOpen.CAE.Result.Filetype is an alias for NXOpen.CAE.ResultFiletype
-
class
NXOpen.CAE.
ResultFiletype
¶ Bases:
object
The result file type
Enum Members
Enum Member Enum Member Description Nastran Ideas Bud Vki Abaqus Ansys Mapped Afu Rs2 AbaqusOdb LsdynaState PermasPost SamcefDes NastranXdb -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-