NodeModifyLabelBuilder Class¶
-
class
NXOpen.CAE.
NodeModifyLabelBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.NodeModifyLabelBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateNodeModifyLabelBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DispCsys | Returns or sets the disp csys |
Increment | Returns or sets the increment |
Label | Returns or sets the label |
LabelOption | Returns or sets the label option |
Node | Returns the node |
Offset | Returns or sets the offset |
RefCsys | Returns or sets the ref csys |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
NodeModifyLabelBuilderLabelType Enumeration | the label types |
Property Detail¶
DispCsys¶
-
NodeModifyLabelBuilder.
DispCsys
¶ Returns or sets the disp csys
-------------------------------------
Getter Method
Signature
DispCsys()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DispCsys(dispCsys)
Parameters: dispCsys ( NXOpen.CoordinateSystem
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Increment¶
-
NodeModifyLabelBuilder.
Increment
¶ Returns or sets the increment
-------------------------------------
Getter Method
Signature
Increment()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Increment(increment)
Parameters: increment (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Label¶
-
NodeModifyLabelBuilder.
Label
¶ Returns or sets the label
-------------------------------------
Getter Method
Signature
Label()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Label(label)
Parameters: label (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
LabelOption¶
-
NodeModifyLabelBuilder.
LabelOption
¶ Returns or sets the label option
-------------------------------------
Getter Method
Signature
LabelOption()
Returns: Return type: NXOpen.CAE.NodeModifyLabelBuilderLabelType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LabelOption(labelOption)
Parameters: labelOption ( NXOpen.CAE.NodeModifyLabelBuilderLabelType
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Node¶
-
NodeModifyLabelBuilder.
Node
¶ Returns the node
-------------------------------------
Getter Method
Signature
Node()
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX5.0.0.
License requirements: None.
Offset¶
-
NodeModifyLabelBuilder.
Offset
¶ Returns or sets the offset
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Offset(offset)
Parameters: offset (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
RefCsys¶
-
NodeModifyLabelBuilder.
RefCsys
¶ Returns or sets the ref csys
-------------------------------------
Getter Method
Signature
RefCsys()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RefCsys(refCsys)
Parameters: refCsys ( NXOpen.CoordinateSystem
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
NodeModifyLabelBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.