BaseResultType Class¶
-
class
NXOpen.CAE.
BaseResultType
¶ Bases:
NXOpen.TaggedObject
This class provides interfaces to query result type attributes
An instance of this class can not be obtained
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Complex | Returns a value indicating whether the result type is a complex value |
Datatype | Returns the NXOpen.CAE.ResultDataType for this result type |
Location | Returns the NXOpen.CAE.ResultLocation where this result type is defined |
Name | Returns the name for this result type |
Quantity | Returns the NXOpen.CAE.ResultQuantity for this result type |
Tag | Returns the Tag for this object. |
UserName | Returns or sets the user defined name of this result type |
Methods¶
Method | Description |
---|---|
AskComponents | Return all results components available for this result type @return |
GetSectionDefined | Returns the sections where this result is defined. |
Property Detail¶
Complex¶
-
BaseResultType.
Complex
¶ Returns a value indicating whether the result type is a complex value
-------------------------------------
Getter Method
Signature
Complex()
Returns: Return type: bool New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Datatype¶
-
BaseResultType.
Datatype
¶ Returns the
NXOpen.CAE.ResultDataType
for this result type-------------------------------------
Getter Method
Signature
Datatype()
Returns: Return type: NXOpen.CAE.ResultDataType
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Location¶
-
BaseResultType.
Location
¶ Returns the
NXOpen.CAE.ResultLocation
where this result type is defined-------------------------------------
Getter Method
Signature
Location()
Returns: Return type: NXOpen.CAE.ResultLocation
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Name¶
-
BaseResultType.
Name
¶ Returns the name for this result type
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Quantity¶
-
BaseResultType.
Quantity
¶ Returns the
NXOpen.CAE.ResultQuantity
for this result type-------------------------------------
Getter Method
Signature
Quantity()
Returns: Return type: NXOpen.CAE.ResultQuantity
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
UserName¶
-
BaseResultType.
UserName
¶ Returns or sets the user defined name of this result type
-------------------------------------
Getter Method
Signature
UserName()
Returns: Return type: str New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
UserName(name)
Parameters: name (str) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
AskComponents¶
-
BaseResultType.
AskComponents
¶ Return all results components available for this result type
Signature
AskComponents()
Returns: a tuple Return type: A tuple consisting of (description, components). description is a list of str. components is a list of NXOpen.CAE.ResultComponent
.New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetSectionDefined¶
-
BaseResultType.
GetSectionDefined
¶ Returns the sections where this result is defined.
This method should be used to find out what are those sections. If a result contain both shell and beam elements and this result is defined in different sections of respective elements, say TOP, BOTTOM, StressRecoveryPointC etc., then all of them will be returned in this array.
Signature
GetSectionDefined()
Returns: Return type: list of NXOpen.CAE.ResultSection
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)