DurabilityEventCollection Class¶
-
class
NXOpen.CAE.
DurabilityEventCollection
¶ Bases:
object
Represents a collection of durability events.
To obtain an instance of this class, refer to
NXOpen.CAE.DurabilityMetaSolution
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
CloneEvent | Makes a clone of a durability event. |
CreateRandomEventBuilder | Creates the builder object of the durability random event. |
CreateStaticEventBuilder | Creates the builder object of the durability static event. |
CreateTransientEventBuilder | Creates the builder object of the durability transient event. |
DeleteEvent | Delete a durability event. |
FindObject | Finds a durability event with a specified name. |
Method Detail¶
CloneEvent¶
-
DurabilityEventCollection.
CloneEvent
¶ Makes a clone of a durability event.
Signature
CloneEvent(source)
Parameters: source ( NXOpen.CAE.DurabilityEvent
) – Source eventReturns: Cloned event Return type: NXOpen.CAE.DurabilityEvent
New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
CreateRandomEventBuilder¶
-
DurabilityEventCollection.
CreateRandomEventBuilder
¶ Creates the builder object of the durability random event.
Signature
CreateRandomEventBuilder(eventTag)
Parameters: eventTag ( NXOpen.CAE.DurabilityRandomEvent
) –Returns: Return type: NXOpen.CAE.DurabilityRandomEventBuilder
New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
CreateStaticEventBuilder¶
-
DurabilityEventCollection.
CreateStaticEventBuilder
¶ Creates the builder object of the durability static event.
Signature
CreateStaticEventBuilder(eventTag)
Parameters: eventTag ( NXOpen.CAE.DurabilityStaticEvent
) –Returns: Return type: NXOpen.CAE.DurabilityStaticEventBuilder
New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
CreateTransientEventBuilder¶
-
DurabilityEventCollection.
CreateTransientEventBuilder
¶ Creates the builder object of the durability transient event.
Signature
CreateTransientEventBuilder(eventTag)
Parameters: eventTag ( NXOpen.CAE.DurabilityTransientEvent
) –Returns: Return type: NXOpen.CAE.DurabilityTransientEventBuilder
New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
DeleteEvent¶
-
DurabilityEventCollection.
DeleteEvent
¶ Delete a durability event.
Signature
DeleteEvent(eventTag)
Parameters: eventTag ( NXOpen.CAE.DurabilityEvent
) – The durability event to be deletedNew in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
FindObject¶
-
DurabilityEventCollection.
FindObject
¶ Finds a durability event with a specified name.
Signature
FindObject(name)
Parameters: name (str) – name of the durability event Returns: The durability event Return type: NXOpen.CAE.DurabilityEvent
New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)