CaeSetGroupFilterType Enumeration¶
-
class
NXOpen.CAE.
CaeSetGroupFilterType
¶ Bases:
object
Used to specify the filter to extract type of objects from a group e.
g geometric face, element, node ..etc Enum Members
Enum Member Enum Member Description Node filter type is nodeElement fitler type is any elementGeomFace filter type is geometric faceGeomBody filter type is geometric bodyGeomCurve filter type is geometric curveGeomPoint filter type is geometric pointPointElement filter type is 0D elementBeamElement filter type is 1D elementShellElement filter type is 2D elementSolidElement filter type is 3D elementGeomPlanarFace filter type is geometric planar faceGeomCylFace filter type is geometric cylindrical faceBeamElementTypeBar filter type is 1D element of type BarBeamElementTypeBeam filter type is 1D element of type BeamBeamElementTypeRod filter type is 1D element of type RodBeamElementTypeBearing filter type is 1D element of type BearingNodeAndElement filter type is any node and elementCaeGeometry filter type is any cae geometryCaeMesh filter type is any cae mesh-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-