WeldBuilderNumberOfPointsOnEdgeType Enumeration¶
NXOpen.CAE.WeldBuilder.NumberOfPointsOnEdgeType is an alias for NXOpen.CAE.WeldBuilderNumberOfPointsOnEdgeType
-
class
NXOpen.CAE.
WeldBuilderNumberOfPointsOnEdgeType
¶ Bases:
object
Represents the options for specifying maximum number of weld points on an edge
Enum Members
Enum Member Enum Member Description MaximumNumber Create the maximum number of points on an edgeSpecifiedNumber Specify the number of points to be created on an edge-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-